<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 iMX8M Plus: MCLK2 select clock on SAI[x] interface</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-MCLK2-select-clock-on-SAI-x-interface/m-p/1308260#M176973</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am trying to enable one of MCLK2 select clocks e.g. on SAI1 interface and don't see any clocks on SAI1_MCLK pin. Default I am using MCLK1 with SAI1_CLK_ROOT clock and it is working. But if I am trying to change CKKEN0 and SAI1_MCLK_SEL registers to enable SAI1_CLK_ROOT on SAI1_MCKL2 then it does't work. I use memtool from Yocto package imx-test to set relevat bits in the AUDIO BKL_CTRL and SAI1 registers. According to the figure 14-4 from ref. man. IMX8MPRM Rev.1, 06/2021 it should be possible to activate MCLK1-3.&lt;/P&gt;&lt;P&gt;I am using rel_imx_5.4.70_2.3.2 based Yocto BSP.&lt;/P&gt;&lt;P&gt;Do you have any ideas or maybe one example how I can enable e.g. SAI1_MCLK2 clock.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
    <pubDate>Thu, 15 Jul 2021 10:32:59 GMT</pubDate>
    <dc:creator>ad-fsdev</dc:creator>
    <dc:date>2021-07-15T10:32:59Z</dc:date>
    <item>
      <title>iMX8M Plus: MCLK2 select clock on SAI[x] interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-MCLK2-select-clock-on-SAI-x-interface/m-p/1308260#M176973</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am trying to enable one of MCLK2 select clocks e.g. on SAI1 interface and don't see any clocks on SAI1_MCLK pin. Default I am using MCLK1 with SAI1_CLK_ROOT clock and it is working. But if I am trying to change CKKEN0 and SAI1_MCLK_SEL registers to enable SAI1_CLK_ROOT on SAI1_MCKL2 then it does't work. I use memtool from Yocto package imx-test to set relevat bits in the AUDIO BKL_CTRL and SAI1 registers. According to the figure 14-4 from ref. man. IMX8MPRM Rev.1, 06/2021 it should be possible to activate MCLK1-3.&lt;/P&gt;&lt;P&gt;I am using rel_imx_5.4.70_2.3.2 based Yocto BSP.&lt;/P&gt;&lt;P&gt;Do you have any ideas or maybe one example how I can enable e.g. SAI1_MCLK2 clock.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Thu, 15 Jul 2021 10:32:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-MCLK2-select-clock-on-SAI-x-interface/m-p/1308260#M176973</guid>
      <dc:creator>ad-fsdev</dc:creator>
      <dc:date>2021-07-15T10:32:59Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8M Plus: MCLK2 select clock on SAI[x] interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-MCLK2-select-clock-on-SAI-x-interface/m-p/1311869#M177338</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;See the following descriptions in Reference Manual, please!&lt;/P&gt;
&lt;P&gt;---------------------------------&lt;/P&gt;
&lt;P&gt;14.1.1.1 SAI Master Clock Inputs/Outputs&lt;BR /&gt;The MCLK pin on each SAI module can be configured as either an input or an output.&lt;BR /&gt;When configured as an output, the SAIn_CLK_ROOT from the CCM or the&lt;BR /&gt;MCLK_OUT from SAIn is routed to the pad output. &lt;STRONG&gt;Note that the SAIn_MCLK_OUT is&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;always derived from the ipg_clk_sai_mclk (MCLK[1]) input&lt;/STRONG&gt;. When configured as an&lt;BR /&gt;input, the external input to the pad will be used as SAIn_MCLK and is routed to&lt;BR /&gt;SAIn_MCLK_IN, which can be used as master clock for SAI.&lt;/P&gt;
&lt;P&gt;------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;It means that only MCLK[1] can be routed to SAI1_MCLK pad.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a nice day!&lt;/P&gt;
&lt;P&gt;regards,&lt;/P&gt;
&lt;P&gt;weidong&lt;/P&gt;</description>
      <pubDate>Thu, 22 Jul 2021 08:42:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-MCLK2-select-clock-on-SAI-x-interface/m-p/1311869#M177338</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2021-07-22T08:42:35Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8M Plus: MCLK2 select clock on SAI[x] interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-MCLK2-select-clock-on-SAI-x-interface/m-p/1311936#M177348</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;thank you for your reply. Would you please confirm some statemans bellow for better understanding from my site.&lt;/P&gt;&lt;P&gt;1) Is the SAIn_MCLK_OUT a out clock from blue block figure 14-4 in ref. man?&lt;/P&gt;&lt;P&gt;2) So if I understand you correctly it is not possiblle to route SAI1_CLK_ROOT or other SAI[x]_CLK_ROOT over SAI1_MCLK_SEL[MCLK2_SEL] multiplexer with enabled CLK_EN[SAI1_MCLK2] (disabled CLK_EN0[SAI1_MCLK1]) as output clock from SAI1 blue block figure 14-4 in ref. man.&lt;BR /&gt;&lt;BR /&gt;Thank you again for your time.&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 22 Jul 2021 10:36:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-MCLK2-select-clock-on-SAI-x-interface/m-p/1311936#M177348</guid>
      <dc:creator>ad-fsdev</dc:creator>
      <dc:date>2021-07-22T10:36:18Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8M Plus: MCLK2 select clock on SAI[x] interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-MCLK2-select-clock-on-SAI-x-interface/m-p/1312343#M177387</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; It means that only &lt;STRONG&gt;MCLK[1]&lt;/STRONG&gt; can be routed out to CPU pad(SAI1_MCLK).&lt;/P&gt;
&lt;P&gt;&amp;nbsp;So &lt;STRONG&gt;MCLK[2]&lt;/STRONG&gt;&amp;nbsp; &lt;STRONG&gt;is only used for internal SAI module.&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;Have a nice day!&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;weidong&lt;/P&gt;</description>
      <pubDate>Fri, 23 Jul 2021 05:30:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-MCLK2-select-clock-on-SAI-x-interface/m-p/1312343#M177387</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2021-07-23T05:30:41Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8M Plus: MCLK2 select clock on SAI[x] interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-MCLK2-select-clock-on-SAI-x-interface/m-p/1320152#M178062</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;thank you.&lt;/P&gt;</description>
      <pubDate>Mon, 09 Aug 2021 07:04:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-MCLK2-select-clock-on-SAI-x-interface/m-p/1320152#M178062</guid>
      <dc:creator>ad-fsdev</dc:creator>
      <dc:date>2021-08-09T07:04:49Z</dc:date>
    </item>
  </channel>
</rss>