<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックModifying CPU and LPDDR4 Frequency</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Modifying-CPU-and-LPDDR4-Frequency/m-p/1307575#M176908</link>
    <description>&lt;P&gt;Hello Community Members,&lt;/P&gt;&lt;P&gt;We are using a DART-MX8MM-Mini based custom board. We are observing that when we execute our application that streams camera captured images on the LCD screen, the temperature reaches 85 deg C which is not acceptable so we want our system to drive at half of CPU &amp;amp; LPDDR4 frequency in the kernel.&lt;/P&gt;&lt;P&gt;Currently, CPU Frequency is 1200MHZ and LPDDR4 frequency is 750MHZ&lt;/P&gt;&lt;P&gt;How can we achieve CPU frequency around 600MHZ and LPDDR4 frequency of 375MHZ?&lt;/P&gt;&lt;P&gt;Please guide.&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
    <pubDate>Wed, 14 Jul 2021 09:17:02 GMT</pubDate>
    <dc:creator>sd05</dc:creator>
    <dc:date>2021-07-14T09:17:02Z</dc:date>
    <item>
      <title>Modifying CPU and LPDDR4 Frequency</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Modifying-CPU-and-LPDDR4-Frequency/m-p/1307575#M176908</link>
      <description>&lt;P&gt;Hello Community Members,&lt;/P&gt;&lt;P&gt;We are using a DART-MX8MM-Mini based custom board. We are observing that when we execute our application that streams camera captured images on the LCD screen, the temperature reaches 85 deg C which is not acceptable so we want our system to drive at half of CPU &amp;amp; LPDDR4 frequency in the kernel.&lt;/P&gt;&lt;P&gt;Currently, CPU Frequency is 1200MHZ and LPDDR4 frequency is 750MHZ&lt;/P&gt;&lt;P&gt;How can we achieve CPU frequency around 600MHZ and LPDDR4 frequency of 375MHZ?&lt;/P&gt;&lt;P&gt;Please guide.&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
      <pubDate>Wed, 14 Jul 2021 09:17:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Modifying-CPU-and-LPDDR4-Frequency/m-p/1307575#M176908</guid>
      <dc:creator>sd05</dc:creator>
      <dc:date>2021-07-14T09:17:02Z</dc:date>
    </item>
    <item>
      <title>Re: Modifying CPU and LPDDR4 Frequency</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Modifying-CPU-and-LPDDR4-Frequency/m-p/1307645#M176916</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/182130"&gt;@sd05&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp; To modify the DRAM Frequency for a custom setting refer to&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/iMX-8M-Mini-Register-Programming-Aid-DRAM-PLL-setting/ta-p/1112094" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/iMX-8M-Mini-Register-Programming-Aid-DRAM-PLL-setting/ta-p/1112094&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;"i.MX 8M Family DDR Tool Release"&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/1104467" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/1104467&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;For CPU frequency - use Linux CPUFREQ settings.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/reference-manual/IMX_REFERENCE_MANUAL.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/reference-manual/IMX_REFERENCE_MANUAL.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Yuri.&lt;/P&gt;</description>
      <pubDate>Wed, 14 Jul 2021 11:06:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Modifying-CPU-and-LPDDR4-Frequency/m-p/1307645#M176916</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2021-07-14T11:06:32Z</dc:date>
    </item>
  </channel>
</rss>