<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: mxrt 1060 cfgTool programming bootable image</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/mxrt-1060-cfgTool-programming-bootable-image/m-p/1307570#M176907</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;now I'm trying to use MCUXpreso MCU setting with flash loader .cfx.&lt;/P&gt;&lt;P&gt;I looks like it works, but probably it doesn't.&lt;/P&gt;&lt;P&gt;But thanks for your time.&lt;/P&gt;</description>
    <pubDate>Wed, 14 Jul 2021 09:08:27 GMT</pubDate>
    <dc:creator>filip091</dc:creator>
    <dc:date>2021-07-14T09:08:27Z</dc:date>
    <item>
      <title>mxrt 1060 cfgTool programming bootable image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mxrt-1060-cfgTool-programming-bootable-image/m-p/1302996#M176454</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have problem with programming bootable image using cfgTool, want to program QSPI flash on MXRT 1060. I've generated bootable image using elftosb tool from Flashloader, I don't know if it works. Now I'm trying to use cfgTool but it writes no device detected. My cfg.ini looks like&amp;nbsp;&lt;/P&gt;&lt;P&gt;[profiles]&lt;/P&gt;&lt;P&gt;chip = MXRT106X&lt;/P&gt;&lt;P&gt;[platform]&lt;/P&gt;&lt;P&gt;board =&lt;/P&gt;&lt;P&gt;[LIST]&lt;BR /&gt;name = MXRT106x-DevBootSerialFlashXiP&lt;/P&gt;&lt;P&gt;I've also tried other names. MfgTool.log shows&lt;/P&gt;&lt;P&gt;DLL version: 2.7.0&lt;BR /&gt;Tuesday, July 06, 2021 10:26:56 Start new logging&lt;BR /&gt;ModuleID[2] LevelID[10]: CMyExceptionHandler thread is running&lt;BR /&gt;ModuleID[2] LevelID[1]: new MxHidDeviceClass&lt;BR /&gt;ModuleID[2] LevelID[1]: new KBLHidDeviceClass&lt;BR /&gt;ModuleID[2] LevelID[10]: Device Manager thread is running&lt;BR /&gt;ModuleID[2] LevelID[1]: Can't set m_hStopEvent before it initialized or it already stop&lt;/P&gt;&lt;P&gt;or with some other names also this:&lt;/P&gt;&lt;P&gt;ModuleID[2] LevelID[10]: CCmdOpreation[0] thread is Closed&lt;BR /&gt;ModuleID[2] LevelID[10]: CCmdOpreation[0] thread is Closed&lt;BR /&gt;ModuleID[2] LevelID[10]: DeviceManager::OnMsgDeviceEvent() - EVENT_KILL&lt;BR /&gt;ModuleID[2] LevelID[10]: CMyExceptionHandler::OnMsgExceptionEvent() - KillExceptionHandlerThread&lt;BR /&gt;ModuleID[2] LevelID[10]: Exception Handler thread is closed&lt;BR /&gt;ModuleID[2] LevelID[1]: delete MxHidDeviceClass&lt;BR /&gt;ModuleID[2] LevelID[1]: delete MxHidDeviceClass&lt;BR /&gt;ModuleID[2] LevelID[10]: Device Manager thread is closed&lt;/P&gt;&lt;P&gt;Thanks for any kind of help.&lt;/P&gt;</description>
      <pubDate>Tue, 06 Jul 2021 08:38:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mxrt-1060-cfgTool-programming-bootable-image/m-p/1302996#M176454</guid>
      <dc:creator>filip091</dc:creator>
      <dc:date>2021-07-06T08:38:50Z</dc:date>
    </item>
    <item>
      <title>Re: mxrt 1060 cfgTool programming bootable image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mxrt-1060-cfgTool-programming-bootable-image/m-p/1305620#M176703</link>
      <description>&lt;P&gt;Hello Filip091,&lt;/P&gt;
&lt;P&gt;If the board is not being detected I would recommend making sure that the i.MXRT1060 is entering Serial Downloader Mode.&lt;/P&gt;
&lt;P&gt;If you have problems with the manufacturing tool, which hasn’t been updated in a while, there are tools that provide similar functionality like the MCU Boot Flasher, which you may obtain from the link below:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://github.com/JayHeng/NXP-MCUBootFlasher" target="_blank"&gt;https://github.com/JayHeng/NXP-MCUBootFlasher&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;I hope that this information helps!&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Gustavo&lt;/P&gt;</description>
      <pubDate>Fri, 09 Jul 2021 19:49:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mxrt-1060-cfgTool-programming-bootable-image/m-p/1305620#M176703</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2021-07-09T19:49:46Z</dc:date>
    </item>
    <item>
      <title>Re: mxrt 1060 cfgTool programming bootable image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mxrt-1060-cfgTool-programming-bootable-image/m-p/1307570#M176907</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;now I'm trying to use MCUXpreso MCU setting with flash loader .cfx.&lt;/P&gt;&lt;P&gt;I looks like it works, but probably it doesn't.&lt;/P&gt;&lt;P&gt;But thanks for your time.&lt;/P&gt;</description>
      <pubDate>Wed, 14 Jul 2021 09:08:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mxrt-1060-cfgTool-programming-bootable-image/m-p/1307570#M176907</guid>
      <dc:creator>filip091</dc:creator>
      <dc:date>2021-07-14T09:08:27Z</dc:date>
    </item>
  </channel>
</rss>