<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic bitbake image for mys6ul14x14 error: Could not include required file recipes-fsl in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/bitbake-image-for-mys6ul14x14-error-Could-not-include-required/m-p/1307040#M176845</link>
    <description>&lt;P&gt;I got the following error attempting to "bitbake core-image-base" for mys6ul14x14:&lt;/P&gt;&lt;P&gt;ERROR: ParseError at /home/totalit/MYS6ULx-devel/fsl-release-yocto/sources/meta-myir-imx6ulx/recipes-fsl/images/fsl-image-gui.bb:4: Could not include required file recipes-fsl/images/fsl-image-validation-imx.bb&lt;/P&gt;&lt;P&gt;I tried to copy this file from meta-fsl-bsp-release directory, but it entails another error.&lt;/P&gt;&lt;P&gt;I'm using MYS-6ULX full package and didn't modify any file except bblayers (it can't find the machine folder without it).&lt;/P&gt;</description>
    <pubDate>Tue, 13 Jul 2021 14:35:54 GMT</pubDate>
    <dc:creator>totalit</dc:creator>
    <dc:date>2021-07-13T14:35:54Z</dc:date>
    <item>
      <title>bitbake image for mys6ul14x14 error: Could not include required file recipes-fsl</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/bitbake-image-for-mys6ul14x14-error-Could-not-include-required/m-p/1307040#M176845</link>
      <description>&lt;P&gt;I got the following error attempting to "bitbake core-image-base" for mys6ul14x14:&lt;/P&gt;&lt;P&gt;ERROR: ParseError at /home/totalit/MYS6ULx-devel/fsl-release-yocto/sources/meta-myir-imx6ulx/recipes-fsl/images/fsl-image-gui.bb:4: Could not include required file recipes-fsl/images/fsl-image-validation-imx.bb&lt;/P&gt;&lt;P&gt;I tried to copy this file from meta-fsl-bsp-release directory, but it entails another error.&lt;/P&gt;&lt;P&gt;I'm using MYS-6ULX full package and didn't modify any file except bblayers (it can't find the machine folder without it).&lt;/P&gt;</description>
      <pubDate>Tue, 13 Jul 2021 14:35:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/bitbake-image-for-mys6ul14x14-error-Could-not-include-required/m-p/1307040#M176845</guid>
      <dc:creator>totalit</dc:creator>
      <dc:date>2021-07-13T14:35:54Z</dc:date>
    </item>
    <item>
      <title>Re: bitbake image for mys6ul14x14 error: Could not include required file recipes-fsl</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/bitbake-image-for-mys6ul14x14-error-Could-not-include-required/m-p/1307694#M176923</link>
      <description>&lt;P&gt;Hello totallit,&lt;/P&gt;
&lt;P&gt;Please Don't do that; this is ugly! You can get similar result using: IMAGE_FEATURES += "tools-sdk" in your local.conf and building: bitbake fsl-image-multimedia .On the other hand, the fsl-image*.bb image recipes are under sources/meta-fsl-demos/recipes-fsl/images/&lt;/P&gt;
&lt;P&gt;Try to download the version 5.10.35 of the BSP and follow up the Yocto User guide document to run yocto on MX6ULL.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 14 Jul 2021 13:03:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/bitbake-image-for-mys6ul14x14-error-Could-not-include-required/m-p/1307694#M176923</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2021-07-14T13:03:37Z</dc:date>
    </item>
    <item>
      <title>Re: bitbake image for mys6ul14x14 error: Could not include required file recipes-fsl</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/bitbake-image-for-mys6ul14x14-error-Could-not-include-required/m-p/1309833#M177146</link>
      <description>&lt;P&gt;Finally, I've created an image using the last BSP and according to&amp;nbsp;&lt;SPAN&gt;Yocto User guide (instead of MYS packages and MYS linux guide). Thank you for the tip!&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 19 Jul 2021 11:44:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/bitbake-image-for-mys6ul14x14-error-Could-not-include-required/m-p/1309833#M177146</guid>
      <dc:creator>totalit</dc:creator>
      <dc:date>2021-07-19T11:44:37Z</dc:date>
    </item>
  </channel>
</rss>