<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックi.MX8MM Accessing Board Serial Number, Assembly and Part Number in Linux OS</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MM-Accessing-Board-Serial-Number-Assembly-and-Part-Number/m-p/1288030#M176839</link>
    <description>&lt;P&gt;I've got an i.MX8MM som running Debian Buster OS and Kernel 4.19.35. I would like to access the Board Serial Number, Assembly and Part Numbers, that are displayed by the U-Boot logs, from the Linux OS.&lt;/P&gt;&lt;P&gt;The U-boot code seems to read these values from an on board EEPROM, is there a way to access the same from the userspace and read the values in the EEPROM?&lt;/P&gt;</description>
    <pubDate>Mon, 07 Jun 2021 07:35:46 GMT</pubDate>
    <dc:creator>harsh1621</dc:creator>
    <dc:date>2021-06-07T07:35:46Z</dc:date>
    <item>
      <title>i.MX8MM Accessing Board Serial Number, Assembly and Part Number in Linux OS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MM-Accessing-Board-Serial-Number-Assembly-and-Part-Number/m-p/1288030#M176839</link>
      <description>&lt;P&gt;I've got an i.MX8MM som running Debian Buster OS and Kernel 4.19.35. I would like to access the Board Serial Number, Assembly and Part Numbers, that are displayed by the U-Boot logs, from the Linux OS.&lt;/P&gt;&lt;P&gt;The U-boot code seems to read these values from an on board EEPROM, is there a way to access the same from the userspace and read the values in the EEPROM?&lt;/P&gt;</description>
      <pubDate>Mon, 07 Jun 2021 07:35:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8MM-Accessing-Board-Serial-Number-Assembly-and-Part-Number/m-p/1288030#M176839</guid>
      <dc:creator>harsh1621</dc:creator>
      <dc:date>2021-06-07T07:35:46Z</dc:date>
    </item>
  </channel>
</rss>