<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: imx8 plus. Resolution 1920x1200 with two cameras in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8-plus-Resolution-1920x1200-with-two-cameras/m-p/1306765#M176809</link>
    <description>&lt;P&gt;the documentation says that the maximum resolution is 1936x1188&lt;BR /&gt;&lt;STRONG&gt;How do we switch to this resolution 1936x1188?&lt;/STRONG&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 13 Jul 2021 09:08:55 GMT</pubDate>
    <dc:creator>Creative</dc:creator>
    <dc:date>2021-07-13T09:08:55Z</dc:date>
    <item>
      <title>imx8 plus. Resolution 1920x1200 with two cameras</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8-plus-Resolution-1920x1200-with-two-cameras/m-p/1302504#M176415</link>
      <description>&lt;P&gt;Hi&lt;BR /&gt;Our iMX8 PLUS platform&lt;BR /&gt;We have two cameras daA3840-30mc&lt;/P&gt;&lt;P&gt;Can't get an image larger than 1920x1080. What needs to be changed in the kernel or driver to get a resolution of 1920x1280?&lt;/P&gt;</description>
      <pubDate>Mon, 05 Jul 2021 14:26:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8-plus-Resolution-1920x1200-with-two-cameras/m-p/1302504#M176415</guid>
      <dc:creator>Creative</dc:creator>
      <dc:date>2021-07-05T14:26:39Z</dc:date>
    </item>
    <item>
      <title>Re: imx8 plus. Resolution 1920x1200 with two cameras</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8-plus-Resolution-1920x1200-with-two-cameras/m-p/1303167#M176468</link>
      <description>&lt;P&gt;Hello Creative,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The i.MX8MP has a resolution maximum of 1920x1080, since is 1080p you cannot get more resolution since is the limit of hardware.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 06 Jul 2021 13:01:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8-plus-Resolution-1920x1200-with-two-cameras/m-p/1303167#M176468</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2021-07-06T13:01:55Z</dc:date>
    </item>
    <item>
      <title>Re: imx8 plus. Resolution 1920x1200 with two cameras</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8-plus-Resolution-1920x1200-with-two-cameras/m-p/1306765#M176809</link>
      <description>&lt;P&gt;the documentation says that the maximum resolution is 1936x1188&lt;BR /&gt;&lt;STRONG&gt;How do we switch to this resolution 1936x1188?&lt;/STRONG&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 13 Jul 2021 09:08:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8-plus-Resolution-1920x1200-with-two-cameras/m-p/1306765#M176809</guid>
      <dc:creator>Creative</dc:creator>
      <dc:date>2021-07-13T09:08:55Z</dc:date>
    </item>
  </channel>
</rss>