<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックError build only kernel image in imx8m mini evk for Android 10 OS</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Error-build-only-kernel-image-in-imx8m-mini-evk-for-Android-10/m-p/1306519#M176791</link>
    <description>&lt;P&gt;Error build only kernel image in imx8m mini evk for Android 10 OS&lt;/P&gt;&lt;P&gt;i am getting error as make mrproper&lt;/P&gt;&lt;P&gt;i have attached screenshot below&lt;/P&gt;&lt;P&gt;Kindly provide the solution&lt;/P&gt;&lt;P&gt;Thanks and regards&lt;/P&gt;&lt;P&gt;Ruban&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 13 Jul 2021 03:57:10 GMT</pubDate>
    <dc:creator>Ruban1</dc:creator>
    <dc:date>2021-07-13T03:57:10Z</dc:date>
    <item>
      <title>Error build only kernel image in imx8m mini evk for Android 10 OS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-build-only-kernel-image-in-imx8m-mini-evk-for-Android-10/m-p/1306519#M176791</link>
      <description>&lt;P&gt;Error build only kernel image in imx8m mini evk for Android 10 OS&lt;/P&gt;&lt;P&gt;i am getting error as make mrproper&lt;/P&gt;&lt;P&gt;i have attached screenshot below&lt;/P&gt;&lt;P&gt;Kindly provide the solution&lt;/P&gt;&lt;P&gt;Thanks and regards&lt;/P&gt;&lt;P&gt;Ruban&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 13 Jul 2021 03:57:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-build-only-kernel-image-in-imx8m-mini-evk-for-Android-10/m-p/1306519#M176791</guid>
      <dc:creator>Ruban1</dc:creator>
      <dc:date>2021-07-13T03:57:10Z</dc:date>
    </item>
    <item>
      <title>Re: Error build only kernel image in imx8m mini evk for Android 10 OS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-build-only-kernel-image-in-imx8m-mini-evk-for-Android-10/m-p/1307030#M176843</link>
      <description>&lt;P&gt;Hello Ruban1,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;At this point we can see that when there is a .config file in the kernel/ directory or a config/ directory exists in the kernel/include/ directory, the shell prints the error message seen at the beginning of this paragraph and exits. The solution to the problem is to delete the 2 objects. Go to the kernel/ directory and look for the .config file. If you go to the kernel/include/ directory, you will find the config/ directory! Go into the directory and see that it is empty (an empty directory can cause the entire project to fail to compile, and the details affect the success or failure!).&lt;/P&gt;
&lt;P&gt;After removing the config/ directory, go back to the top of the Android project, re-execute the source and lunch commands, and recompile.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Tue, 13 Jul 2021 14:14:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-build-only-kernel-image-in-imx8m-mini-evk-for-Android-10/m-p/1307030#M176843</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2021-07-13T14:14:03Z</dc:date>
    </item>
    <item>
      <title>Re: Error build only kernel image in imx8m mini evk for Android 10 OS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-build-only-kernel-image-in-imx8m-mini-evk-for-Android-10/m-p/1307319#M176873</link>
      <description>&lt;P&gt;I am not able to find .config file.. the only file available is config.list.&lt;/P&gt;&lt;P&gt;Regard&amp;nbsp;&lt;/P&gt;&lt;P&gt;Ruban&lt;/P&gt;</description>
      <pubDate>Wed, 14 Jul 2021 04:00:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-build-only-kernel-image-in-imx8m-mini-evk-for-Android-10/m-p/1307319#M176873</guid>
      <dc:creator>Ruban1</dc:creator>
      <dc:date>2021-07-14T04:00:58Z</dc:date>
    </item>
  </channel>
</rss>