<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: FlexCAN Message Filtering</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/FlexCAN-Message-Filtering/m-p/1305656#M176706</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;You may try by modifying the rxIdentifier value to the ID you expect to receive from.&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
    <pubDate>Fri, 09 Jul 2021 21:51:23 GMT</pubDate>
    <dc:creator>AldoG</dc:creator>
    <dc:date>2021-07-09T21:51:23Z</dc:date>
    <item>
      <title>FlexCAN Message Filtering</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FlexCAN-Message-Filtering/m-p/1295396#M175792</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm developing an application on one of the Cortex-M4 using flexCAN.&lt;/P&gt;&lt;P&gt;Using the "flexcan_interrupt_transfer" from the SDK as a base for my development a question about ID filtering arised. I'm using standard ID and data frames, nothing out of the ordinary. At this point I am able to filter a single ID or let all ID pass. However, I'd like to know if it is possible to filter determined ranges of ID. The software I'm doing is for a device controller that sends and receives messages to and from a bunch of other devices (CAN nodes), so I want to filter all the messages that my device is supposed to receive from the other devices and not all of the spectrum of ID (from 1 to 2047).&lt;/P&gt;&lt;P&gt;Also, I'd like to know if it is possible to assign a Message Buffer to a determined range of ID, for example, ID 1 to 100 to Rx MB 1, ID 101 to 200&amp;nbsp;to Rx MB 2, and so on.&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Juan&lt;/P&gt;</description>
      <pubDate>Mon, 21 Jun 2021 11:19:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FlexCAN-Message-Filtering/m-p/1295396#M175792</guid>
      <dc:creator>juanigevo</dc:creator>
      <dc:date>2021-06-21T11:19:16Z</dc:date>
    </item>
    <item>
      <title>Re: FlexCAN Message Filtering</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FlexCAN-Message-Filtering/m-p/1305656#M176706</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;You may try by modifying the rxIdentifier value to the ID you expect to receive from.&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Fri, 09 Jul 2021 21:51:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FlexCAN-Message-Filtering/m-p/1305656#M176706</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2021-07-09T21:51:23Z</dc:date>
    </item>
  </channel>
</rss>