<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: BOOT_CFG pin pull ups during reset in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/BOOT-CFG-pin-pull-ups-during-reset/m-p/232093#M17669</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Pull up / down options of i.MX6 pins are software configurable, therefore BOOT_CFG pins pulling during reset / power-up are not fully&lt;/P&gt;&lt;P&gt;defined. This means external resistors should be applied (except the case fuse-only boot configuration), as recommended in the Design Checklist :&lt;BR /&gt;"The BOOT_CFG signals are required for proper functionality and operation and should not be left floating."&lt;/P&gt;&lt;P&gt;"Each EIM boot signal should connect to a series resistor to isolate the bus from the resistors and/or switchers; [...].&lt;/P&gt;&lt;P&gt;Each configured EIM boot signal sees either a 14.7 kΩ pulldown or a 4.7 kΩ pullup. For each switch-enabled&lt;/P&gt;&lt;P&gt;pulled-up signal, the supply is presented with a 10 kΩ current load. "&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 14 Jan 2014 03:15:37 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2014-01-14T03:15:37Z</dc:date>
    <item>
      <title>BOOT_CFG pin pull ups during reset</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/BOOT-CFG-pin-pull-ups-during-reset/m-p/232092#M17668</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The BOOT_CFG balls are listed as having pull ups, and I would like to know if these pull-ups are active during reset. This would let us save the routing to those balls if we want them to be set to 1, and aren't using them after reset. I could not find any details about this in the SRC, Fusemap, or System Boot chapters of the iMX6 Reference Manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This would be using Internal Boot Mode (BOOT_MODE[1:0] = 0b10).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Jan 2014 18:58:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/BOOT-CFG-pin-pull-ups-during-reset/m-p/232092#M17668</guid>
      <dc:creator>AlexHarford</dc:creator>
      <dc:date>2014-01-13T18:58:17Z</dc:date>
    </item>
    <item>
      <title>Re: BOOT_CFG pin pull ups during reset</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/BOOT-CFG-pin-pull-ups-during-reset/m-p/232093#M17669</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Pull up / down options of i.MX6 pins are software configurable, therefore BOOT_CFG pins pulling during reset / power-up are not fully&lt;/P&gt;&lt;P&gt;defined. This means external resistors should be applied (except the case fuse-only boot configuration), as recommended in the Design Checklist :&lt;BR /&gt;"The BOOT_CFG signals are required for proper functionality and operation and should not be left floating."&lt;/P&gt;&lt;P&gt;"Each EIM boot signal should connect to a series resistor to isolate the bus from the resistors and/or switchers; [...].&lt;/P&gt;&lt;P&gt;Each configured EIM boot signal sees either a 14.7 kΩ pulldown or a 4.7 kΩ pullup. For each switch-enabled&lt;/P&gt;&lt;P&gt;pulled-up signal, the supply is presented with a 10 kΩ current load. "&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Jan 2014 03:15:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/BOOT-CFG-pin-pull-ups-during-reset/m-p/232093#M17669</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2014-01-14T03:15:37Z</dc:date>
    </item>
    <item>
      <title>Re: BOOT_CFG pin pull ups during reset</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/BOOT-CFG-pin-pull-ups-during-reset/m-p/232094#M17670</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Yuri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if we want to use serial boot mode ("01"), in order to program the fuses with manufacturer tool kit (over USB) or JTAG tool software, do we still need to use all of these resistors? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Mehmet Ali Ipin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Oct 2014 05:51:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/BOOT-CFG-pin-pull-ups-during-reset/m-p/232094#M17670</guid>
      <dc:creator>MehmetAliIpin</dc:creator>
      <dc:date>2014-10-24T05:51:43Z</dc:date>
    </item>
    <item>
      <title>Re: BOOT_CFG pin pull ups during reset</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/BOOT-CFG-pin-pull-ups-during-reset/m-p/232095#M17671</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt; For fuse only or serial boot modes there is no need for the resistors. &lt;/P&gt;&lt;P&gt;In the same time, &lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;SD Manufacture mode may influence here :&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/392591"&gt;Re: i.MX6 solo: problem forcing it into USB serial downloader mode&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; ~Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Oct 2014 06:39:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/BOOT-CFG-pin-pull-ups-during-reset/m-p/232095#M17671</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2014-10-24T06:39:23Z</dc:date>
    </item>
  </channel>
</rss>