<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: NFS with post-build helper script in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/NFS-with-post-build-helper-script/m-p/1304798#M176614</link>
    <description>&lt;P&gt;I know this site. I'm already familiar with the setup at all. However, a shortcoming is the lack of specific setting when NFSv4 is used (pseudo root).&lt;/P&gt;&lt;P&gt;But far more important: The script automatically adjusts to the appropriate Image &amp;amp; (default) device tree files as well as mount the appropriate root file system location to &lt;FONT face="andale mono,times"&gt;/srv/nfsv4/&lt;/FONT&gt; if I &lt;STRONG&gt;bitbake&lt;/STRONG&gt; another project image. Although fully automatic, if the script would be called automatically as a post build action.&lt;/P&gt;&lt;P&gt;BTW: For i.MX8, a more appropriate Variscite wiki-entry would be &lt;A href="https://variwiki.com/index.php?title=Yocto_Setup_TFTP/NFS&amp;amp;release=RELEASE_HARDKNOTT_V1.0_DART-MX8M-MINI," target="_blank"&gt;https://variwiki.com/index.php?title=Yocto_Setup_TFTP/NFS&amp;amp;release=RELEASE_HARDKNOTT_V1.0_DART-MX8M-MINI&lt;/A&gt;, because it recognizes that zImage is no longer used.&lt;/P&gt;</description>
    <pubDate>Thu, 08 Jul 2021 13:22:09 GMT</pubDate>
    <dc:creator>rjm</dc:creator>
    <dc:date>2021-07-08T13:22:09Z</dc:date>
    <item>
      <title>NFS with post-build helper script</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/NFS-with-post-build-helper-script/m-p/1304055#M176550</link>
      <description>&lt;P&gt;For the (new) helper script, see &lt;A href="https://community.nxp.com/t5/i-MX-Processors/Boot-i-MX8MM-using-NFS/m-p/1302365/highlight/true#M176404" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/Boot-i-MX8MM-using-NFS/m-p/1302365/highlight/true#M176404&lt;/A&gt;&lt;/P&gt;&lt;P&gt;It is preliminary but operates very well. If anybody is able to make a post-build &lt;STRONG&gt;bitbake&lt;/STRONG&gt; hook of this, that would be appreciated.&lt;/P&gt;</description>
      <pubDate>Wed, 07 Jul 2021 14:48:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/NFS-with-post-build-helper-script/m-p/1304055#M176550</guid>
      <dc:creator>rjm</dc:creator>
      <dc:date>2021-07-07T14:48:41Z</dc:date>
    </item>
    <item>
      <title>Re: NFS with post-build helper script</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/NFS-with-post-build-helper-script/m-p/1304786#M176613</link>
      <description>&lt;P&gt;Hello rjm,&lt;/P&gt;
&lt;P&gt;Are you able to try:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://variwiki.com/index.php?title=Yocto_Setup_TFTP/NFS" target="_blank"&gt;https://variwiki.com/index.php?title=Yocto_Setup_TFTP/NFS&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Thu, 08 Jul 2021 13:08:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/NFS-with-post-build-helper-script/m-p/1304786#M176613</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2021-07-08T13:08:33Z</dc:date>
    </item>
    <item>
      <title>Re: NFS with post-build helper script</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/NFS-with-post-build-helper-script/m-p/1304798#M176614</link>
      <description>&lt;P&gt;I know this site. I'm already familiar with the setup at all. However, a shortcoming is the lack of specific setting when NFSv4 is used (pseudo root).&lt;/P&gt;&lt;P&gt;But far more important: The script automatically adjusts to the appropriate Image &amp;amp; (default) device tree files as well as mount the appropriate root file system location to &lt;FONT face="andale mono,times"&gt;/srv/nfsv4/&lt;/FONT&gt; if I &lt;STRONG&gt;bitbake&lt;/STRONG&gt; another project image. Although fully automatic, if the script would be called automatically as a post build action.&lt;/P&gt;&lt;P&gt;BTW: For i.MX8, a more appropriate Variscite wiki-entry would be &lt;A href="https://variwiki.com/index.php?title=Yocto_Setup_TFTP/NFS&amp;amp;release=RELEASE_HARDKNOTT_V1.0_DART-MX8M-MINI," target="_blank"&gt;https://variwiki.com/index.php?title=Yocto_Setup_TFTP/NFS&amp;amp;release=RELEASE_HARDKNOTT_V1.0_DART-MX8M-MINI&lt;/A&gt;, because it recognizes that zImage is no longer used.&lt;/P&gt;</description>
      <pubDate>Thu, 08 Jul 2021 13:22:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/NFS-with-post-build-helper-script/m-p/1304798#M176614</guid>
      <dc:creator>rjm</dc:creator>
      <dc:date>2021-07-08T13:22:09Z</dc:date>
    </item>
  </channel>
</rss>