<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Virtual channel support on IMX8M Mini</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Virtual-channel-support-on-IMX8M-Mini/m-p/1303954#M176539</link>
    <description>&lt;P&gt;Perfect, thanks&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/26366"&gt;@weidong_sun&lt;/a&gt; for this clear answer which helps me lot!&lt;/P&gt;&lt;P&gt;I would appreciate if someone has a solution for Q3 &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 07 Jul 2021 12:09:23 GMT</pubDate>
    <dc:creator>jfontain88</dc:creator>
    <dc:date>2021-07-07T12:09:23Z</dc:date>
    <item>
      <title>Virtual channel support on IMX8M Mini</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Virtual-channel-support-on-IMX8M-Mini/m-p/1303824#M176522</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I read a lot of posts on the forums about virtuals channels support but some of them says different things. The main question of the topic is:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Q1.&lt;/STRONG&gt; Does the IMX8M Mini support virtual channels (in order to split one incoming MIPI CSI-2 stream into different camera flows based on their VC-ID) ?&lt;/P&gt;&lt;P&gt;This is not clear because the RM of the 8M Mini mentions "virtual channels" (at section 13.4.15.16) without explaining clearly if it is supported or not... Moreover, the driver mxc-mipi-csi2_yav.c stores a "csi2dev-&amp;gt;vchannel" boolean but seems to be unused.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Q2.&lt;/STRONG&gt; If not supported, which IMX processors support it? I read the IMX7D RM and it seems that it support it but what about the others 8M series or the 6 series?&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Q3.&lt;/STRONG&gt; Last question but not the least, is there any way to implement "by hand" a virtual channel support by reading packet header of incoming data stream for example? Or maybe by doing similarly to this post: &lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/iMX6DQ-MAX9286-MIPI-CSI2-720P-camera-surround-view-solution-for/ta-p/1116501" target="_blank" rel="noopener"&gt;iMX6DQ-MAX9286-MIPI-CSI2-720P-camera-surround-view-solution&lt;/A&gt; ?&amp;nbsp; Do you have any idea or the best solution is to go on another processor?&lt;/P&gt;&lt;P&gt;Thanks a lot for your answers!&lt;/P&gt;&lt;P&gt;Jfontain&lt;/P&gt;</description>
      <pubDate>Wed, 07 Jul 2021 09:04:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Virtual-channel-support-on-IMX8M-Mini/m-p/1303824#M176522</guid>
      <dc:creator>jfontain88</dc:creator>
      <dc:date>2021-07-07T09:04:13Z</dc:date>
    </item>
    <item>
      <title>Re: Virtual channel support on IMX8M Mini</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Virtual-channel-support-on-IMX8M-Mini/m-p/1303938#M176536</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;1. The MIPI CSI-2 of&amp;nbsp; i.MX8M/MINI doesn't support virtual channel.&lt;/P&gt;&lt;P&gt;2. The following i.mx processors , you can evaluate, their MIPI CSI-2 supports virtual channel.&lt;/P&gt;&lt;P&gt;--i.MX6Q &amp;amp; i.MX6QP&lt;/P&gt;&lt;P&gt;--I.MX8QM &amp;amp; I.MX8X&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Have a nice day!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;weidong&lt;/P&gt;</description>
      <pubDate>Wed, 07 Jul 2021 11:41:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Virtual-channel-support-on-IMX8M-Mini/m-p/1303938#M176536</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2021-07-07T11:41:29Z</dc:date>
    </item>
    <item>
      <title>Re: Virtual channel support on IMX8M Mini</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Virtual-channel-support-on-IMX8M-Mini/m-p/1303954#M176539</link>
      <description>&lt;P&gt;Perfect, thanks&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/26366"&gt;@weidong_sun&lt;/a&gt; for this clear answer which helps me lot!&lt;/P&gt;&lt;P&gt;I would appreciate if someone has a solution for Q3 &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 07 Jul 2021 12:09:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Virtual-channel-support-on-IMX8M-Mini/m-p/1303954#M176539</guid>
      <dc:creator>jfontain88</dc:creator>
      <dc:date>2021-07-07T12:09:23Z</dc:date>
    </item>
    <item>
      <title>Re: Virtual channel support on IMX8M Mini</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Virtual-channel-support-on-IMX8M-Mini/m-p/1305059#M176631</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;For Q3, &lt;SPAN class="VIiyi"&gt;&lt;SPAN class="JLqJ4b ChMk0b" data-language-for-alternatives="en" data-language-to-translate-into="zh-CN" data-phrase-index="0"&gt;&lt;SPAN&gt;you can only refer to iMX6DQ-MAX9286-MIPI-CSI2-720P-camera-surround-view-solution.&lt;/SPAN&gt;&lt;/SPAN&gt; &lt;SPAN class="JLqJ4b ChMk0b" data-language-for-alternatives="en" data-language-to-translate-into="zh-CN" data-phrase-index="1"&gt;&lt;SPAN&gt;Apart from this, there are no other examples.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="VIiyi"&gt;&lt;SPAN class="JLqJ4b ChMk0b" data-language-for-alternatives="en" data-language-to-translate-into="zh-CN" data-phrase-index="1"&gt;&lt;SPAN&gt;Have a goog day!&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="VIiyi"&gt;&lt;SPAN class="JLqJ4b ChMk0b" data-language-for-alternatives="en" data-language-to-translate-into="zh-CN" data-phrase-index="1"&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="VIiyi"&gt;&lt;SPAN class="JLqJ4b ChMk0b" data-language-for-alternatives="en" data-language-to-translate-into="zh-CN" data-phrase-index="1"&gt;&lt;SPAN&gt;weidong&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 09 Jul 2021 00:16:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Virtual-channel-support-on-IMX8M-Mini/m-p/1305059#M176631</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2021-07-09T00:16:15Z</dc:date>
    </item>
  </channel>
</rss>