<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MFGTool2 get MAC address on error in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MFGTool2-get-MAC-address-on-error/m-p/1303897#M176531</link>
    <description>&lt;P&gt;I am using MFGTool2 (ucl2.xml) for burning 4 devices at the same time. I would like to get the MAC address of the device if any of the processes does not success. I have tried to obtain the MAC address on a .txt before and after the proccess to compare it later with the following comand:&lt;/P&gt;&lt;P&gt;&amp;lt;CMD state="Updater" type="push" body="read [.txt with the MAC]" savedfile="MAC.txt"&amp;gt;Obtaining MAC&amp;lt;/CMD&amp;gt;&lt;/P&gt;&lt;P&gt;Since the 4 processes happen paralelly the .txt is overwritten resulting in only the last MAC address. I have not found much info of ucl2 commands.&lt;/P&gt;&lt;P&gt;So is it possible to just append the MAC instead of overwrite it to the .txt or just to get the .txt when an error occurs?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Wed, 07 Jul 2021 10:30:41 GMT</pubDate>
    <dc:creator>Alex_S</dc:creator>
    <dc:date>2021-07-07T10:30:41Z</dc:date>
    <item>
      <title>MFGTool2 get MAC address on error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MFGTool2-get-MAC-address-on-error/m-p/1303897#M176531</link>
      <description>&lt;P&gt;I am using MFGTool2 (ucl2.xml) for burning 4 devices at the same time. I would like to get the MAC address of the device if any of the processes does not success. I have tried to obtain the MAC address on a .txt before and after the proccess to compare it later with the following comand:&lt;/P&gt;&lt;P&gt;&amp;lt;CMD state="Updater" type="push" body="read [.txt with the MAC]" savedfile="MAC.txt"&amp;gt;Obtaining MAC&amp;lt;/CMD&amp;gt;&lt;/P&gt;&lt;P&gt;Since the 4 processes happen paralelly the .txt is overwritten resulting in only the last MAC address. I have not found much info of ucl2 commands.&lt;/P&gt;&lt;P&gt;So is it possible to just append the MAC instead of overwrite it to the .txt or just to get the .txt when an error occurs?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Wed, 07 Jul 2021 10:30:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MFGTool2-get-MAC-address-on-error/m-p/1303897#M176531</guid>
      <dc:creator>Alex_S</dc:creator>
      <dc:date>2021-07-07T10:30:41Z</dc:date>
    </item>
  </channel>
</rss>