<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX8 CPU temperature in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8-CPU-temperature/m-p/1302151#M176385</link>
    <description>We use the industrial grade part with Tj max 105C, while the BSP for EVK by default has the commercial grade part, which is only supported up to 95C. We need detail guidance to change the shut down temperature to a higher number.</description>
    <pubDate>Mon, 05 Jul 2021 02:46:31 GMT</pubDate>
    <dc:creator>MinminGu</dc:creator>
    <dc:date>2021-07-05T02:46:31Z</dc:date>
    <item>
      <title>i.MX8 CPU temperature</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8-CPU-temperature/m-p/1302151#M176385</link>
      <description>We use the industrial grade part with Tj max 105C, while the BSP for EVK by default has the commercial grade part, which is only supported up to 95C. We need detail guidance to change the shut down temperature to a higher number.</description>
      <pubDate>Mon, 05 Jul 2021 02:46:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8-CPU-temperature/m-p/1302151#M176385</guid>
      <dc:creator>MinminGu</dc:creator>
      <dc:date>2021-07-05T02:46:31Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8 CPU temperature</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8-CPU-temperature/m-p/1304613#M176596</link>
      <description>&lt;P&gt;Which product are you using?&lt;/P&gt;</description>
      <pubDate>Thu, 08 Jul 2021 08:23:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8-CPU-temperature/m-p/1304613#M176596</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2021-07-08T08:23:09Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8 CPU temperature</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8-CPU-temperature/m-p/1884303#M224731</link>
      <description>&lt;P&gt;MIMX8MQ6CVAHZAB&lt;/P&gt;</description>
      <pubDate>Mon, 10 Jun 2024 14:38:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8-CPU-temperature/m-p/1884303#M224731</guid>
      <dc:creator>dhacker</dc:creator>
      <dc:date>2024-06-10T14:38:01Z</dc:date>
    </item>
  </channel>
</rss>