<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Issue in enabling LCDIF clock at uboot level in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Issue-in-enabling-LCDIF-clock-at-uboot-level/m-p/1302012#M176364</link>
    <description>&lt;P&gt;Hi Sunidhi&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;for uboot mipi-dsi usage one can look at&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/uboot-imx/tree/board/freescale/imx8mm_evk/imx8mm_evk.c?h=imx_v2018.03_4.14.98_2.0.0_ga" target="_blank"&gt;https://source.codeaurora.org/external/imx/uboot-imx/tree/board/freescale/imx8mm_evk/imx8mm_evk.c?h=imx_v2018.03_4.14.98_2.0.0_ga&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
    <pubDate>Fri, 02 Jul 2021 23:37:33 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2021-07-02T23:37:33Z</dc:date>
    <item>
      <title>Issue in enabling LCDIF clock at uboot level</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issue-in-enabling-LCDIF-clock-at-uboot-level/m-p/1301876#M176354</link>
      <description>&lt;P&gt;&lt;SPAN class="RFZYhc"&gt;We are having a imx8m mini based customboard we want to port&amp;nbsp; MIPI DSI based st7703 lcd panel driver at uboot and display splash screen.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="RFZYhc"&gt;1. We are able to port the st7703 driver (taking&amp;nbsp; reference of rm67191 driver) with uboot 2020 version for our board as well. Probe is getting call and please see the logs, video-link is being created with lcdif, video bridge and panel. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="RFZYhc"&gt;2. Since the mipi panel is already working in the kernel, so we kind of ported the clock values as well. But as attached in clk-dump the usecnt is 0 for all the display related clocks. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="RFZYhc"&gt;3. We also see in imx8mm.dtsi file there is display-subsystem node, whose compatible string matches with the drm core. But in uboot we do not have support for it. Do we need to add that?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="RFZYhc"&gt;Currently everything is working fine, but somehow the clock is not getting init. We also probed the hardware and we do not see the clk with the probe too&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 02 Jul 2021 14:07:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issue-in-enabling-LCDIF-clock-at-uboot-level/m-p/1301876#M176354</guid>
      <dc:creator>sd05</dc:creator>
      <dc:date>2021-07-02T14:07:27Z</dc:date>
    </item>
    <item>
      <title>Re: Issue in enabling LCDIF clock at uboot level</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issue-in-enabling-LCDIF-clock-at-uboot-level/m-p/1302012#M176364</link>
      <description>&lt;P&gt;Hi Sunidhi&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;for uboot mipi-dsi usage one can look at&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/uboot-imx/tree/board/freescale/imx8mm_evk/imx8mm_evk.c?h=imx_v2018.03_4.14.98_2.0.0_ga" target="_blank"&gt;https://source.codeaurora.org/external/imx/uboot-imx/tree/board/freescale/imx8mm_evk/imx8mm_evk.c?h=imx_v2018.03_4.14.98_2.0.0_ga&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Fri, 02 Jul 2021 23:37:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issue-in-enabling-LCDIF-clock-at-uboot-level/m-p/1302012#M176364</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-07-02T23:37:33Z</dc:date>
    </item>
  </channel>
</rss>