<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic iMX8M Plus SDIO external pull-ups necessary or internal pull-ups are enough? (For WiFi/BTH module) in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-SDIO-external-pull-ups-necessary-or-internal-pull-ups/m-p/1300174#M176226</link>
    <description>&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;I have some doubts about the real need of externall pull-ups for SDIO lines used for a WiFi Module (in our case JODY-W2 by Ublox).&lt;/P&gt;&lt;P&gt;Due to reviewing some EVKs, I have seen that external pull-ups are not used for the SDIO lines, and we wonder if just with the configuration of the pin, in the NXP Pinmux tool, as "internal pull-up enabled" it would work.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Charlie_Owz_0-1625035626835.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/148343i78FFCA633787644B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Charlie_Owz_0-1625035626835.png" alt="Charlie_Owz_0-1625035626835.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Is that right? &lt;SPAN class="VIiyi"&gt;&lt;SPAN class="JLqJ4b ChMk0b"&gt;&lt;SPAN&gt;Would that be enough?&lt;/SPAN&gt;&lt;/SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="VIiyi"&gt;&lt;SPAN class="JLqJ4b ChMk0b"&gt;&lt;SPAN&gt;Or on the contrary, Is it necessary to add the pullup?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="VIiyi"&gt;&lt;SPAN class="JLqJ4b ChMk0b"&gt;&lt;SPAN&gt;Many thanks in advance.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 30 Jun 2021 06:53:22 GMT</pubDate>
    <dc:creator>Charlie_Owz</dc:creator>
    <dc:date>2021-06-30T06:53:22Z</dc:date>
    <item>
      <title>iMX8M Plus SDIO external pull-ups necessary or internal pull-ups are enough? (For WiFi/BTH module)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-SDIO-external-pull-ups-necessary-or-internal-pull-ups/m-p/1300174#M176226</link>
      <description>&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;I have some doubts about the real need of externall pull-ups for SDIO lines used for a WiFi Module (in our case JODY-W2 by Ublox).&lt;/P&gt;&lt;P&gt;Due to reviewing some EVKs, I have seen that external pull-ups are not used for the SDIO lines, and we wonder if just with the configuration of the pin, in the NXP Pinmux tool, as "internal pull-up enabled" it would work.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Charlie_Owz_0-1625035626835.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/148343i78FFCA633787644B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Charlie_Owz_0-1625035626835.png" alt="Charlie_Owz_0-1625035626835.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Is that right? &lt;SPAN class="VIiyi"&gt;&lt;SPAN class="JLqJ4b ChMk0b"&gt;&lt;SPAN&gt;Would that be enough?&lt;/SPAN&gt;&lt;/SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="VIiyi"&gt;&lt;SPAN class="JLqJ4b ChMk0b"&gt;&lt;SPAN&gt;Or on the contrary, Is it necessary to add the pullup?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="VIiyi"&gt;&lt;SPAN class="JLqJ4b ChMk0b"&gt;&lt;SPAN&gt;Many thanks in advance.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 30 Jun 2021 06:53:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-SDIO-external-pull-ups-necessary-or-internal-pull-ups/m-p/1300174#M176226</guid>
      <dc:creator>Charlie_Owz</dc:creator>
      <dc:date>2021-06-30T06:53:22Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8M Plus SDIO external pull-ups necessary or internal pull-ups are enough? (For WiFi/BTH modul</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-SDIO-external-pull-ups-necessary-or-internal-pull-ups/m-p/1300213#M176233</link>
      <description>&lt;P&gt;Hi Charlie_Owz,&lt;/P&gt;
&lt;P&gt;Use internal pull up, please! which is enough.&lt;/P&gt;
&lt;P&gt;don't need external pull-up resistors.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a good day!&lt;/P&gt;
&lt;P&gt;B.R,&lt;/P&gt;
&lt;P&gt;weidong&lt;/P&gt;</description>
      <pubDate>Wed, 30 Jun 2021 07:25:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-SDIO-external-pull-ups-necessary-or-internal-pull-ups/m-p/1300213#M176233</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2021-06-30T07:25:54Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8M Plus SDIO external pull-ups necessary or internal pull-ups are enough? (For WiFi/BTH modul</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-SDIO-external-pull-ups-necessary-or-internal-pull-ups/m-p/1376592#M183507</link>
      <description>&lt;P&gt;plz, place external pull up resistor for test. some case(ATWILC3000-MR110xA), internal resistor is not enough.&lt;/P&gt;</description>
      <pubDate>Wed, 24 Nov 2021 23:43:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-SDIO-external-pull-ups-necessary-or-internal-pull-ups/m-p/1376592#M183507</guid>
      <dc:creator>at-at-at-at-at</dc:creator>
      <dc:date>2021-11-24T23:43:54Z</dc:date>
    </item>
  </channel>
</rss>