<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 boot from RAM via u-boot bootm</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/boot-from-RAM-via-u-boot-bootm/m-p/1299556#M176170</link>
    <description>&lt;P&gt;I'm missing documentation regarding booting from u-boot simply from RAM. The official i.MX Linux User's guide only tells one how to flash SD/eMMC etc.&lt;/P&gt;&lt;P&gt;Use case: quick test runs, besides the NFS-boot use case.&lt;/P&gt;</description>
    <pubDate>Tue, 29 Jun 2021 08:44:37 GMT</pubDate>
    <dc:creator>rjm</dc:creator>
    <dc:date>2021-06-29T08:44:37Z</dc:date>
    <item>
      <title>boot from RAM via u-boot bootm</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/boot-from-RAM-via-u-boot-bootm/m-p/1299556#M176170</link>
      <description>&lt;P&gt;I'm missing documentation regarding booting from u-boot simply from RAM. The official i.MX Linux User's guide only tells one how to flash SD/eMMC etc.&lt;/P&gt;&lt;P&gt;Use case: quick test runs, besides the NFS-boot use case.&lt;/P&gt;</description>
      <pubDate>Tue, 29 Jun 2021 08:44:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/boot-from-RAM-via-u-boot-bootm/m-p/1299556#M176170</guid>
      <dc:creator>rjm</dc:creator>
      <dc:date>2021-06-29T08:44:37Z</dc:date>
    </item>
    <item>
      <title>Re: boot from RAM via u-boot bootm</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/boot-from-RAM-via-u-boot-bootm/m-p/1300831#M176276</link>
      <description>&lt;P&gt;Our Linux build does not support such boot.&lt;/P&gt;&lt;P&gt;As for u-boot itself it is able to boot something from the RAM.&lt;BR /&gt;I mean it has commands like fatload or ext4load to load the binary to the RAM and bootm one to run it.&lt;/P&gt;</description>
      <pubDate>Thu, 01 Jul 2021 02:55:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/boot-from-RAM-via-u-boot-bootm/m-p/1300831#M176276</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2021-07-01T02:55:39Z</dc:date>
    </item>
  </channel>
</rss>