<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: FAT partition for Kernel image imx8m Mini</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/FAT-partition-for-Kernel-image-imx8m-Mini/m-p/1299378#M176146</link>
    <description>&lt;P&gt;Recently u-boot did not support ext2/ext3/ext4 filesystems and one was forced to place the kernel on FAT (or directly on the drive, outside of the filesystem).&lt;BR /&gt;Also you can access device tree from windows machine if you attach the card with a cardreader.&lt;/P&gt;
&lt;P&gt;However I suppose there is no strong reason to have this FAT partition instead of using rootfs.&lt;BR /&gt;But it if still recommended.&lt;/P&gt;</description>
    <pubDate>Tue, 29 Jun 2021 04:03:06 GMT</pubDate>
    <dc:creator>b36401</dc:creator>
    <dc:date>2021-06-29T04:03:06Z</dc:date>
    <item>
      <title>FAT partition for Kernel image imx8m Mini</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FAT-partition-for-Kernel-image-imx8m-Mini/m-p/1298352#M176043</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;by default the Linux BSP for imx8m mini creates a FAT partition, separated from RootFS partition, that comprises the Kernel image.&lt;/P&gt;&lt;P&gt;What is the reason why this is a better solution than having a RootFS partition with the Kernel image in it and no FAT partition at all ?&lt;/P&gt;&lt;P&gt;Is it because in the case of corrupted RootFS then Kernel at least will be loaded and can try recovering the RootFS ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thank you&lt;/P&gt;</description>
      <pubDate>Fri, 25 Jun 2021 09:31:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FAT-partition-for-Kernel-image-imx8m-Mini/m-p/1298352#M176043</guid>
      <dc:creator>antonio_santagi</dc:creator>
      <dc:date>2021-06-25T09:31:05Z</dc:date>
    </item>
    <item>
      <title>Re: FAT partition for Kernel image imx8m Mini</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FAT-partition-for-Kernel-image-imx8m-Mini/m-p/1299378#M176146</link>
      <description>&lt;P&gt;Recently u-boot did not support ext2/ext3/ext4 filesystems and one was forced to place the kernel on FAT (or directly on the drive, outside of the filesystem).&lt;BR /&gt;Also you can access device tree from windows machine if you attach the card with a cardreader.&lt;/P&gt;
&lt;P&gt;However I suppose there is no strong reason to have this FAT partition instead of using rootfs.&lt;BR /&gt;But it if still recommended.&lt;/P&gt;</description>
      <pubDate>Tue, 29 Jun 2021 04:03:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FAT-partition-for-Kernel-image-imx8m-Mini/m-p/1299378#M176146</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2021-06-29T04:03:06Z</dc:date>
    </item>
  </channel>
</rss>