<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: 8MMINILPD4-CPU2-DESIGNFILES</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/8MMINILPD4-CPU2-DESIGNFILES/m-p/1298994#M176108</link>
    <description>&lt;P&gt;Yes,When using M.2 WIFI Module on Base Board, remove R215, and populate R116&lt;/P&gt;</description>
    <pubDate>Mon, 28 Jun 2021 09:17:20 GMT</pubDate>
    <dc:creator>Rita_Wang</dc:creator>
    <dc:date>2021-06-28T09:17:20Z</dc:date>
    <item>
      <title>8MMINILPD4-CPU2-DESIGNFILES</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/8MMINILPD4-CPU2-DESIGNFILES/m-p/1298241#M176041</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;We are considering the SOM design with reference to 8MMINILPD4-CPU2.&lt;/P&gt;&lt;P&gt;The SPF-47712_A1.pdf file in 8MMINILPD4-CPU2-DESIGNFILES.zip contains the WIFI/BT Module(Page 10/13) and the SOM Interface(Page 13/13).&lt;/P&gt;&lt;P&gt;In addition, the explanation of "R116" in SOM Interface(Page 13/13) is as folows.&lt;/P&gt;&lt;P&gt;"When using M.2 WIFI Module on Base Board, remove R115, and populate R116!"&lt;/P&gt;&lt;P&gt;However, the WIFI/BT Module(Page 10/13) only has R215 resister as 32K CLKIN.&lt;/P&gt;&lt;P&gt;Isn't R115 described in the SOM Interface (page13/13) a typo in R215 ?&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Tori.&lt;/P&gt;</description>
      <pubDate>Fri, 25 Jun 2021 07:24:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/8MMINILPD4-CPU2-DESIGNFILES/m-p/1298241#M176041</guid>
      <dc:creator>Tori-san</dc:creator>
      <dc:date>2021-06-25T07:24:53Z</dc:date>
    </item>
    <item>
      <title>Re: 8MMINILPD4-CPU2-DESIGNFILES</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/8MMINILPD4-CPU2-DESIGNFILES/m-p/1298956#M176102</link>
      <description>&lt;P&gt;Yes, you are right, for the new board use the R215, you can see it in the new schematic.&lt;/P&gt;</description>
      <pubDate>Mon, 28 Jun 2021 08:09:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/8MMINILPD4-CPU2-DESIGNFILES/m-p/1298956#M176102</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2021-06-28T08:09:02Z</dc:date>
    </item>
    <item>
      <title>Re: 8MMINILPD4-CPU2-DESIGNFILES</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/8MMINILPD4-CPU2-DESIGNFILES/m-p/1298971#M176104</link>
      <description>&lt;P&gt;"When using M.2 WIFI Module on Base Board, remove R115, and populate R116!"&lt;/P&gt;&lt;P&gt;Above comment on "SOM Interface (page13/13)" shoule be replaced as follows, right?&lt;/P&gt;&lt;P&gt;"When using M.2 WIFI Module on Base Board, remove R215, and populate R116!"&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Tori.&lt;/P&gt;</description>
      <pubDate>Mon, 28 Jun 2021 08:27:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/8MMINILPD4-CPU2-DESIGNFILES/m-p/1298971#M176104</guid>
      <dc:creator>Tori-san</dc:creator>
      <dc:date>2021-06-28T08:27:20Z</dc:date>
    </item>
    <item>
      <title>Re: 8MMINILPD4-CPU2-DESIGNFILES</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/8MMINILPD4-CPU2-DESIGNFILES/m-p/1298994#M176108</link>
      <description>&lt;P&gt;Yes,When using M.2 WIFI Module on Base Board, remove R215, and populate R116&lt;/P&gt;</description>
      <pubDate>Mon, 28 Jun 2021 09:17:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/8MMINILPD4-CPU2-DESIGNFILES/m-p/1298994#M176108</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2021-06-28T09:17:20Z</dc:date>
    </item>
  </channel>
</rss>