<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: android p auto source code build for imx8qm failed in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/android-p-auto-source-code-build-for-imx8qm-failed/m-p/1298917#M176099</link>
    <description>&lt;P&gt;There is Android P9.0.0_2.1.1_AUTO (Linux 4.14.98 Kernel)​. You can download it from here.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/software/embedded-software/software-technology-for-android-auto:ANDROID-AUTO?tab=In-Depth_Tab" target="_blank"&gt;https://www.nxp.com/design/software/embedded-software/software-technology-for-android-auto:ANDROID-AUTO?tab=In-Depth_Tab&lt;/A&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 28 Jun 2021 07:23:46 GMT</pubDate>
    <dc:creator>jimmychan</dc:creator>
    <dc:date>2021-06-28T07:23:46Z</dc:date>
    <item>
      <title>android p auto source code build for imx8qm failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/android-p-auto-source-code-build-for-imx8qm-failed/m-p/1295015#M175740</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm building android p auto source code for imx8qm, according to &amp;lt;Android™ User's Guide, Rev. P9.0.0_2.1.0-AUTO-ga&amp;gt;, cmds as below:&lt;/P&gt;&lt;P&gt;source build/envsetup.sh&lt;/P&gt;&lt;P&gt;lunch mek_8q_car-userdebug&lt;/P&gt;&lt;P&gt;make&lt;/P&gt;&lt;P&gt;and then, there are some error messages:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;[ 2% 2872/97727] Merging KERNEL config&lt;BR /&gt;Using /nxp/android_build/vendor/nxp-opensource/kernel_imx/arch/arm64/configs/android_car_defconfig as base&lt;BR /&gt;Merging /nxp/android_build/vendor/nxp-opensource/kernel_imx&lt;BR /&gt;sed: read error on /nxp/android_build/vendor/nxp-opensource/kernel_imx: Is a directory&lt;BR /&gt;cat: /nxp/android_build/vendor/nxp-opensource/kernel_imx: Is a directory&lt;BR /&gt;make[1]: Entering directory '/nxp/android_build/out/target/product/mek_8q/obj/KERNEL_OBJ'&lt;BR /&gt;HOSTCC scripts/basic/fixdep&lt;BR /&gt;GEN ./Makefile&lt;BR /&gt;HOSTCC scripts/kconfig/conf.o&lt;BR /&gt;SHIPPED scripts/kconfig/zconf.tab.c&lt;BR /&gt;SHIPPED scripts/kconfig/zconf.lex.c&lt;BR /&gt;HOSTCC scripts/kconfig/zconf.tab.o&lt;BR /&gt;HOSTLD scripts/kconfig/conf&lt;BR /&gt;scripts/kconfig/conf --alldefconfig Kconfig&lt;BR /&gt;#&lt;BR /&gt;# configuration written to .config&lt;BR /&gt;#&lt;BR /&gt;make[1]: Leaving directory '/nxp/android_build/out/target/product/mek_8q/obj/KERNEL_OBJ'&lt;BR /&gt;Value requested for CONFIG_BT_HS not in final .config&lt;BR /&gt;Requested value: # CONFIG_BT_HS is not set&lt;BR /&gt;Actual value:&lt;/P&gt;&lt;P&gt;Value requested for CONFIG_XEN_BLKDEV_BACKEND not in final .config&lt;BR /&gt;Requested value: CONFIG_XEN_BLKDEV_BACKEND=y&lt;BR /&gt;Actual value:&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;[ 3% 3651/97727] target C++: libv8base &amp;lt;= external/v8/src/base/platform/condition-variable.cc&lt;BR /&gt;[ 3% 3652/97727] target C++: libv8base &amp;lt;= external/v8/src/base/logging.cc&lt;BR /&gt;[ 3% 3653/97727] target C++: libv8base &amp;lt;= external/v8/src/base/sys-info.cc&lt;BR /&gt;[ 3% 3654/97727] Building arm64 4.14 kernel ...&lt;BR /&gt;FAILED: out/target/product/mek_8q/obj/KERNEL_OBJ/arch/arm64/boot/Image.lz4&lt;BR /&gt;/bin/bash -c "(PATH=\$PATH make -j8 SHELL=/bin/bash -C vendor/nxp-opensource/kernel_imx mrproper ) &amp;amp;&amp;amp; (PATH=\$(cd prebuilts/misc/linux-x86/lz4; pwd):\$PATH CCACHE_NODIRECT=\"true\" make -j8 SHELL=/bin/bash -C vendor/nxp-opensource/kernel_imx O=\$(/nxp/android_build/prebuilts/build-tools/linux-x86/bin/ckati --realpath out/target/product/mek_8q/obj/KERNEL_OBJ 2&amp;gt; /dev/null) ARCH=arm64 CROSS_COMPILE=\" /nxp/android_build/prebuilts/gcc/linux-x86/aarch64/aarch64-linux-android-4.9/bin/aarch64-linux-androidkernel-\" KCFLAGS=\"\" KAFLAGS=\"\" Image.lz4 ) &amp;amp;&amp;amp; (PATH=\$(cd prebuilts/misc/linux-x86/lz4; pwd):\$PATH CCACHE_NODIRECT=\"true\" make -j8 SHELL=/bin/bash -C vendor/nxp-opensource/kernel_imx O=\$(/nxp/android_build/prebuilts/build-tools/linux-x86/bin/ckati --realpath out/target/product/mek_8q/obj/KERNEL_OBJ 2&amp;gt; /dev/null) ARCH=arm64 CROSS_COMPILE=\" /nxp/android_build/prebuilts/gcc/linux-x86/aarch64/aarch64-linux-android-4.9/bin/aarch64-linux-androidkernel-\" KCFLAGS=\"\" KAFLAGS=\"\" modules )"&lt;BR /&gt;make: Entering directory '/nxp/android_build/vendor/nxp-opensource/kernel_imx'&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;so why?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 20 Jun 2021 13:46:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/android-p-auto-source-code-build-for-imx8qm-failed/m-p/1295015#M175740</guid>
      <dc:creator>zfreeman2321</dc:creator>
      <dc:date>2021-06-20T13:46:49Z</dc:date>
    </item>
    <item>
      <title>Re: android p auto source code build for imx8qm failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/android-p-auto-source-code-build-for-imx8qm-failed/m-p/1298917#M176099</link>
      <description>&lt;P&gt;There is Android P9.0.0_2.1.1_AUTO (Linux 4.14.98 Kernel)​. You can download it from here.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/software/embedded-software/software-technology-for-android-auto:ANDROID-AUTO?tab=In-Depth_Tab" target="_blank"&gt;https://www.nxp.com/design/software/embedded-software/software-technology-for-android-auto:ANDROID-AUTO?tab=In-Depth_Tab&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 28 Jun 2021 07:23:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/android-p-auto-source-code-build-for-imx8qm-failed/m-p/1298917#M176099</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2021-06-28T07:23:46Z</dc:date>
    </item>
  </channel>
</rss>