<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックEthernet issue when flashing u-boot to RAM using imx_usb</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Ethernet-issue-when-flashing-u-boot-to-RAM-using-imx-usb/m-p/1298693#M176079</link>
    <description>&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;I am flashing u-boot using imx_usb to RAM in my custom board based on NXP IMX6UL EVK, I am getting the following boot logs in the board terminal. The ethernet chip and the ethernet lines are same.Are there any changes i have to make in u-boot?&lt;/P&gt;&lt;P&gt;error:&lt;/P&gt;&lt;P&gt;---------------------------------------------&lt;/P&gt;&lt;P&gt;default u-boot&lt;BR /&gt;--------------------&lt;/P&gt;&lt;P&gt;Welcome to minicom 2.7.1&lt;/P&gt;&lt;P&gt;OPTIONS: I18n&lt;BR /&gt;Compiled on Aug 13 2017, 15:25:34.&lt;BR /&gt;Port /dev/ttyUSB0, 21:06:43&lt;/P&gt;&lt;P&gt;Press CTRL-A Z for help on special keys&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;U-Boot 2020.04-00108-g4979a99482 (Jun 26 2021 - 21:05:42 +0530)&lt;/P&gt;&lt;P&gt;CPU: i.MX6UL rev1.2 528 MHz (running at 396 MHz)&lt;BR /&gt;CPU: Industrial temperature grade (-40C to 105C) at 43C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Model: Freescale i.MX6 UltraLite 14x14 EVK Board&lt;BR /&gt;Board: MX6UL 14x14 EVK&lt;BR /&gt;DRAM: 512 MiB&lt;BR /&gt;MMC: FSL_SDHC: 0, FSL_SDHC: 1&lt;BR /&gt;Loading Environment from MMC... *** Warning - bad CRC, using default environment&lt;/P&gt;&lt;P&gt;[*]-Video Link 0 (480 x 272)&lt;BR /&gt;[0] lcdif@21c8000, video&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc1(part 0) is current device&lt;BR /&gt;Net: Could not get PHY for FEC1: addr 1&lt;BR /&gt;Could not get PHY for FEC1: addr 1&lt;BR /&gt;Get shared mii bus on &lt;A href="mailto:ethernet@2188000" target="_blank"&gt;ethernet@2188000&lt;/A&gt;&lt;/P&gt;&lt;P&gt;----------------------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Sun, 27 Jun 2021 09:03:21 GMT</pubDate>
    <dc:creator>shamiullah</dc:creator>
    <dc:date>2021-06-27T09:03:21Z</dc:date>
    <item>
      <title>Ethernet issue when flashing u-boot to RAM using imx_usb</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Ethernet-issue-when-flashing-u-boot-to-RAM-using-imx-usb/m-p/1298693#M176079</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;I am flashing u-boot using imx_usb to RAM in my custom board based on NXP IMX6UL EVK, I am getting the following boot logs in the board terminal. The ethernet chip and the ethernet lines are same.Are there any changes i have to make in u-boot?&lt;/P&gt;&lt;P&gt;error:&lt;/P&gt;&lt;P&gt;---------------------------------------------&lt;/P&gt;&lt;P&gt;default u-boot&lt;BR /&gt;--------------------&lt;/P&gt;&lt;P&gt;Welcome to minicom 2.7.1&lt;/P&gt;&lt;P&gt;OPTIONS: I18n&lt;BR /&gt;Compiled on Aug 13 2017, 15:25:34.&lt;BR /&gt;Port /dev/ttyUSB0, 21:06:43&lt;/P&gt;&lt;P&gt;Press CTRL-A Z for help on special keys&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;U-Boot 2020.04-00108-g4979a99482 (Jun 26 2021 - 21:05:42 +0530)&lt;/P&gt;&lt;P&gt;CPU: i.MX6UL rev1.2 528 MHz (running at 396 MHz)&lt;BR /&gt;CPU: Industrial temperature grade (-40C to 105C) at 43C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Model: Freescale i.MX6 UltraLite 14x14 EVK Board&lt;BR /&gt;Board: MX6UL 14x14 EVK&lt;BR /&gt;DRAM: 512 MiB&lt;BR /&gt;MMC: FSL_SDHC: 0, FSL_SDHC: 1&lt;BR /&gt;Loading Environment from MMC... *** Warning - bad CRC, using default environment&lt;/P&gt;&lt;P&gt;[*]-Video Link 0 (480 x 272)&lt;BR /&gt;[0] lcdif@21c8000, video&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc1(part 0) is current device&lt;BR /&gt;Net: Could not get PHY for FEC1: addr 1&lt;BR /&gt;Could not get PHY for FEC1: addr 1&lt;BR /&gt;Get shared mii bus on &lt;A href="mailto:ethernet@2188000" target="_blank"&gt;ethernet@2188000&lt;/A&gt;&lt;/P&gt;&lt;P&gt;----------------------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Sun, 27 Jun 2021 09:03:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Ethernet-issue-when-flashing-u-boot-to-RAM-using-imx-usb/m-p/1298693#M176079</guid>
      <dc:creator>shamiullah</dc:creator>
      <dc:date>2021-06-27T09:03:21Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet issue when flashing u-boot to RAM using imx_usb</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Ethernet-issue-when-flashing-u-boot-to-RAM-using-imx-usb/m-p/1298721#M176089</link>
      <description>&lt;P&gt;Hi Shamiullah&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;for "Could not get PHY for FEC1: addr 1" error one can check&lt;/P&gt;
&lt;P&gt;mdio phy addresses in dts&lt;BR /&gt;&lt;A href="https://source.codeaurora.org/external/imx/uboot-imx/tree/arch/arm/dts/imx6ul-14x14-evk.dtsi?h=imx_v2020.04_5.4.70_2.3.0" target="_blank"&gt;https://source.codeaurora.org/external/imx/uboot-imx/tree/arch/arm/dts/imx6ul-14x14-evk.dtsi?h=imx_v2020.04_5.4.70_2.3.0&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;and PHYAD[2:0] in i.MX6UL EVK schematic SPF-28616 p.10&lt;/P&gt;
&lt;H3 class="media-flex-heading"&gt;&lt;A id="docsAndSoftware_designResultTitle1_1" class="dtmcustomrulelink" href="https://www.nxp.com/webapp/Download?colCode=MCIMX6UL-EVK_DESIGNFILES" data-dtmaction="Documents and Software Results - Software Link click" data-dtmsubaction="Design files, Including Hardware Schematics, Gerbers, and OrCAD Files" target="_blank"&gt;Design files, Including Hardware Schematics, Gerbers, and OrCAD Files&lt;/A&gt;&lt;/H3&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Mon, 28 Jun 2021 00:40:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Ethernet-issue-when-flashing-u-boot-to-RAM-using-imx-usb/m-p/1298721#M176089</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-06-28T00:40:01Z</dc:date>
    </item>
  </channel>
</rss>