<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックGot exception while loading hdmitxfw.bin into imx8qm</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Got-exception-while-loading-hdmitxfw-bin-into-imx8qm/m-p/1298512#M176058</link>
    <description>&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I got following exception while loading hdmitxfw.bin into imx8qm custom platform which have only HDMI IN/OUT.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;PRE&gt;++++++++++++++++++++++ board_late_init +++++++++++++++++&lt;BR /&gt;+++++++++ do_hdp +++++++++++&lt;BR /&gt;Loading hdp firmware from 0x0000000084000000 offset 0x0000000000002000&lt;BR /&gt;++++++++++++++++ do_hdp: power on display +++++++++++++++++&lt;BR /&gt;++++++++++++++++ do_hdp: setting display clock +++++++++++++++++&lt;BR /&gt;++++++++++++++++ do_hdp: enable display clock +++++++++++++++++&lt;BR /&gt;++++++++++++++++ do_hdp: cdn_api_loadfirmware +++++++++++++++++&lt;BR /&gt;++++++++++++++++ cdn_api_loadfirmware: +++++++++++++++++&lt;BR /&gt;++++++++++++++++ do_hdp: cdn_api_loadfirmware + 1 +++++++++++++++++&lt;BR /&gt;Loading hdp firmware Complete&lt;BR /&gt;-------------------- do_hdp -----------------&lt;BR /&gt;-------------------- board_late_init --------------------&lt;BR /&gt;++++++++++++++++ initr_fastboot_setup: +++++++++++++++++&lt;BR /&gt;flash target is MMC:0&lt;BR /&gt;libtipc.c: INFO Initializing Trusty device&lt;BR /&gt;invalid exception, which 0x13&lt;BR /&gt;iframe 0xffffffff001686b0:&lt;BR /&gt;x0 0x bc00000b x1 0x 3 x2 0x 0 x3 0x 0&lt;BR /&gt;x4 0x 0 x5 0x 0 x6 0x 0 x7 0x 0&lt;BR /&gt;x8 0x 0 x9 0x ffffffff x10 0x 0 x11 0x 1&lt;BR /&gt;x12 0xffffffff0012b698 x13 0x 1 x14 0x 2 x15 0xffffffff0012b698&lt;BR /&gt;x16 0xffffffff0012b6a0 x17 0xffffffff001675f8 x18 0x 0 x19 0xffffffff001221f0&lt;BR /&gt;x20 0xffffffff00016275 x21 0xffffffff00016264 x22 0xffffffff00016249 x23 0xffffffff00016337&lt;BR /&gt;x24 0xfffffffffffffff1 x25 0x 3c000003 x26 0xffffffff00122500 x27 0x 3c000000&lt;BR /&gt;x28 0xfffffffffffffff9 x29 0xffffffff00168830 lr 0xffffffff00008258 usp 0x 1000000&lt;BR /&gt;elr 0xffffffff000077c8&lt;BR /&gt;spsr 0x a00002c5&lt;BR /&gt;panic (caller 0xffffffff000013e0): die&lt;BR /&gt;HALT: (reason = 9)&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 25 Jun 2021 14:39:50 GMT</pubDate>
    <dc:creator>vinothkumars</dc:creator>
    <dc:date>2021-06-25T14:39:50Z</dc:date>
    <item>
      <title>Got exception while loading hdmitxfw.bin into imx8qm</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Got-exception-while-loading-hdmitxfw-bin-into-imx8qm/m-p/1298512#M176058</link>
      <description>&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I got following exception while loading hdmitxfw.bin into imx8qm custom platform which have only HDMI IN/OUT.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;PRE&gt;++++++++++++++++++++++ board_late_init +++++++++++++++++&lt;BR /&gt;+++++++++ do_hdp +++++++++++&lt;BR /&gt;Loading hdp firmware from 0x0000000084000000 offset 0x0000000000002000&lt;BR /&gt;++++++++++++++++ do_hdp: power on display +++++++++++++++++&lt;BR /&gt;++++++++++++++++ do_hdp: setting display clock +++++++++++++++++&lt;BR /&gt;++++++++++++++++ do_hdp: enable display clock +++++++++++++++++&lt;BR /&gt;++++++++++++++++ do_hdp: cdn_api_loadfirmware +++++++++++++++++&lt;BR /&gt;++++++++++++++++ cdn_api_loadfirmware: +++++++++++++++++&lt;BR /&gt;++++++++++++++++ do_hdp: cdn_api_loadfirmware + 1 +++++++++++++++++&lt;BR /&gt;Loading hdp firmware Complete&lt;BR /&gt;-------------------- do_hdp -----------------&lt;BR /&gt;-------------------- board_late_init --------------------&lt;BR /&gt;++++++++++++++++ initr_fastboot_setup: +++++++++++++++++&lt;BR /&gt;flash target is MMC:0&lt;BR /&gt;libtipc.c: INFO Initializing Trusty device&lt;BR /&gt;invalid exception, which 0x13&lt;BR /&gt;iframe 0xffffffff001686b0:&lt;BR /&gt;x0 0x bc00000b x1 0x 3 x2 0x 0 x3 0x 0&lt;BR /&gt;x4 0x 0 x5 0x 0 x6 0x 0 x7 0x 0&lt;BR /&gt;x8 0x 0 x9 0x ffffffff x10 0x 0 x11 0x 1&lt;BR /&gt;x12 0xffffffff0012b698 x13 0x 1 x14 0x 2 x15 0xffffffff0012b698&lt;BR /&gt;x16 0xffffffff0012b6a0 x17 0xffffffff001675f8 x18 0x 0 x19 0xffffffff001221f0&lt;BR /&gt;x20 0xffffffff00016275 x21 0xffffffff00016264 x22 0xffffffff00016249 x23 0xffffffff00016337&lt;BR /&gt;x24 0xfffffffffffffff1 x25 0x 3c000003 x26 0xffffffff00122500 x27 0x 3c000000&lt;BR /&gt;x28 0xfffffffffffffff9 x29 0xffffffff00168830 lr 0xffffffff00008258 usp 0x 1000000&lt;BR /&gt;elr 0xffffffff000077c8&lt;BR /&gt;spsr 0x a00002c5&lt;BR /&gt;panic (caller 0xffffffff000013e0): die&lt;BR /&gt;HALT: (reason = 9)&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 25 Jun 2021 14:39:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Got-exception-while-loading-hdmitxfw-bin-into-imx8qm/m-p/1298512#M176058</guid>
      <dc:creator>vinothkumars</dc:creator>
      <dc:date>2021-06-25T14:39:50Z</dc:date>
    </item>
    <item>
      <title>Re: Got exception while loading hdmitxfw.bin into imx8qm</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Got-exception-while-loading-hdmitxfw-bin-into-imx8qm/m-p/1298626#M176070</link>
      <description>&lt;P&gt;Hi Vinothkumar&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;one can try to rebuild all image from scratch, carefully checking revisions all sotware components&lt;/P&gt;
&lt;P&gt;as described in Release Notes for each BSP on link&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX?tab=In-Depth_Tab" target="_blank"&gt;https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX?tab=In-Depth_Tab&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Sat, 26 Jun 2021 05:21:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Got-exception-while-loading-hdmitxfw-bin-into-imx8qm/m-p/1298626#M176070</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-06-26T05:21:34Z</dc:date>
    </item>
    <item>
      <title>Re: Got exception while loading hdmitxfw.bin into imx8qm</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Got-exception-while-loading-hdmitxfw-bin-into-imx8qm/m-p/1298694#M176080</link>
      <description>&lt;P&gt;Thank you&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/37066"&gt;@igorpadykov&lt;/a&gt;&amp;nbsp;for the reply,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But, I need how to load and port HDMI TX and RX firmware ( &lt;STRONG&gt;hdmitxfw.bin&lt;/STRONG&gt; &amp;amp; &lt;STRONG&gt;hdmirxfw.bin&lt;/STRONG&gt; ) in uboot as well as kernel in Android 9 Automotive with &lt;STRONG&gt;IMX8QM&lt;/STRONG&gt; which is don't have any lvds connector and we have only &lt;STRONG&gt;hdmi&lt;/STRONG&gt; connection.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is it possible please provide the &lt;STRONG&gt;hdmi porting guide&lt;/STRONG&gt; in Android imx8qm.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;And also MEK board ram size is : &lt;STRONG&gt;6 GB&amp;nbsp;&lt;/STRONG&gt;but custom board ram size is &lt;STRONG&gt;2 GB.&lt;/STRONG&gt;&lt;/P&gt;&lt;PRE&gt;#define IMX_HDMI_FIRMWARE_LOAD_ADDR (CONFIG_SYS_SDRAM_BASE + &lt;STRONG&gt;SZ_64M&lt;/STRONG&gt;)&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Do I needs to configure the IMX_HDMI_FIRMWARE_LOAD_ADDR for custom board ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 27 Jun 2021 13:50:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Got-exception-while-loading-hdmitxfw-bin-into-imx8qm/m-p/1298694#M176080</guid>
      <dc:creator>vinothkumars</dc:creator>
      <dc:date>2021-06-27T13:50:36Z</dc:date>
    </item>
  </channel>
</rss>