<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic I.MX6ULL FEC Memory Leak in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6ULL-FEC-Memory-Leak/m-p/1296712#M175912</link>
    <description>&lt;P&gt;Hi,&lt;BR /&gt;I am using I.MX6ULL BSP 4.1.15_2.0.0ga. A memory leak occurs when monitoring using the free command while LAN is connected. Free memory decreases little by little. Is there a memory leak in the FEC driver?&lt;BR /&gt;(When I unplug the LAN connector, the memory leak stops.)&lt;BR /&gt;However, after 4 days of testing, it seems to converge.&lt;BR /&gt;Is this normal?&amp;nbsp;I would appreciate it if you could tell me the reason for this phenomenon.&lt;/P&gt;&lt;P&gt;# while true; do echo 3 &amp;gt; /proc/sys/vm/drop_caches ; free -b | grep 'buffers/cache' | awk '{ print $4 }'; sleep 1;&amp;nbsp; done&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Sungkyun_0-1624437325674.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/147762iAD541BB72953400B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Sungkyun_0-1624437325674.png" alt="Sungkyun_0-1624437325674.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
    <pubDate>Wed, 23 Jun 2021 08:51:19 GMT</pubDate>
    <dc:creator>Sungkyun</dc:creator>
    <dc:date>2021-06-23T08:51:19Z</dc:date>
    <item>
      <title>I.MX6ULL FEC Memory Leak</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6ULL-FEC-Memory-Leak/m-p/1296712#M175912</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;I am using I.MX6ULL BSP 4.1.15_2.0.0ga. A memory leak occurs when monitoring using the free command while LAN is connected. Free memory decreases little by little. Is there a memory leak in the FEC driver?&lt;BR /&gt;(When I unplug the LAN connector, the memory leak stops.)&lt;BR /&gt;However, after 4 days of testing, it seems to converge.&lt;BR /&gt;Is this normal?&amp;nbsp;I would appreciate it if you could tell me the reason for this phenomenon.&lt;/P&gt;&lt;P&gt;# while true; do echo 3 &amp;gt; /proc/sys/vm/drop_caches ; free -b | grep 'buffers/cache' | awk '{ print $4 }'; sleep 1;&amp;nbsp; done&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Sungkyun_0-1624437325674.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/147762iAD541BB72953400B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Sungkyun_0-1624437325674.png" alt="Sungkyun_0-1624437325674.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Wed, 23 Jun 2021 08:51:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6ULL-FEC-Memory-Leak/m-p/1296712#M175912</guid>
      <dc:creator>Sungkyun</dc:creator>
      <dc:date>2021-06-23T08:51:19Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX6ULL FEC Memory Leak</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6ULL-FEC-Memory-Leak/m-p/1296816#M175924</link>
      <description>&lt;P&gt;Hi Sungkyun&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;L4.1.15_2.0.0 BSP is not more supported as outdated, recommended to migrate to&lt;/P&gt;
&lt;P&gt;latest nxp releases described on&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX?tab=In-Depth_Tab" target="_blank"&gt;https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX?tab=In-Depth_Tab&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Wed, 23 Jun 2021 10:42:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6ULL-FEC-Memory-Leak/m-p/1296816#M175924</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-06-23T10:42:33Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX6ULL FEC Memory Leak</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6ULL-FEC-Memory-Leak/m-p/1296826#M175926</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;The kernel cannot be upgraded because this product is already on sale. Could you explain whether this phenomenon is normal or not?&lt;/P&gt;&lt;P&gt;If it is normal for free memory to decrease for a certain period of time, could it be because of the Ring Buffer?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Thu, 24 Jun 2021 05:57:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6ULL-FEC-Memory-Leak/m-p/1296826#M175926</guid>
      <dc:creator>Sungkyun</dc:creator>
      <dc:date>2021-06-24T05:57:00Z</dc:date>
    </item>
  </channel>
</rss>