<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i.MX8M plus QT Support</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-plus-QT-Support/m-p/1296642#M175907</link>
    <description>&lt;P&gt;The recipes-qt5 is under sources/meta-qt5. If you have the recipes of your old version QT5, you may try to replace the recipes-qt5 there. But I think this is very hard to modify and you may need to spend a lot of time to fix the errors of compiling. Do you mean your old QT application cannot run on the new version of QT? I think you may modify your code to make your application can run on the new version of QT is more easier.&lt;/P&gt;</description>
    <pubDate>Wed, 23 Jun 2021 07:41:55 GMT</pubDate>
    <dc:creator>jimmychan</dc:creator>
    <dc:date>2021-06-23T07:41:55Z</dc:date>
    <item>
      <title>i.MX8M plus QT Support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-plus-QT-Support/m-p/1295826#M175824</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have two QT&amp;nbsp; applications developed using QT 5.6.3 &amp;amp; QT 5.5.1&amp;nbsp; which are running on i.MX6 platform.&lt;/P&gt;&lt;P&gt;I want to run the same QT applications on the i.MX8M Plus.&amp;nbsp;i.MX8M Plus yocto build has QT latest version(5.15.2).&lt;/P&gt;&lt;P&gt;I don't want to upgrade my QT applications.&lt;/P&gt;&lt;P&gt;Can I downgrade the QT version in&amp;nbsp;i.MX8 M Plus yocto build?&amp;nbsp;What changes are required to perform this activity?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Tue, 22 Jun 2021 05:47:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-plus-QT-Support/m-p/1295826#M175824</guid>
      <dc:creator>Akash_Shinde25</dc:creator>
      <dc:date>2021-06-22T05:47:30Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8M plus QT Support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-plus-QT-Support/m-p/1296642#M175907</link>
      <description>&lt;P&gt;The recipes-qt5 is under sources/meta-qt5. If you have the recipes of your old version QT5, you may try to replace the recipes-qt5 there. But I think this is very hard to modify and you may need to spend a lot of time to fix the errors of compiling. Do you mean your old QT application cannot run on the new version of QT? I think you may modify your code to make your application can run on the new version of QT is more easier.&lt;/P&gt;</description>
      <pubDate>Wed, 23 Jun 2021 07:41:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-plus-QT-Support/m-p/1296642#M175907</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2021-06-23T07:41:55Z</dc:date>
    </item>
  </channel>
</rss>