<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX8QXP Pinmux problem with SPDIF0_RX/TX in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-Pinmux-problem-with-SPDIF0-RX-TX/m-p/1296541#M175896</link>
    <description>&lt;P&gt;Sorry for the late replay. Adding this&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="c"&gt;IMX8QXP_COMP_CTL_GPIO_1V8_3V3_GPIORHB_PAD	0x000514a0&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;DIV&gt;to the device tree node&amp;nbsp;&lt;SPAN&gt;pinctrl_hog&lt;/SPAN&gt;&lt;SPAN&gt;:&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;hoggrp did the trick even it is not clear to me what the settings are changing. Setting bits 0 and 2 from field&amp;nbsp;READ_NASRC which is not documented.&lt;/SPAN&gt;&lt;/DIV&gt;</description>
    <pubDate>Wed, 23 Jun 2021 06:12:48 GMT</pubDate>
    <dc:creator>mod42</dc:creator>
    <dc:date>2021-06-23T06:12:48Z</dc:date>
    <item>
      <title>i.MX8QXP Pinmux problem with SPDIF0_RX/TX</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-Pinmux-problem-with-SPDIF0-RX-TX/m-p/1266665#M173061</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;We have a custom iMX8XQP board where we want to use the pads&amp;nbsp;SPDIF0_RX /&amp;nbsp;SPDIF0_TX as GPIOs (LSIO_GPIO0_IO10 /&amp;nbsp;LSIO_GPIO0_IO11). I added the following entries to the pinctrl_hog&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;IMX8QXP_SPDIF0_RX_LSIO_GPIO0_IO10       0x00000041
IMX8QXP_SPDIF0_TX_LSIO_GPIO0_IO11       0x00000041&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;and test the GPIOs through sysfs. The gpios are exported correctly and I can use the files in sysfs but the corresponding pins are always low. I used this approach with a couple of other GPIOs and there it works as expected. Is there anything special about these two pads?&lt;/DIV&gt;&lt;DIV&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/DIV&gt;</description>
      <pubDate>Thu, 22 Apr 2021 12:58:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-Pinmux-problem-with-SPDIF0-RX-TX/m-p/1266665#M173061</guid>
      <dc:creator>mod42</dc:creator>
      <dc:date>2021-04-22T12:58:27Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8QXP Pinmux problem with SPDIF0_RX/TX</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-Pinmux-problem-with-SPDIF0-RX-TX/m-p/1266933#M173081</link>
      <description>&lt;P&gt;Hi Matthias&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;as these pads are dual voltage pads one can try to add GPIORHB setting, described&lt;/P&gt;
&lt;P&gt;in sect.9.2.5.1.75 IOMUXD_COMP_CTL_GPIO_1V8_3V3_GPIORHB (IOMUXD_COMP_CTL_GPIO_1V8_3V3_GPIORHB) &lt;/P&gt;
&lt;P&gt;&lt;A id="relatedDocsClick_2" href="https://www.nxp.com/webapp/Download?colCode=IMX8DQXPRM" target="_blank" rel="noopener"&gt;&lt;STRONG&gt;i.MX 8DualXPlus/8QuadXPlus Applications Processor Reference Manual&lt;/STRONG&gt;&lt;/A&gt;&lt;BR /&gt;as in example :&lt;BR /&gt;&lt;A href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8x-mek.dtsi?h=imx_5.4.70_2.3.0" target="_blank"&gt;https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8x-mek.dtsi?h=imx_5.4.70_2.3.0&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Fri, 23 Apr 2021 00:41:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-Pinmux-problem-with-SPDIF0-RX-TX/m-p/1266933#M173081</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-04-23T00:41:49Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8QXP Pinmux problem with SPDIF0_RX/TX</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-Pinmux-problem-with-SPDIF0-RX-TX/m-p/1296541#M175896</link>
      <description>&lt;P&gt;Sorry for the late replay. Adding this&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="c"&gt;IMX8QXP_COMP_CTL_GPIO_1V8_3V3_GPIORHB_PAD	0x000514a0&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;DIV&gt;to the device tree node&amp;nbsp;&lt;SPAN&gt;pinctrl_hog&lt;/SPAN&gt;&lt;SPAN&gt;:&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;hoggrp did the trick even it is not clear to me what the settings are changing. Setting bits 0 and 2 from field&amp;nbsp;READ_NASRC which is not documented.&lt;/SPAN&gt;&lt;/DIV&gt;</description>
      <pubDate>Wed, 23 Jun 2021 06:12:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-Pinmux-problem-with-SPDIF0-RX-TX/m-p/1296541#M175896</guid>
      <dc:creator>mod42</dc:creator>
      <dc:date>2021-06-23T06:12:48Z</dc:date>
    </item>
  </channel>
</rss>