<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Fast ethernet Performance issue on IMX6  based hardware in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Fast-ethernet-Performance-issue-on-IMX6-based-hardware/m-p/1296457#M175886</link>
    <description>&lt;P&gt;Hi Fast Ethernet controller driver performance is as follows on the same hardware based on IMX6d7cvt08ae.&lt;/P&gt;&lt;P&gt;Its a Gigabit interface.. There are No overruns as well on low performance.&lt;/P&gt;&lt;P&gt;We are seeing this low performance on 4.19.125-fslc+gd839dc0169b3.. But the performance is as expected around 390 Mbps on 4.9.124.&lt;/P&gt;&lt;P&gt;on Linux 4.9.124&lt;/P&gt;&lt;P&gt;root@tcs-imx6:~# iperf3 -c 10.42.0.1&lt;BR /&gt;Connecting to host 10.42.0.1, port 5201&lt;BR /&gt;[ 5] local 10.42.0.137 port 44278 connected to 10.42.0.1 port 5201&lt;BR /&gt;[ ID] Interval Transfer Bitrate Retr Cwnd&lt;BR /&gt;[ 5] 0.00-1.00 sec 46.8 MBytes 392 Mbits/sec 0 327 KBytes&lt;BR /&gt;[ 5] 1.00-2.00 sec 45.7 MBytes 383 Mbits/sec 0 355 KBytes&lt;BR /&gt;[ 5] 2.00-3.00 sec 46.4 MBytes 388 Mbits/sec 0 355 KBytes&lt;BR /&gt;[ 5] 3.00-4.00 sec 45.2 MBytes 381 Mbits/sec 0 379 KBytes&lt;BR /&gt;[ 5] 4.00-5.00 sec 45.8 MBytes 384 Mbits/sec 0 379 KBytes&lt;BR /&gt;[ 5] 5.00-6.01 sec 43.4 MBytes 362 Mbits/sec 0 416 KBytes&lt;BR /&gt;[ 5] 6.01-7.01 sec 46.0 MBytes 386 Mbits/sec 0 440 KBytes&lt;BR /&gt;[ 5] 7.01-8.01 sec 46.7 MBytes 391 Mbits/sec 0 440 KBytes&lt;BR /&gt;[ 5] 8.01-9.02 sec 46.4 MBytes 386 Mbits/sec 0 440 KBytes&lt;BR /&gt;[ 5] 9.02-10.01 sec 45.6 MBytes 386 Mbits/sec 0 440 KBytes&lt;BR /&gt;- - - - - - - - - - - - - - - - - - - - - - - - -&lt;BR /&gt;[ ID] Interval Transfer Bitrate Retr&lt;BR /&gt;[ 5] 0.00-10.01 sec 458 MBytes 384 Mbits/sec 0 sender&lt;BR /&gt;[ 5] 0.00-10.01 sec 457 MBytes 383 Mbits/sec receiver&lt;/P&gt;&lt;P&gt;On Linux 4.19&lt;/P&gt;&lt;P&gt;root@tcs-imx6:~# iperf3 -c 10.42.0.1&lt;BR /&gt;Connecting to host 10.42.0.1, port 5201&lt;BR /&gt;[ 5] local 10.42.0.228 port 44486 connected to 10.42.0.1 port 5201&lt;BR /&gt;[ ID] Interval Transfer Bitrate Retr Cwnd&lt;BR /&gt;[ 5] 0.00-1.00 sec 35.9 MBytes 301 Mbits/sec 0 260 KBytes&lt;BR /&gt;[ 5] 1.00-2.00 sec 37.3 MBytes 312 Mbits/sec 0 272 KBytes&lt;BR /&gt;[ 5] 2.00-3.00 sec 37.1 MBytes 313 Mbits/sec 0 310 KBytes&lt;BR /&gt;[ 5] 3.00-4.00 sec 35.4 MBytes 296 Mbits/sec 0 359 KBytes&lt;BR /&gt;[ 5] 4.00-5.00 sec 38.0 MBytes 319 Mbits/sec 0 373 KBytes&lt;BR /&gt;[ 5] 5.00-6.00 sec 38.8 MBytes 325 Mbits/sec 0 393 KBytes&lt;BR /&gt;[ 5] 6.00-7.00 sec 38.5 MBytes 323 Mbits/sec 0 393 KBytes&lt;BR /&gt;[ 5] 7.00-8.00 sec 41.0 MBytes 344 Mbits/sec 0 393 KBytes&lt;BR /&gt;[ 5] 8.00-9.00 sec 47.2 MBytes 396 Mbits/sec 0 393 KBytes&lt;BR /&gt;[ 5] 9.00-10.00 sec 46.7 MBytes 392 Mbits/sec 0 393 KBytes&lt;BR /&gt;- - - - - - - - - - - - - - - - - - - - - - - - -&lt;BR /&gt;[ ID] Interval Transfer Bitrate Retr&lt;BR /&gt;[ 5] 0.00-10.00 sec 396 MBytes 332 Mbits/sec 0 sender&lt;BR /&gt;[ 5] 0.00-10.00 sec 395 MBytes 332 Mbits/sec receiver&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 23 Jun 2021 02:51:36 GMT</pubDate>
    <dc:creator>suryakanta_moha</dc:creator>
    <dc:date>2021-06-23T02:51:36Z</dc:date>
    <item>
      <title>Fast ethernet Performance issue on IMX6  based hardware</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Fast-ethernet-Performance-issue-on-IMX6-based-hardware/m-p/1296457#M175886</link>
      <description>&lt;P&gt;Hi Fast Ethernet controller driver performance is as follows on the same hardware based on IMX6d7cvt08ae.&lt;/P&gt;&lt;P&gt;Its a Gigabit interface.. There are No overruns as well on low performance.&lt;/P&gt;&lt;P&gt;We are seeing this low performance on 4.19.125-fslc+gd839dc0169b3.. But the performance is as expected around 390 Mbps on 4.9.124.&lt;/P&gt;&lt;P&gt;on Linux 4.9.124&lt;/P&gt;&lt;P&gt;root@tcs-imx6:~# iperf3 -c 10.42.0.1&lt;BR /&gt;Connecting to host 10.42.0.1, port 5201&lt;BR /&gt;[ 5] local 10.42.0.137 port 44278 connected to 10.42.0.1 port 5201&lt;BR /&gt;[ ID] Interval Transfer Bitrate Retr Cwnd&lt;BR /&gt;[ 5] 0.00-1.00 sec 46.8 MBytes 392 Mbits/sec 0 327 KBytes&lt;BR /&gt;[ 5] 1.00-2.00 sec 45.7 MBytes 383 Mbits/sec 0 355 KBytes&lt;BR /&gt;[ 5] 2.00-3.00 sec 46.4 MBytes 388 Mbits/sec 0 355 KBytes&lt;BR /&gt;[ 5] 3.00-4.00 sec 45.2 MBytes 381 Mbits/sec 0 379 KBytes&lt;BR /&gt;[ 5] 4.00-5.00 sec 45.8 MBytes 384 Mbits/sec 0 379 KBytes&lt;BR /&gt;[ 5] 5.00-6.01 sec 43.4 MBytes 362 Mbits/sec 0 416 KBytes&lt;BR /&gt;[ 5] 6.01-7.01 sec 46.0 MBytes 386 Mbits/sec 0 440 KBytes&lt;BR /&gt;[ 5] 7.01-8.01 sec 46.7 MBytes 391 Mbits/sec 0 440 KBytes&lt;BR /&gt;[ 5] 8.01-9.02 sec 46.4 MBytes 386 Mbits/sec 0 440 KBytes&lt;BR /&gt;[ 5] 9.02-10.01 sec 45.6 MBytes 386 Mbits/sec 0 440 KBytes&lt;BR /&gt;- - - - - - - - - - - - - - - - - - - - - - - - -&lt;BR /&gt;[ ID] Interval Transfer Bitrate Retr&lt;BR /&gt;[ 5] 0.00-10.01 sec 458 MBytes 384 Mbits/sec 0 sender&lt;BR /&gt;[ 5] 0.00-10.01 sec 457 MBytes 383 Mbits/sec receiver&lt;/P&gt;&lt;P&gt;On Linux 4.19&lt;/P&gt;&lt;P&gt;root@tcs-imx6:~# iperf3 -c 10.42.0.1&lt;BR /&gt;Connecting to host 10.42.0.1, port 5201&lt;BR /&gt;[ 5] local 10.42.0.228 port 44486 connected to 10.42.0.1 port 5201&lt;BR /&gt;[ ID] Interval Transfer Bitrate Retr Cwnd&lt;BR /&gt;[ 5] 0.00-1.00 sec 35.9 MBytes 301 Mbits/sec 0 260 KBytes&lt;BR /&gt;[ 5] 1.00-2.00 sec 37.3 MBytes 312 Mbits/sec 0 272 KBytes&lt;BR /&gt;[ 5] 2.00-3.00 sec 37.1 MBytes 313 Mbits/sec 0 310 KBytes&lt;BR /&gt;[ 5] 3.00-4.00 sec 35.4 MBytes 296 Mbits/sec 0 359 KBytes&lt;BR /&gt;[ 5] 4.00-5.00 sec 38.0 MBytes 319 Mbits/sec 0 373 KBytes&lt;BR /&gt;[ 5] 5.00-6.00 sec 38.8 MBytes 325 Mbits/sec 0 393 KBytes&lt;BR /&gt;[ 5] 6.00-7.00 sec 38.5 MBytes 323 Mbits/sec 0 393 KBytes&lt;BR /&gt;[ 5] 7.00-8.00 sec 41.0 MBytes 344 Mbits/sec 0 393 KBytes&lt;BR /&gt;[ 5] 8.00-9.00 sec 47.2 MBytes 396 Mbits/sec 0 393 KBytes&lt;BR /&gt;[ 5] 9.00-10.00 sec 46.7 MBytes 392 Mbits/sec 0 393 KBytes&lt;BR /&gt;- - - - - - - - - - - - - - - - - - - - - - - - -&lt;BR /&gt;[ ID] Interval Transfer Bitrate Retr&lt;BR /&gt;[ 5] 0.00-10.00 sec 396 MBytes 332 Mbits/sec 0 sender&lt;BR /&gt;[ 5] 0.00-10.00 sec 395 MBytes 332 Mbits/sec receiver&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 23 Jun 2021 02:51:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Fast-ethernet-Performance-issue-on-IMX6-based-hardware/m-p/1296457#M175886</guid>
      <dc:creator>suryakanta_moha</dc:creator>
      <dc:date>2021-06-23T02:51:36Z</dc:date>
    </item>
    <item>
      <title>Re: Fast ethernet Performance issue on IMX6  based hardware</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Fast-ethernet-Performance-issue-on-IMX6-based-hardware/m-p/1296813#M175922</link>
      <description>&lt;P&gt;Most likely, this is the software driver issue in the 4.19.125 BSP. Will report &lt;BR /&gt;it to R&amp;amp;D. Also, please try the latest 5.10.9 BSP:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX" target="_blank"&gt;https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Artur&lt;/P&gt;</description>
      <pubDate>Wed, 23 Jun 2021 10:38:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Fast-ethernet-Performance-issue-on-IMX6-based-hardware/m-p/1296813#M175922</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2021-06-23T10:38:22Z</dc:date>
    </item>
  </channel>
</rss>