<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic DRAM Trim Controls in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/DRAM-Trim-Controls/m-p/1295704#M175815</link>
    <description>&lt;P&gt;&lt;SPAN class="fontstyle0"&gt;Hello,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="fontstyle0"&gt;Document Number: IMX6DQRM,&amp;nbsp;Rev. 5, 06/2018.&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;In section 44.11.9, it talks about a 2-bit control field to add a fixed delay to SDCLK or SDQS signals.&amp;nbsp; Is it true?&amp;nbsp; I could not find any information on the reference manual.&amp;nbsp; The referenced registers do not contain such control field.&amp;nbsp; The corresponding bit fields in IOMUXC_SW_PAD_CTL_PAD_DRAM_ADDR00&lt;SPAN class="fontstyle0"&gt;&amp;nbsp;(IOMUX_SW_PAD_CTL_PAD_ADDR00) are for something else.&amp;nbsp; Does that feature exist to a fixed delay to SDCLK?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="fontstyle0"&gt;Thanks,&lt;BR /&gt;Rob&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 22 Jun 2021 01:31:38 GMT</pubDate>
    <dc:creator>RobertC</dc:creator>
    <dc:date>2021-06-22T01:31:38Z</dc:date>
    <item>
      <title>DRAM Trim Controls</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DRAM-Trim-Controls/m-p/1295704#M175815</link>
      <description>&lt;P&gt;&lt;SPAN class="fontstyle0"&gt;Hello,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="fontstyle0"&gt;Document Number: IMX6DQRM,&amp;nbsp;Rev. 5, 06/2018.&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;In section 44.11.9, it talks about a 2-bit control field to add a fixed delay to SDCLK or SDQS signals.&amp;nbsp; Is it true?&amp;nbsp; I could not find any information on the reference manual.&amp;nbsp; The referenced registers do not contain such control field.&amp;nbsp; The corresponding bit fields in IOMUXC_SW_PAD_CTL_PAD_DRAM_ADDR00&lt;SPAN class="fontstyle0"&gt;&amp;nbsp;(IOMUX_SW_PAD_CTL_PAD_ADDR00) are for something else.&amp;nbsp; Does that feature exist to a fixed delay to SDCLK?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="fontstyle0"&gt;Thanks,&lt;BR /&gt;Rob&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 22 Jun 2021 01:31:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DRAM-Trim-Controls/m-p/1295704#M175815</guid>
      <dc:creator>RobertC</dc:creator>
      <dc:date>2021-06-22T01:31:38Z</dc:date>
    </item>
    <item>
      <title>Re: DRAM Trim Controls</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DRAM-Trim-Controls/m-p/1295816#M175822</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/187826"&gt;@RobertC&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp; according to section 8 (External memory) of i.MX 6Dual/6Quad and i.MX 6DualPlus/6QuadPlus&amp;nbsp; Comparison the trim control was introduced for i.MX 6DualPlus/6QuadPlus &lt;BR /&gt;(i.MX 6Dual/6Quad&amp;nbsp; does not support such feature):&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;&lt;EM&gt;&amp;nbsp; The i.MX 6DualPlus/6QuadPlus will have the same external Memory as i.MX 6Dual/6Quad.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Although the DRAM controller and frequency will remain the same, the overall DRAM utilization is&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;significantly improved, due to the improvements in the bus fabric and graphics IP.&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;&amp;nbsp;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; The DRAM controller has also been enhanced with additional trim controls for the SDCLKx and SDQSx&amp;nbsp; signals.&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; This updated fine tuning control has been copied from the i. MX 6SoloX family of processors, where it&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;has been successfully verified on actual products.&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Yuri.&lt;/P&gt;</description>
      <pubDate>Tue, 22 Jun 2021 05:32:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DRAM-Trim-Controls/m-p/1295816#M175822</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2021-06-22T05:32:44Z</dc:date>
    </item>
  </channel>
</rss>