<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: iMX8QXP - RPMsg BSP  - Dynamic channel creation</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QXP-RPMsg-BSP-Dynamic-channel-creation/m-p/1295678#M175810</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Yes that is correct, as per kernel documentation&amp;nbsp;&lt;A href="https://www.kernel.org/doc/Documentation/rpmsg.txt" target="_blank"&gt;https://www.kernel.org/doc/Documentation/rpmsg.txt&lt;/A&gt;&amp;nbsp;:&lt;/P&gt;
&lt;PRE&gt;The plan is also to add static creation of rpmsg channels via the virtio
config space, but it's not implemented yet.&lt;/PRE&gt;
&lt;P&gt;&amp;nbsp;So for now it only support dynamic allocation of the RPMsg channels.&lt;BR /&gt;&lt;BR /&gt;BR.&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
    <pubDate>Tue, 22 Jun 2021 00:16:06 GMT</pubDate>
    <dc:creator>AldoG</dc:creator>
    <dc:date>2021-06-22T00:16:06Z</dc:date>
    <item>
      <title>iMX8QXP - RPMsg BSP  - Dynamic channel creation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QXP-RPMsg-BSP-Dynamic-channel-creation/m-p/1290248#M175293</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Could you please confirm . &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Currently NXP RPMsg linux bsps &amp;nbsp;creation of rpmsg devices (i.e. channels) is completely dynamic: the remote processor announces the existence of a remote rpmsg service by sending a name service message from M4 to A35 Linux side for creating channel. No static channel creation is supported in current nxp bsp on linux side. could you please confirm.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Jithesh&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 09 Jun 2021 23:14:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QXP-RPMsg-BSP-Dynamic-channel-creation/m-p/1290248#M175293</guid>
      <dc:creator>jithesh77</dc:creator>
      <dc:date>2021-06-09T23:14:13Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8QXP - RPMsg BSP  - Dynamic channel creation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QXP-RPMsg-BSP-Dynamic-channel-creation/m-p/1295678#M175810</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Yes that is correct, as per kernel documentation&amp;nbsp;&lt;A href="https://www.kernel.org/doc/Documentation/rpmsg.txt" target="_blank"&gt;https://www.kernel.org/doc/Documentation/rpmsg.txt&lt;/A&gt;&amp;nbsp;:&lt;/P&gt;
&lt;PRE&gt;The plan is also to add static creation of rpmsg channels via the virtio
config space, but it's not implemented yet.&lt;/PRE&gt;
&lt;P&gt;&amp;nbsp;So for now it only support dynamic allocation of the RPMsg channels.&lt;BR /&gt;&lt;BR /&gt;BR.&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Tue, 22 Jun 2021 00:16:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QXP-RPMsg-BSP-Dynamic-channel-creation/m-p/1295678#M175810</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2021-06-22T00:16:06Z</dc:date>
    </item>
  </channel>
</rss>