<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic ERROR : HID(R):LIBUSB_ERROR_TIMEOUT in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/ERROR-HID-R-LIBUSB-ERROR-TIMEOUT/m-p/1294406#M175684</link>
    <description>&lt;DIV class="lia-message-body lia-component-message-view-widget-body lia-component-body-signature-highlight-escalation lia-component-message-view-widget-body-signature-highlight-escalation"&gt;&lt;DIV class="lia-message-body-content"&gt;&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;We are using a customized board based on IMX6UL evk NXP board. We are using the RAM D2516ECMDXGME-U&lt;/P&gt;&lt;P&gt;I have tested the callibration and stress tests. I filled the values from the callibration test in imximage.cfg.&lt;/P&gt;&lt;P&gt;I compiled the u-boot and i filled the values in board/freescale/mx6ul_14x14_evk/imximage.cfg&lt;/P&gt;&lt;P&gt;The following are the values from the files imximage.cfg&lt;/P&gt;&lt;P&gt;----------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;/*&lt;BR /&gt;* Copyright (C) 2015 Freescale Semiconductor, Inc.&lt;BR /&gt;* Copyright 2017 NXP&lt;BR /&gt;*&lt;BR /&gt;* SPDX-License-Identifier: GPL-2.0+&lt;BR /&gt;*&lt;BR /&gt;* Refer docs/README.imxmage for more details about how-to configure&lt;BR /&gt;* and create imximage boot image&lt;BR /&gt;*&lt;BR /&gt;* The syntax is taken as close as possible with the kwbimage&lt;BR /&gt;*/&lt;/P&gt;&lt;P&gt;#define __ASSEMBLY__&lt;BR /&gt;#include &amp;lt;config.h&amp;gt;&lt;/P&gt;&lt;P&gt;/* image version */&lt;/P&gt;&lt;P&gt;IMAGE_VERSION 2&lt;/P&gt;&lt;P&gt;/*&lt;BR /&gt;* Boot Device : one of&lt;BR /&gt;* spi/sd/nand/onenand, qspi/nor&lt;BR /&gt;*/&lt;/P&gt;&lt;P&gt;#ifdef CONFIG_QSPI_BOOT&lt;BR /&gt;BOOT_FROM qspi&lt;BR /&gt;#elif defined(CONFIG_NOR_BOOT)&lt;BR /&gt;BOOT_FROM nor&lt;BR /&gt;#else&lt;BR /&gt;BOOT_FROM sd&lt;BR /&gt;#endif&lt;/P&gt;&lt;P&gt;#ifdef CONFIG_USE_IMXIMG_PLUGIN&lt;BR /&gt;/*PLUGIN plugin-binary-file IRAM_FREE_START_ADDR*/&lt;BR /&gt;PLUGIN board/freescale/mx6ul_14x14_evk/plugin.bin 0x00907000&lt;BR /&gt;#else&lt;/P&gt;&lt;P&gt;#ifdef CONFIG_IMX_HAB&lt;BR /&gt;CSF CONFIG_CSF_SIZE&lt;BR /&gt;#endif&lt;/P&gt;&lt;P&gt;/*&lt;BR /&gt;* Device Configuration Data (DCD)&lt;BR /&gt;*&lt;BR /&gt;* Each entry must have the format:&lt;BR /&gt;* Addr-type Address Value&lt;BR /&gt;*&lt;BR /&gt;* where:&lt;BR /&gt;* Addr-type register length (1,2 or 4 bytes)&lt;BR /&gt;* Address absolute address of the register&lt;BR /&gt;* value value to be stored in the register&lt;BR /&gt;*/&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;/* DDR type MT41K256M16HA-125 which is EOL */&lt;/P&gt;&lt;P&gt;/* Enable all clocks */&lt;BR /&gt;DATA 4 0x020c4068 0xffffffff&lt;BR /&gt;DATA 4 0x020c406c 0xffffffff&lt;BR /&gt;DATA 4 0x020c4070 0xffffffff&lt;BR /&gt;DATA 4 0x020c4074 0xffffffff&lt;BR /&gt;DATA 4 0x020c4078 0xffffffff&lt;BR /&gt;DATA 4 0x020c407c 0xffffffff&lt;BR /&gt;DATA 4 0x020c4080 0xffffffff&lt;/P&gt;&lt;P&gt;DATA 4 0x020D8004 0x00000872&lt;BR /&gt;DATA 4 0x020D801C 0x01000041&lt;/P&gt;&lt;P&gt;#ifdef CONFIG_IMX_OPTEE&lt;BR /&gt;DATA 4 0x20e4024 0x00000001&lt;BR /&gt;CHECK_BITS_SET 4 0x20e4024 0x1&lt;BR /&gt;#endif&lt;/P&gt;&lt;P&gt;DATA 4 0x020E04B4 0x000C0000&lt;BR /&gt;DATA 4 0x020E04AC 0x00000000&lt;BR /&gt;DATA 4 0x020E027C 0x00000030&lt;BR /&gt;DATA 4 0x020E0250 0x00000030&lt;BR /&gt;DATA 4 0x020E024C 0x00000030&lt;BR /&gt;DATA 4 0x020E0490 0x00000030&lt;BR /&gt;DATA 4 0x020E0288 0x00000030&lt;BR /&gt;DATA 4 0x020E0270 0x00000000&lt;BR /&gt;DATA 4 0x020E0260 0x00000030&lt;BR /&gt;DATA 4 0x020E0264 0x00000030&lt;BR /&gt;DATA 4 0x020E04A0 0x00000030&lt;BR /&gt;DATA 4 0x020E0494 0x00020000&lt;BR /&gt;DATA 4 0x020E0280 0x00000030&lt;BR /&gt;DATA 4 0x020E0284 0x00000030&lt;BR /&gt;DATA 4 0x020E04B0 0x00020000&lt;BR /&gt;DATA 4 0x020E0498 0x00000030&lt;BR /&gt;DATA 4 0x020E04A4 0x00000030&lt;BR /&gt;DATA 4 0x020E0244 0x00000030&lt;BR /&gt;DATA 4 0x020E0248 0x00000030&lt;BR /&gt;DATA 4 0x021B001C 0x00008000&lt;BR /&gt;DATA 4 0x021B0800 0xA1390003&lt;BR /&gt;DATA 4 0x021B080C 0x00010000&lt;BR /&gt;DATA 4 0x021B083C 0x4168016C&lt;BR /&gt;DATA 4 0x021B0840 0x00000000&lt;BR /&gt;DATA 4 0x021B0848 0x40405052&lt;BR /&gt;DATA 4 0x021B0850 0x40404E44&lt;BR /&gt;DATA 4 0x021B081C 0x33333333&lt;BR /&gt;DATA 4 0x021B0820 0x33333333&lt;BR /&gt;DATA 4 0x021B082C 0xf3333333&lt;BR /&gt;DATA 4 0x021B0830 0xf3333333&lt;BR /&gt;DATA 4 0x021B08C0 0x00921012&lt;BR /&gt;DATA 4 0x021B08B8 0x00000800&lt;BR /&gt;DATA 4 0x021B0004 0x0002002D&lt;BR /&gt;DATA 4 0x021B0008 0x1B333030&lt;BR /&gt;DATA 4 0x021B000C 0x676B52F3&lt;BR /&gt;DATA 4 0x021B0010 0xB64D0B63&lt;BR /&gt;DATA 4 0x021B0014 0x01FF00DB&lt;BR /&gt;DATA 4 0x021B0018 0x00201740&lt;BR /&gt;DATA 4 0x021B002C 0x000026D2&lt;BR /&gt;DATA 4 0x021B0030 0x006B1023&lt;BR /&gt;DATA 4 0x021B0040 0x0000004F&lt;BR /&gt;DATA 4 0x021B0000 0x84180000&lt;BR /&gt;DATA 4 0x021B001C 0x02008032&lt;BR /&gt;DATA 4 0x021B001C 0x00008033&lt;BR /&gt;DATA 4 0x021B001C 0x00048031&lt;BR /&gt;DATA 4 0x021B001C 0x15208030&lt;BR /&gt;DATA 4 0x021B001C 0x04008040&lt;BR /&gt;DATA 4 0x021B0020 0x00000800&lt;BR /&gt;DATA 4 0x021B0818 0x00000227&lt;BR /&gt;DATA 4 0x021B0004 0x0002556D&lt;BR /&gt;DATA 4 0x021B0404 0x00011006&lt;BR /&gt;DATA 4 0x021B001C 0x00000000&lt;BR /&gt;#endif&lt;/P&gt;&lt;P&gt;------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But when i am trying the flash the image, i am getting the following error .&lt;/P&gt;&lt;P&gt;ERROR : HID(R):LIBUSB_ERROR_TIMEOUT&lt;/P&gt;&lt;P&gt;Thanks...........&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
    <pubDate>Fri, 18 Jun 2021 11:29:58 GMT</pubDate>
    <dc:creator>embedded_Dev</dc:creator>
    <dc:date>2021-06-18T11:29:58Z</dc:date>
    <item>
      <title>ERROR : HID(R):LIBUSB_ERROR_TIMEOUT</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ERROR-HID-R-LIBUSB-ERROR-TIMEOUT/m-p/1294406#M175684</link>
      <description>&lt;DIV class="lia-message-body lia-component-message-view-widget-body lia-component-body-signature-highlight-escalation lia-component-message-view-widget-body-signature-highlight-escalation"&gt;&lt;DIV class="lia-message-body-content"&gt;&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;We are using a customized board based on IMX6UL evk NXP board. We are using the RAM D2516ECMDXGME-U&lt;/P&gt;&lt;P&gt;I have tested the callibration and stress tests. I filled the values from the callibration test in imximage.cfg.&lt;/P&gt;&lt;P&gt;I compiled the u-boot and i filled the values in board/freescale/mx6ul_14x14_evk/imximage.cfg&lt;/P&gt;&lt;P&gt;The following are the values from the files imximage.cfg&lt;/P&gt;&lt;P&gt;----------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;/*&lt;BR /&gt;* Copyright (C) 2015 Freescale Semiconductor, Inc.&lt;BR /&gt;* Copyright 2017 NXP&lt;BR /&gt;*&lt;BR /&gt;* SPDX-License-Identifier: GPL-2.0+&lt;BR /&gt;*&lt;BR /&gt;* Refer docs/README.imxmage for more details about how-to configure&lt;BR /&gt;* and create imximage boot image&lt;BR /&gt;*&lt;BR /&gt;* The syntax is taken as close as possible with the kwbimage&lt;BR /&gt;*/&lt;/P&gt;&lt;P&gt;#define __ASSEMBLY__&lt;BR /&gt;#include &amp;lt;config.h&amp;gt;&lt;/P&gt;&lt;P&gt;/* image version */&lt;/P&gt;&lt;P&gt;IMAGE_VERSION 2&lt;/P&gt;&lt;P&gt;/*&lt;BR /&gt;* Boot Device : one of&lt;BR /&gt;* spi/sd/nand/onenand, qspi/nor&lt;BR /&gt;*/&lt;/P&gt;&lt;P&gt;#ifdef CONFIG_QSPI_BOOT&lt;BR /&gt;BOOT_FROM qspi&lt;BR /&gt;#elif defined(CONFIG_NOR_BOOT)&lt;BR /&gt;BOOT_FROM nor&lt;BR /&gt;#else&lt;BR /&gt;BOOT_FROM sd&lt;BR /&gt;#endif&lt;/P&gt;&lt;P&gt;#ifdef CONFIG_USE_IMXIMG_PLUGIN&lt;BR /&gt;/*PLUGIN plugin-binary-file IRAM_FREE_START_ADDR*/&lt;BR /&gt;PLUGIN board/freescale/mx6ul_14x14_evk/plugin.bin 0x00907000&lt;BR /&gt;#else&lt;/P&gt;&lt;P&gt;#ifdef CONFIG_IMX_HAB&lt;BR /&gt;CSF CONFIG_CSF_SIZE&lt;BR /&gt;#endif&lt;/P&gt;&lt;P&gt;/*&lt;BR /&gt;* Device Configuration Data (DCD)&lt;BR /&gt;*&lt;BR /&gt;* Each entry must have the format:&lt;BR /&gt;* Addr-type Address Value&lt;BR /&gt;*&lt;BR /&gt;* where:&lt;BR /&gt;* Addr-type register length (1,2 or 4 bytes)&lt;BR /&gt;* Address absolute address of the register&lt;BR /&gt;* value value to be stored in the register&lt;BR /&gt;*/&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;/* DDR type MT41K256M16HA-125 which is EOL */&lt;/P&gt;&lt;P&gt;/* Enable all clocks */&lt;BR /&gt;DATA 4 0x020c4068 0xffffffff&lt;BR /&gt;DATA 4 0x020c406c 0xffffffff&lt;BR /&gt;DATA 4 0x020c4070 0xffffffff&lt;BR /&gt;DATA 4 0x020c4074 0xffffffff&lt;BR /&gt;DATA 4 0x020c4078 0xffffffff&lt;BR /&gt;DATA 4 0x020c407c 0xffffffff&lt;BR /&gt;DATA 4 0x020c4080 0xffffffff&lt;/P&gt;&lt;P&gt;DATA 4 0x020D8004 0x00000872&lt;BR /&gt;DATA 4 0x020D801C 0x01000041&lt;/P&gt;&lt;P&gt;#ifdef CONFIG_IMX_OPTEE&lt;BR /&gt;DATA 4 0x20e4024 0x00000001&lt;BR /&gt;CHECK_BITS_SET 4 0x20e4024 0x1&lt;BR /&gt;#endif&lt;/P&gt;&lt;P&gt;DATA 4 0x020E04B4 0x000C0000&lt;BR /&gt;DATA 4 0x020E04AC 0x00000000&lt;BR /&gt;DATA 4 0x020E027C 0x00000030&lt;BR /&gt;DATA 4 0x020E0250 0x00000030&lt;BR /&gt;DATA 4 0x020E024C 0x00000030&lt;BR /&gt;DATA 4 0x020E0490 0x00000030&lt;BR /&gt;DATA 4 0x020E0288 0x00000030&lt;BR /&gt;DATA 4 0x020E0270 0x00000000&lt;BR /&gt;DATA 4 0x020E0260 0x00000030&lt;BR /&gt;DATA 4 0x020E0264 0x00000030&lt;BR /&gt;DATA 4 0x020E04A0 0x00000030&lt;BR /&gt;DATA 4 0x020E0494 0x00020000&lt;BR /&gt;DATA 4 0x020E0280 0x00000030&lt;BR /&gt;DATA 4 0x020E0284 0x00000030&lt;BR /&gt;DATA 4 0x020E04B0 0x00020000&lt;BR /&gt;DATA 4 0x020E0498 0x00000030&lt;BR /&gt;DATA 4 0x020E04A4 0x00000030&lt;BR /&gt;DATA 4 0x020E0244 0x00000030&lt;BR /&gt;DATA 4 0x020E0248 0x00000030&lt;BR /&gt;DATA 4 0x021B001C 0x00008000&lt;BR /&gt;DATA 4 0x021B0800 0xA1390003&lt;BR /&gt;DATA 4 0x021B080C 0x00010000&lt;BR /&gt;DATA 4 0x021B083C 0x4168016C&lt;BR /&gt;DATA 4 0x021B0840 0x00000000&lt;BR /&gt;DATA 4 0x021B0848 0x40405052&lt;BR /&gt;DATA 4 0x021B0850 0x40404E44&lt;BR /&gt;DATA 4 0x021B081C 0x33333333&lt;BR /&gt;DATA 4 0x021B0820 0x33333333&lt;BR /&gt;DATA 4 0x021B082C 0xf3333333&lt;BR /&gt;DATA 4 0x021B0830 0xf3333333&lt;BR /&gt;DATA 4 0x021B08C0 0x00921012&lt;BR /&gt;DATA 4 0x021B08B8 0x00000800&lt;BR /&gt;DATA 4 0x021B0004 0x0002002D&lt;BR /&gt;DATA 4 0x021B0008 0x1B333030&lt;BR /&gt;DATA 4 0x021B000C 0x676B52F3&lt;BR /&gt;DATA 4 0x021B0010 0xB64D0B63&lt;BR /&gt;DATA 4 0x021B0014 0x01FF00DB&lt;BR /&gt;DATA 4 0x021B0018 0x00201740&lt;BR /&gt;DATA 4 0x021B002C 0x000026D2&lt;BR /&gt;DATA 4 0x021B0030 0x006B1023&lt;BR /&gt;DATA 4 0x021B0040 0x0000004F&lt;BR /&gt;DATA 4 0x021B0000 0x84180000&lt;BR /&gt;DATA 4 0x021B001C 0x02008032&lt;BR /&gt;DATA 4 0x021B001C 0x00008033&lt;BR /&gt;DATA 4 0x021B001C 0x00048031&lt;BR /&gt;DATA 4 0x021B001C 0x15208030&lt;BR /&gt;DATA 4 0x021B001C 0x04008040&lt;BR /&gt;DATA 4 0x021B0020 0x00000800&lt;BR /&gt;DATA 4 0x021B0818 0x00000227&lt;BR /&gt;DATA 4 0x021B0004 0x0002556D&lt;BR /&gt;DATA 4 0x021B0404 0x00011006&lt;BR /&gt;DATA 4 0x021B001C 0x00000000&lt;BR /&gt;#endif&lt;/P&gt;&lt;P&gt;------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But when i am trying the flash the image, i am getting the following error .&lt;/P&gt;&lt;P&gt;ERROR : HID(R):LIBUSB_ERROR_TIMEOUT&lt;/P&gt;&lt;P&gt;Thanks...........&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Fri, 18 Jun 2021 11:29:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ERROR-HID-R-LIBUSB-ERROR-TIMEOUT/m-p/1294406#M175684</guid>
      <dc:creator>embedded_Dev</dc:creator>
      <dc:date>2021-06-18T11:29:58Z</dc:date>
    </item>
    <item>
      <title>Re: ERROR : HID(R):LIBUSB_ERROR_TIMEOUT</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ERROR-HID-R-LIBUSB-ERROR-TIMEOUT/m-p/1316395#M177728</link>
      <description>&lt;P&gt;Does it work now?&lt;/P&gt;</description>
      <pubDate>Mon, 02 Aug 2021 04:35:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ERROR-HID-R-LIBUSB-ERROR-TIMEOUT/m-p/1316395#M177728</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2021-08-02T04:35:42Z</dc:date>
    </item>
    <item>
      <title>Re: ERROR : HID(R):LIBUSB_ERROR_TIMEOUT</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ERROR-HID-R-LIBUSB-ERROR-TIMEOUT/m-p/1341902#M180266</link>
      <description>&lt;P&gt;Yeah it is working now&lt;/P&gt;</description>
      <pubDate>Fri, 17 Sep 2021 05:21:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ERROR-HID-R-LIBUSB-ERROR-TIMEOUT/m-p/1341902#M180266</guid>
      <dc:creator>embedded_Dev</dc:creator>
      <dc:date>2021-09-17T05:21:16Z</dc:date>
    </item>
  </channel>
</rss>