<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: iMX8 as a USB3.0 composite device in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8-as-a-USB3-0-composite-device/m-p/1292283#M175520</link>
    <description>&lt;P&gt;Is there any example that iMX8 as a UAC device?&lt;/P&gt;</description>
    <pubDate>Tue, 15 Jun 2021 05:20:08 GMT</pubDate>
    <dc:creator>mm2021</dc:creator>
    <dc:date>2021-06-15T05:20:08Z</dc:date>
    <item>
      <title>iMX8 as a USB3.0 composite device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8-as-a-USB3-0-composite-device/m-p/950967#M142187</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&amp;nbsp;&lt;/P&gt;&lt;P&gt;On an iMX8 that runs Linux (based on Yocto project),&lt;/P&gt;&lt;P&gt;Is it possible that the iMX8 will be recognized by a PC as a USB3.0 composite device (i.e. support both&amp;nbsp;UVC and&amp;nbsp;VSC&amp;nbsp;USB classes)?&lt;/P&gt;&lt;P&gt;Can you share with me some useful links\application notes of how this can be achieved from programming point of view?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Nissim&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Oct 2019 15:34:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8-as-a-USB3-0-composite-device/m-p/950967#M142187</guid>
      <dc:creator>nissim_beja</dc:creator>
      <dc:date>2019-10-22T15:34:18Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8 as a USB3.0 composite device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8-as-a-USB3-0-composite-device/m-p/950968#M142188</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nissim,&lt;/P&gt;&lt;P&gt;You could take a look to the following Community threads for reference information:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/508145"&gt;i.MX 6,7,8 support USB device mode support to UVC&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/514214"&gt;UVC gadget on imx8mevk&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also, on application note AN12103 is implemented a UVC, but based on a i.MX RT processor:&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12103.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN12103.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Oct 2019 23:59:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8-as-a-USB3-0-composite-device/m-p/950968#M142188</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2019-10-22T23:59:06Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8 as a USB3.0 composite device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8-as-a-USB3-0-composite-device/m-p/950969#M142189</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Carlos,&lt;/P&gt;&lt;P&gt;Thank you for your quick replay.&lt;/P&gt;&lt;P&gt;It seems that the links you sent&amp;nbsp;does not&amp;nbsp;provide a clear answer if there is a way to use the iMX8 as a USB 3.0 UVC device.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to point out that I am in the process of considering a solution for a new product based on&amp;nbsp;&lt;SPAN&gt;USB 3.0 UVC.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please advise,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Nissim&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Oct 2019 06:10:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8-as-a-USB3-0-composite-device/m-p/950969#M142189</guid>
      <dc:creator>nissim_beja</dc:creator>
      <dc:date>2019-10-23T06:10:19Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8 as a USB3.0 composite device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8-as-a-USB3-0-composite-device/m-p/950970#M142190</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nissim,&lt;BR /&gt;Summarizing, the UVC could be implemented on the i.MX8, but it is not supported by default on the Linux BSP as Device (the BSP supports UVC as Host); therefore, it would be required being implemented on your side. I’m afraid that there are not reference documents or step-by-step guide from NXP side, as it should be implemented using generic Gadget driver from Linux.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Are you in contact with any Sales or FAE to discuss about your opportunity?&lt;BR /&gt;Other option would be considering “Commercial Support and Engineering Services” scheme. You could refer to the following link for additional details:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/design/engineering-services:SW-SUPPORT" title="https://www.nxp.com/design/engineering-services:SW-SUPPORT"&gt;Commercial Support and Engineering Services | NXP&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Oct 2019 22:12:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8-as-a-USB3-0-composite-device/m-p/950970#M142190</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2019-10-24T22:12:33Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8 as a USB3.0 composite device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8-as-a-USB3-0-composite-device/m-p/950971#M142191</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Carlos,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for you replay.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I just started a discussion with ARROW about using the IMX8 for our project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Nissim.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 27 Oct 2019 05:43:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8-as-a-USB3-0-composite-device/m-p/950971#M142191</guid>
      <dc:creator>nissim_beja</dc:creator>
      <dc:date>2019-10-27T05:43:39Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8 as a USB3.0 composite device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8-as-a-USB3-0-composite-device/m-p/1292283#M175520</link>
      <description>&lt;P&gt;Is there any example that iMX8 as a UAC device?&lt;/P&gt;</description>
      <pubDate>Tue, 15 Jun 2021 05:20:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8-as-a-USB3-0-composite-device/m-p/1292283#M175520</guid>
      <dc:creator>mm2021</dc:creator>
      <dc:date>2021-06-15T05:20:08Z</dc:date>
    </item>
  </channel>
</rss>