<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MIPI CSI2 without I2C in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-CSI2-without-I2C/m-p/1291690#M175448</link>
    <description>&lt;P&gt;Hi Yannick&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;one can look at below thread with links to some examples&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/Parallel-video-on-IPU0-CSI-Input-without-I2C/td-p/1291372" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/Parallel-video-on-IPU0-CSI-Input-without-I2C/td-p/1291372&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
    <pubDate>Mon, 14 Jun 2021 00:26:00 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2021-06-14T00:26:00Z</dc:date>
    <item>
      <title>MIPI CSI2 without I2C</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-CSI2-without-I2C/m-p/1290484#M175319</link>
      <description>&lt;P&gt;Hi all,&amp;nbsp;&lt;/P&gt;&lt;P&gt;For a project I am connecting a camera with a Google Coral board (imx8 running Mendel). However, the camera does not run the MIPI protocol but a parallel protocol. Hence, there is a bridge which converts to MIPI. But this means that there is no way of communicating with the camera with I2C. So we will have to write a custom driver for it without the I2C. We are already looking at the v4l2 to do this.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Because we have zero experience doing this, we wonder if there are any examples which we can look into, and where they are.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance!!&lt;/P&gt;</description>
      <pubDate>Thu, 10 Jun 2021 06:49:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIPI-CSI2-without-I2C/m-p/1290484#M175319</guid>
      <dc:creator>DYD</dc:creator>
      <dc:date>2021-06-10T06:49:15Z</dc:date>
    </item>
    <item>
      <title>Re: MIPI CSI2 without I2C</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-CSI2-without-I2C/m-p/1291690#M175448</link>
      <description>&lt;P&gt;Hi Yannick&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;one can look at below thread with links to some examples&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/Parallel-video-on-IPU0-CSI-Input-without-I2C/td-p/1291372" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/Parallel-video-on-IPU0-CSI-Input-without-I2C/td-p/1291372&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Mon, 14 Jun 2021 00:26:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIPI-CSI2-without-I2C/m-p/1291690#M175448</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-06-14T00:26:00Z</dc:date>
    </item>
  </channel>
</rss>