<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic iMX8M Mini Use PI6CFGL201BZDIEX as PCIe REF_CLK in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-Use-PI6CFGL201BZDIEX-as-PCIe-REF-CLK/m-p/1290940#M175363</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Following reference design, we are making custom board with iMX8M Mini but replace the default PCIe clock generator (&lt;SPAN&gt;9FGV0241AKLF)&lt;/SPAN&gt; with&amp;nbsp;&lt;SPAN&gt;PI6CFGL201BZDIEX.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Also, a related post&amp;nbsp;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-CLK-Generator-Clocking-Issue/m-p/1258056" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-CLK-Generator-Clocking-Issue/m-p/1258056&lt;/A&gt;&amp;nbsp;indicates that&amp;nbsp;&lt;SPAN&gt;PI6CFGL201BZDIEX can be used.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;However,&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;when it is replaced with&amp;nbsp;PI6CFGL201BZDIEX, the driver (imx6q-pcie) will panic after reporting "PLL lock timeout". Then, kernel gets stuck and just hangs.&lt;/SPAN&gt;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;[ 2.677860] imx6q-pcie 33800000.pcie: EXT REF_CLK is used!.
[ 2.734722] imx6q-pcie 33800000.pcie: PCIe PLL lock timeout&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there any driver change needed for the driver&amp;nbsp;(drivers/pci/controller/dwc/pci-imx6.c )? Or, we need to change the DTS because of the replacement?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Weichen&lt;/P&gt;</description>
    <pubDate>Thu, 10 Jun 2021 22:18:26 GMT</pubDate>
    <dc:creator>Anonymous</dc:creator>
    <dc:date>2021-06-10T22:18:26Z</dc:date>
    <item>
      <title>iMX8M Mini Use PI6CFGL201BZDIEX as PCIe REF_CLK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-Use-PI6CFGL201BZDIEX-as-PCIe-REF-CLK/m-p/1290940#M175363</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Following reference design, we are making custom board with iMX8M Mini but replace the default PCIe clock generator (&lt;SPAN&gt;9FGV0241AKLF)&lt;/SPAN&gt; with&amp;nbsp;&lt;SPAN&gt;PI6CFGL201BZDIEX.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Also, a related post&amp;nbsp;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-CLK-Generator-Clocking-Issue/m-p/1258056" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-CLK-Generator-Clocking-Issue/m-p/1258056&lt;/A&gt;&amp;nbsp;indicates that&amp;nbsp;&lt;SPAN&gt;PI6CFGL201BZDIEX can be used.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;However,&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;when it is replaced with&amp;nbsp;PI6CFGL201BZDIEX, the driver (imx6q-pcie) will panic after reporting "PLL lock timeout". Then, kernel gets stuck and just hangs.&lt;/SPAN&gt;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;[ 2.677860] imx6q-pcie 33800000.pcie: EXT REF_CLK is used!.
[ 2.734722] imx6q-pcie 33800000.pcie: PCIe PLL lock timeout&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there any driver change needed for the driver&amp;nbsp;(drivers/pci/controller/dwc/pci-imx6.c )? Or, we need to change the DTS because of the replacement?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Weichen&lt;/P&gt;</description>
      <pubDate>Thu, 10 Jun 2021 22:18:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-Use-PI6CFGL201BZDIEX-as-PCIe-REF-CLK/m-p/1290940#M175363</guid>
      <dc:creator>Anonymous</dc:creator>
      <dc:date>2021-06-10T22:18:26Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8M Mini Use PI6CFGL201BZDIEX as PCIe REF_CLK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-Use-PI6CFGL201BZDIEX-as-PCIe-REF-CLK/m-p/1292232#M175514</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;these 2 clock generators are pin to pin compatible, but PIN7 and PIN5 are different definitions.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="weidong_sun_0-1623726174619.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/147059i3A6484764618BD6E/image-size/medium?v=v2&amp;amp;px=400" role="button" title="weidong_sun_0-1623726174619.png" alt="weidong_sun_0-1623726174619.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;weidong_sun_0-1623726174619.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;--The clock generator can output 2-channel 100MHz clocks, one channel is for CPU side, the other is for M.2 connector.&lt;/P&gt;
&lt;P&gt;--The clock generator doesn't need linux driver, default configuration is OK.&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;So now you can measure whether 100MHz clock OUPUT or not.&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;According to your description, obviously, CPU side doesn't get the clock input or bad clock waveform.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a nice day!&lt;/P&gt;
&lt;P&gt;B.R,&lt;/P&gt;
&lt;P&gt;weidong&lt;/P&gt;</description>
      <pubDate>Tue, 15 Jun 2021 03:28:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-Use-PI6CFGL201BZDIEX-as-PCIe-REF-CLK/m-p/1292232#M175514</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2021-06-15T03:28:33Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8M Mini Use PI6CFGL201BZDIEX as PCIe REF_CLK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-Use-PI6CFGL201BZDIEX-as-PCIe-REF-CLK/m-p/1293642#M175613</link>
      <description>&lt;P&gt;Hi&amp;nbsp;weidong_sun,&lt;/P&gt;&lt;P&gt;We tried to put the PCI module to M.2 and it worked. Like you mentioned, it seems that M.2 side of channel is working but the CPU-side doesn't. We are still investigating why it acts like this.&lt;/P&gt;</description>
      <pubDate>Thu, 17 Jun 2021 00:01:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-Use-PI6CFGL201BZDIEX-as-PCIe-REF-CLK/m-p/1293642#M175613</guid>
      <dc:creator>Anonymous</dc:creator>
      <dc:date>2021-06-17T00:01:12Z</dc:date>
    </item>
  </channel>
</rss>