<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Touch on IMX6SLLEVK + IMXEBOOKDC4</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Touch-on-IMX6SLLEVK-IMXEBOOKDC4/m-p/1290317#M175300</link>
    <description>&lt;P&gt;I have tried to adjust the DTD in&amp;nbsp;imx6sll-evk.dts:&lt;BR /&gt;&amp;amp;i2c3 {&lt;BR /&gt;...&lt;BR /&gt;elan@10 {&lt;BR /&gt;pinctrl-names = "default";&lt;BR /&gt;pinctrl-0 = &amp;lt;&amp;amp;pinctrl_epdc_elan_touch&amp;gt;;&lt;BR /&gt;compatible = "elan,elan-touch";&lt;BR /&gt;reg = &amp;lt;0x10&amp;gt;;&lt;BR /&gt;interrupt-parent = &amp;lt;&amp;amp;gpio4&amp;gt;;&lt;BR /&gt;interrupts = &amp;lt;19 IRQ_TYPE_EDGE_FALLING&amp;gt;;&lt;BR /&gt;gpio_elan_cs = &amp;lt;&amp;amp;gpio2 8 0&amp;gt;;&lt;BR /&gt;gpio_elan_rst = &amp;lt;&amp;amp;gpio4 20 0&amp;gt;;&lt;BR /&gt;gpio_intr = &amp;lt;&amp;amp;gpio4 19 0&amp;gt;;&lt;BR /&gt;status = "okay";&lt;BR /&gt;};&lt;BR /&gt;};&lt;BR /&gt;pinctrl_epdc_elan_touch: epdc_elan_touch_grp {&lt;BR /&gt;fsl,pins = &amp;lt;&lt;BR /&gt;MX6SLL_PAD_GPIO4_IO19__GPIO4_IO19 0x17059&lt;BR /&gt;MX6SLL_PAD_GPIO4_IO20__GPIO4_IO20 0x17059&lt;BR /&gt;MX6SLL_PAD_EPDC_PWR_CTRL1__GPIO2_IO009 0x17059&lt;BR /&gt;&amp;gt;;&lt;BR /&gt;};&lt;BR /&gt;After doing this, I get an error:&lt;BR /&gt;root@imx6sllevk:~# dmesg | grep -i elan&lt;BR /&gt;[ 1.989701] elan-touch 2-0010: elan - Read Hello Packet Failed&lt;/P&gt;</description>
    <pubDate>Tue, 15 Jun 2021 01:45:31 GMT</pubDate>
    <dc:creator>ekerebel</dc:creator>
    <dc:date>2021-06-15T01:45:31Z</dc:date>
    <item>
      <title>Touch on IMX6SLLEVK + IMXEBOOKDC4</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Touch-on-IMX6SLLEVK-IMXEBOOKDC4/m-p/1289495#M175223</link>
      <description>&lt;P&gt;I am trying to test TOUCH on the combo&amp;nbsp;IMX6SLLEVK + IMXEBOOKDC4.&lt;/P&gt;&lt;P&gt;I have tried&amp;nbsp;loading the full image: LF_v5.10_1.0.0_images_IMX6SLLEVK&amp;gt;imx-image-full-imx6sllevk.wic&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &lt;EM&gt;cat /proc/bus/input/devices&lt;/EM&gt; does not detect the i2c for the touch device&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;It looks like ELAN is enabled in the config:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;EM&gt; root@imx6sllevk:~# zcat /proc/config.gz | grep -i ELAN_TS &lt;/EM&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp; CONFIG_TOUCHSCREEN_ELAN_TS=y&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;EM&gt;dmesg | grep -i elan&lt;/EM&gt;&amp;nbsp; does not return anything&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I also tried building an image via Yocto but not sure what to add to the dts to configure ELAN.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Can anyone help?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 09 Jun 2021 02:01:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Touch-on-IMX6SLLEVK-IMXEBOOKDC4/m-p/1289495#M175223</guid>
      <dc:creator>ekerebel</dc:creator>
      <dc:date>2021-06-09T02:01:43Z</dc:date>
    </item>
    <item>
      <title>Re: Touch on IMX6SLLEVK + IMXEBOOKDC4</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Touch-on-IMX6SLLEVK-IMXEBOOKDC4/m-p/1290317#M175300</link>
      <description>&lt;P&gt;I have tried to adjust the DTD in&amp;nbsp;imx6sll-evk.dts:&lt;BR /&gt;&amp;amp;i2c3 {&lt;BR /&gt;...&lt;BR /&gt;elan@10 {&lt;BR /&gt;pinctrl-names = "default";&lt;BR /&gt;pinctrl-0 = &amp;lt;&amp;amp;pinctrl_epdc_elan_touch&amp;gt;;&lt;BR /&gt;compatible = "elan,elan-touch";&lt;BR /&gt;reg = &amp;lt;0x10&amp;gt;;&lt;BR /&gt;interrupt-parent = &amp;lt;&amp;amp;gpio4&amp;gt;;&lt;BR /&gt;interrupts = &amp;lt;19 IRQ_TYPE_EDGE_FALLING&amp;gt;;&lt;BR /&gt;gpio_elan_cs = &amp;lt;&amp;amp;gpio2 8 0&amp;gt;;&lt;BR /&gt;gpio_elan_rst = &amp;lt;&amp;amp;gpio4 20 0&amp;gt;;&lt;BR /&gt;gpio_intr = &amp;lt;&amp;amp;gpio4 19 0&amp;gt;;&lt;BR /&gt;status = "okay";&lt;BR /&gt;};&lt;BR /&gt;};&lt;BR /&gt;pinctrl_epdc_elan_touch: epdc_elan_touch_grp {&lt;BR /&gt;fsl,pins = &amp;lt;&lt;BR /&gt;MX6SLL_PAD_GPIO4_IO19__GPIO4_IO19 0x17059&lt;BR /&gt;MX6SLL_PAD_GPIO4_IO20__GPIO4_IO20 0x17059&lt;BR /&gt;MX6SLL_PAD_EPDC_PWR_CTRL1__GPIO2_IO009 0x17059&lt;BR /&gt;&amp;gt;;&lt;BR /&gt;};&lt;BR /&gt;After doing this, I get an error:&lt;BR /&gt;root@imx6sllevk:~# dmesg | grep -i elan&lt;BR /&gt;[ 1.989701] elan-touch 2-0010: elan - Read Hello Packet Failed&lt;/P&gt;</description>
      <pubDate>Tue, 15 Jun 2021 01:45:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Touch-on-IMX6SLLEVK-IMXEBOOKDC4/m-p/1290317#M175300</guid>
      <dc:creator>ekerebel</dc:creator>
      <dc:date>2021-06-15T01:45:31Z</dc:date>
    </item>
    <item>
      <title>Re: Touch on IMX6SLLEVK + IMXEBOOKDC4</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Touch-on-IMX6SLLEVK-IMXEBOOKDC4/m-p/1298717#M176087</link>
      <description>&lt;P&gt;OK, I managed to solve this, the address was 0x15, not 0x10&lt;/P&gt;&lt;P&gt;Also i2c1, not i2c3&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 27 Jun 2021 23:30:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Touch-on-IMX6SLLEVK-IMXEBOOKDC4/m-p/1298717#M176087</guid>
      <dc:creator>ekerebel</dc:creator>
      <dc:date>2021-06-27T23:30:19Z</dc:date>
    </item>
  </channel>
</rss>