<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Flash wic image with UUU on Linux in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Flash-wic-image-with-UUU-on-Linux/m-p/1290179#M175286</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;
&lt;P&gt;Could you try by decompressing the .bz2 file?&lt;/P&gt;
&lt;P&gt;It may be using too much memory like in the scenario below:&lt;BR /&gt;&lt;A href="https://github.com/NXPmicro/mfgtools/issues/179" target="_blank"&gt;https://github.com/NXPmicro/mfgtools/issues/179&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Also, I think this may be a tool related issue, I would suggest to post it in the github as well.&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
    <pubDate>Wed, 09 Jun 2021 19:10:23 GMT</pubDate>
    <dc:creator>AldoG</dc:creator>
    <dc:date>2021-06-09T19:10:23Z</dc:date>
    <item>
      <title>Flash wic image with UUU on Linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Flash-wic-image-with-UUU-on-Linux/m-p/1289101#M175180</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am working on an IMX8M Mini, and I recently started to used fully partionned .wic.bz2 image instead of sdcard.bz2.&lt;/P&gt;&lt;P&gt;Flashing my emmc with uuu is not functional on my Linux laptop (Ubuntu 18.04 - 64bit) with .wic.bz2 image. This is working fine with a Windows laptop so I know my .wic.bz2 is correctly built. I had no trouble to flash on my Linux when I used .sdcard.bz2 image.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;uuu command used is:&amp;nbsp;&lt;EM&gt;sudo ${UUU_DIR}/uuu -v -b emmc_all \&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;${BIN_DIR}imx-boot-smarthub-hw-sd.bin-flash_evk \&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;${BIN_DIR}winegard-smarthub-smarthub-hw.wic.bz2&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Here is the output of uuu:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Wait for Known USB Device Appear...&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;New USB Device Attached at 1:91&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;1:91&amp;gt;Start Cmd:FB: ucmd setenv fastboot_dev mmc&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;1:91&amp;gt;Okay (0.012s)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;1:91&amp;gt;Start Cmd:FB: ucmd setenv mmcdev ${emmc_dev}&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;1:91&amp;gt;Okay (0s)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;1:91&amp;gt;Start Cmd:FB: ucmd mmc dev ${emmc_dev}&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;1:91&amp;gt;Okay (0.097s)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;1:91&amp;gt;Start Cmd:FB: flash -raw2sparse all /mnt/dev/1_Projects/SMARTHUB/bin/winegard-smarthub-smarthub-hw.wic.bz2/*&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;16775680terminate called without an active exception&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Aborted&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Version used is:&amp;nbsp;libuuu_1.4.138-0-g051a8fe,&amp;nbsp;uuu_version 1.2.39&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Below the output of U-Boot if it helps:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;u-boot=&amp;gt; fastboot USB0&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;switch to partitions #0, OK&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;mmc1(part 0) is current device&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Starting download of 16776232 bytes&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;..........................................................................&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;.....................................................&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;downloading of 16776232 bytes finished&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;writing to partition 'all'&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;sparse flash target is mmc:1&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;writing to partition 'all' for sparse, buffer size 16776232&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Flashing sparse image at offset 0&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Flashing Sparse Image&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;........ wrote 16776192 bytes to 'all'&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Starting download of 16776244 bytes&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;..........................................................................&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;.....................................................&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;downloading of 16776244 bytes finished&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;writing to partition 'all'&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;sparse flash target is mmc:1&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;writing to partition 'all' for sparse, buffer size 16776244&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Flashing sparse image at offset 0&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Flashing Sparse Image&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;........ wrote 16776192 bytes to 'all'&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does anyone know if there is some restrictions on Linux side with the uuu tool ? Are they any patch to fix it ?&lt;/P&gt;&lt;P&gt;Thanks for your help&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 08 Jun 2021 12:03:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Flash-wic-image-with-UUU-on-Linux/m-p/1289101#M175180</guid>
      <dc:creator>ebecam_</dc:creator>
      <dc:date>2021-06-08T12:03:06Z</dc:date>
    </item>
    <item>
      <title>Re: Flash wic image with UUU on Linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Flash-wic-image-with-UUU-on-Linux/m-p/1290179#M175286</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;
&lt;P&gt;Could you try by decompressing the .bz2 file?&lt;/P&gt;
&lt;P&gt;It may be using too much memory like in the scenario below:&lt;BR /&gt;&lt;A href="https://github.com/NXPmicro/mfgtools/issues/179" target="_blank"&gt;https://github.com/NXPmicro/mfgtools/issues/179&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Also, I think this may be a tool related issue, I would suggest to post it in the github as well.&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Wed, 09 Jun 2021 19:10:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Flash-wic-image-with-UUU-on-Linux/m-p/1290179#M175286</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2021-06-09T19:10:23Z</dc:date>
    </item>
    <item>
      <title>Re: Flash wic image with UUU on Linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Flash-wic-image-with-UUU-on-Linux/m-p/1290653#M175340</link>
      <description>&lt;P&gt;Hi Aldo,&lt;/P&gt;&lt;P&gt;Thanks for your reply, using the uncompressed image solved my issue. I have another question on my mind. My .wic image is a 15G image and takes around 20min to flash with UUU.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Do you know if this can be speed up ? Out of the 15G, only a small part really contains data, most of image is 0 bytes, so is there a way to bypass those ?&lt;/P&gt;&lt;P&gt;Thanks for your help,&lt;/P&gt;&lt;P&gt;Elise&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 10 Jun 2021 10:05:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Flash-wic-image-with-UUU-on-Linux/m-p/1290653#M175340</guid>
      <dc:creator>ebecam_</dc:creator>
      <dc:date>2021-06-10T10:05:22Z</dc:date>
    </item>
    <item>
      <title>Re: Flash wic image with UUU on Linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Flash-wic-image-with-UUU-on-Linux/m-p/1295626#M175807</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;Well actually this is more of a yocto thing, if you want to reduce the size of the .wic image you may check the following:&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/Yocto-WIC-image-creator-with-fixed-partition-sizes/m-p/500088" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/Yocto-WIC-image-creator-with-fixed-partition-sizes/m-p/500088&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;I don't know if it may be possible for the tool to bypass partitions since it will copy the whole .wic image, some customers have removed messages from UART port to speed up a bit the flash process.&lt;BR /&gt;&lt;BR /&gt;BR,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Mon, 21 Jun 2021 19:52:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Flash-wic-image-with-UUU-on-Linux/m-p/1295626#M175807</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2021-06-21T19:52:06Z</dc:date>
    </item>
  </channel>
</rss>