<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: i.MX6ULL UART(RTS CTS)</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6ULL-UART-RTS-CTS/m-p/1289594#M175236</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;Both can be set with the tool.&lt;BR /&gt;Do the RTS and CTS listed in the tool mean DCE / DTE = 0?&lt;/P&gt;&lt;P&gt;best regard&lt;/P&gt;</description>
    <pubDate>Wed, 09 Jun 2021 05:06:06 GMT</pubDate>
    <dc:creator>ban45</dc:creator>
    <dc:date>2021-06-09T05:06:06Z</dc:date>
    <item>
      <title>i.MX6ULL UART(RTS CTS)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6ULL-UART-RTS-CTS/m-p/1289510#M175227</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I swapped only CTS and RTS using the CnfigTools for i.MX Version 9.0, but no error or warning. (TX, RX are unchanged)&lt;BR /&gt;Which register should be changed to switch the functions in use? Is it possible to replace CTS and RTS without changing TX and RX?&lt;/P&gt;&lt;P&gt;best regard&lt;/P&gt;</description>
      <pubDate>Wed, 09 Jun 2021 02:25:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6ULL-UART-RTS-CTS/m-p/1289510#M175227</guid>
      <dc:creator>ban45</dc:creator>
      <dc:date>2021-06-09T02:25:12Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6ULL UART(RTS CTS)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6ULL-UART-RTS-CTS/m-p/1289575#M175232</link>
      <description>&lt;P&gt;Hi Yasunori&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;gt;Is it possible to replace CTS and RTS without changing TX and RX?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;sorry this is not possible. For details one can look at Figure 55-2. UART external signals&lt;/P&gt;
&lt;P&gt;to module signals routing with respect to DCE/DTE mode&lt;/P&gt;
&lt;P&gt;&lt;A id="relatedDocsClick_1" href="https://www.nxp.com/webapp/Download?colCode=IMX6ULLRM" target="_blank" rel="noopener"&gt;&lt;STRONG&gt;i.MX 6ULL Applications Processor Reference Manual&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Wed, 09 Jun 2021 04:30:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6ULL-UART-RTS-CTS/m-p/1289575#M175232</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-06-09T04:30:58Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6ULL UART(RTS CTS)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6ULL-UART-RTS-CTS/m-p/1289594#M175236</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;Both can be set with the tool.&lt;BR /&gt;Do the RTS and CTS listed in the tool mean DCE / DTE = 0?&lt;/P&gt;&lt;P&gt;best regard&lt;/P&gt;</description>
      <pubDate>Wed, 09 Jun 2021 05:06:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6ULL-UART-RTS-CTS/m-p/1289594#M175236</guid>
      <dc:creator>ban45</dc:creator>
      <dc:date>2021-06-09T05:06:06Z</dc:date>
    </item>
  </channel>
</rss>