<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Add v4l2loopback.ko to yocto imx8 yocto image</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Add-v4l2loopback-ko-to-yocto-imx8-yocto-image/m-p/1289584#M175235</link>
    <description>&lt;P&gt;how do you build it? could you find the v4l2loopback when you use the command like "bitbake -c menuconfig linux-imx" ? if yes, try to enable it in the menuconfig list&lt;/P&gt;</description>
    <pubDate>Wed, 09 Jun 2021 04:44:45 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2021-06-09T04:44:45Z</dc:date>
    <item>
      <title>Add v4l2loopback.ko to yocto imx8 yocto image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Add-v4l2loopback-ko-to-yocto-imx8-yocto-image/m-p/1287622#M175060</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have built the v4l2looback.ko (source:&lt;A href="https://github.com/umlaeute/v4l2loopback" target="_blank" rel="nofollow noopener"&gt;https://github.com/umlaeute/v4l2loopback&lt;/A&gt;) on the imx8 target. My goal is to add it to the yocto image. Has anybody done this? Create a kernel module recipe for v4l2loopback and include it in the yocto building?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Lijun&lt;/P&gt;</description>
      <pubDate>Fri, 04 Jun 2021 14:55:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Add-v4l2loopback-ko-to-yocto-imx8-yocto-image/m-p/1287622#M175060</guid>
      <dc:creator>lchen</dc:creator>
      <dc:date>2021-06-04T14:55:38Z</dc:date>
    </item>
    <item>
      <title>Re: Add v4l2loopback.ko to yocto imx8 yocto image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Add-v4l2loopback-ko-to-yocto-imx8-yocto-image/m-p/1289584#M175235</link>
      <description>&lt;P&gt;how do you build it? could you find the v4l2loopback when you use the command like "bitbake -c menuconfig linux-imx" ? if yes, try to enable it in the menuconfig list&lt;/P&gt;</description>
      <pubDate>Wed, 09 Jun 2021 04:44:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Add-v4l2loopback-ko-to-yocto-imx8-yocto-image/m-p/1289584#M175235</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2021-06-09T04:44:45Z</dc:date>
    </item>
  </channel>
</rss>