<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックGPIOCHIP5 in imx8mm</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/GPIOCHIP5-in-imx8mm/m-p/1289442#M175219</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I hope you are doing well. I'm working on a project based on imx8mm evk board. Here is complete part number : MIMX8MM6DVTLZAA.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For past few months I was working on 2018 nxp b.v 8MMINILPD4-CPU but our company recently get new 2020 nxp B.V&amp;nbsp;8MMINILPD4-CPU2. When I flash my Linux into these new board. I can not see GPIOCHIP5 anymore. I can only see GPIOCHIP0-4, on the other hand in last board there were GPIOCHIP0-5 available. I'm using same Linux version what I used in previous board. Even if I flash Linux on old boards I can see&amp;nbsp;GPIOCHIP0-5. Is there anything I'm missing? I'm kind a new to Linux as well as NXP.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Is there any difference in the hardware or do I need to do something different with this board. Also, please direct my towards any document that have a map between GPIOCHIP and actual GPIO.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;</description>
    <pubDate>Tue, 08 Jun 2021 22:29:31 GMT</pubDate>
    <dc:creator>hsiddiquee</dc:creator>
    <dc:date>2021-06-08T22:29:31Z</dc:date>
    <item>
      <title>GPIOCHIP5 in imx8mm</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GPIOCHIP5-in-imx8mm/m-p/1289442#M175219</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I hope you are doing well. I'm working on a project based on imx8mm evk board. Here is complete part number : MIMX8MM6DVTLZAA.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For past few months I was working on 2018 nxp b.v 8MMINILPD4-CPU but our company recently get new 2020 nxp B.V&amp;nbsp;8MMINILPD4-CPU2. When I flash my Linux into these new board. I can not see GPIOCHIP5 anymore. I can only see GPIOCHIP0-4, on the other hand in last board there were GPIOCHIP0-5 available. I'm using same Linux version what I used in previous board. Even if I flash Linux on old boards I can see&amp;nbsp;GPIOCHIP0-5. Is there anything I'm missing? I'm kind a new to Linux as well as NXP.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Is there any difference in the hardware or do I need to do something different with this board. Also, please direct my towards any document that have a map between GPIOCHIP and actual GPIO.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;</description>
      <pubDate>Tue, 08 Jun 2021 22:29:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GPIOCHIP5-in-imx8mm/m-p/1289442#M175219</guid>
      <dc:creator>hsiddiquee</dc:creator>
      <dc:date>2021-06-08T22:29:31Z</dc:date>
    </item>
    <item>
      <title>Re: GPIOCHIP5 in imx8mm</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GPIOCHIP5-in-imx8mm/m-p/1291905#M175489</link>
      <description>&lt;P&gt;Hey Guys,&lt;/P&gt;&lt;P&gt;Does anyone found anything related. I have attached the log from old and new NXP imx8mm and the device files.&lt;/P&gt;</description>
      <pubDate>Mon, 14 Jun 2021 12:08:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GPIOCHIP5-in-imx8mm/m-p/1291905#M175489</guid>
      <dc:creator>hsiddiquee</dc:creator>
      <dc:date>2021-06-14T12:08:36Z</dc:date>
    </item>
    <item>
      <title>Re: GPIOCHIP5 in imx8mm</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GPIOCHIP5-in-imx8mm/m-p/1294936#M175724</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;8MMINILPD4-CPU2 have the following differences from the 8MMINILPD4-CPU:&lt;/P&gt;
&lt;P&gt;1. Change 16GB to 32GB eMMC, due to Android10 density requirement. &lt;BR /&gt;2. Change Wi-FI chip Murata LBEE5KL1PJ to Azurewave AW-CM358SM. &lt;BR /&gt;3. Change PMIC ROHM BD71847A to NXP PCA9450A. &lt;BR /&gt;4. Add J8 for alternative M.2 WiFi/BT module on Base Board&lt;/P&gt;
&lt;P&gt;You may refer to the CPU card schematic for this information:&lt;BR /&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=8MMINILPD4-CPU2-DESIGNFILES" target="_blank"&gt;https://www.nxp.com/webapp/Download?colCode=8MMINILPD4-CPU2-DESIGNFILES&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;If possible could you try with latest Linux release(L5.4.70_2.3.0)?&lt;BR /&gt;This because in this version CPU2 card is fully supported.&lt;BR /&gt;&lt;BR /&gt;For more information about GPIOCHIP you may take a look to the kernel documentation:&lt;BR /&gt;&lt;A href="https://www.kernel.org/doc/html/latest/driver-api/gpio/board.html#device-tree" target="_blank"&gt;https://www.kernel.org/doc/html/latest/driver-api/gpio/board.html#device-tree&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;This should be useful as well:&lt;BR /&gt;&lt;A href="https://variwiki.com/index.php?title=MX8M_GPIO" target="_blank"&gt;https://variwiki.com/index.php?title=MX8M_GPIO&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Sat, 19 Jun 2021 01:18:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GPIOCHIP5-in-imx8mm/m-p/1294936#M175724</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2021-06-19T01:18:33Z</dc:date>
    </item>
  </channel>
</rss>