<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 imx8: perl error while creating code coverage file using lcov on i.MX8MQ with googletest framework</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8-perl-error-while-creating-code-coverage-file-using-lcov-on/m-p/1286999#M174999</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Trying to create code coverage file after unit testing with googletest framework using lcov on i.MX8MQ target. But failing with some perl error. Here are the error logs:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;i&lt;STRONG&gt;mx8mqevk:/home/new_case1# lcov --capture --directory . --output-file main_coverage.info&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;Capturing coverage data from .&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;Can't locate bytes.pm in @INC (you may need to install the bytes module) (@INC contains: /usr/lib/perl5/site_perl/5.30.1/aarch64-linux /usr/lib/perl5/site_perl/5.30.1 /usr/lib/perl5/vendor_perl/5.30.1/aarch64-linux /usr/lib/perl5/vendor_perl/5.30.1 /usr/lib/perl5/5.30.1/aarch64-linux /usr/lib/perl5/5.30.1 .) at /usr/lib/perl5/vendor_perl/5.30.1/JSON/backportPP.pm line 751.&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;BEGIN failed--compilation aborted at /usr/lib/perl5/vendor_perl/5.30.1/JSON/backportPP.pm line 751.&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;Compilation failed in require at (eval 15) line 1.&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;at /usr/bin/geninfo line 63.&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;Compilation failed in require at /usr/bin/geninfo line 63.&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;BEGIN failed--compilation aborted at /usr/bin/geninfo line 63.&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;Can you please suggest what could be the issue here. The same thing working on ubuntu 16.04 without error.&lt;/P&gt;</description>
    <pubDate>Thu, 03 Jun 2021 17:50:21 GMT</pubDate>
    <dc:creator>vsuneja63</dc:creator>
    <dc:date>2021-06-03T17:50:21Z</dc:date>
    <item>
      <title>imx8: perl error while creating code coverage file using lcov on i.MX8MQ with googletest framework</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8-perl-error-while-creating-code-coverage-file-using-lcov-on/m-p/1286999#M174999</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Trying to create code coverage file after unit testing with googletest framework using lcov on i.MX8MQ target. But failing with some perl error. Here are the error logs:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;i&lt;STRONG&gt;mx8mqevk:/home/new_case1# lcov --capture --directory . --output-file main_coverage.info&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;Capturing coverage data from .&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;Can't locate bytes.pm in @INC (you may need to install the bytes module) (@INC contains: /usr/lib/perl5/site_perl/5.30.1/aarch64-linux /usr/lib/perl5/site_perl/5.30.1 /usr/lib/perl5/vendor_perl/5.30.1/aarch64-linux /usr/lib/perl5/vendor_perl/5.30.1 /usr/lib/perl5/5.30.1/aarch64-linux /usr/lib/perl5/5.30.1 .) at /usr/lib/perl5/vendor_perl/5.30.1/JSON/backportPP.pm line 751.&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;BEGIN failed--compilation aborted at /usr/lib/perl5/vendor_perl/5.30.1/JSON/backportPP.pm line 751.&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;Compilation failed in require at (eval 15) line 1.&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;at /usr/bin/geninfo line 63.&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;Compilation failed in require at /usr/bin/geninfo line 63.&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;BEGIN failed--compilation aborted at /usr/bin/geninfo line 63.&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;Can you please suggest what could be the issue here. The same thing working on ubuntu 16.04 without error.&lt;/P&gt;</description>
      <pubDate>Thu, 03 Jun 2021 17:50:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8-perl-error-while-creating-code-coverage-file-using-lcov-on/m-p/1286999#M174999</guid>
      <dc:creator>vsuneja63</dc:creator>
      <dc:date>2021-06-03T17:50:21Z</dc:date>
    </item>
    <item>
      <title>Re: imx8: perl error while creating code coverage file using lcov on i.MX8MQ with googletest framewo</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8-perl-error-while-creating-code-coverage-file-using-lcov-on/m-p/1287561#M175057</link>
      <description>&lt;P&gt;Hello vsuneja63,&lt;/P&gt;
&lt;P&gt;This error is due to bad installation of perl, you can see this link to better installation:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/How-to-add-missing-perl-modules-into-yocto/m-p/626125?ru=244295&amp;amp;sr=stream" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/How-to-add-missing-perl-modules-into-yocto/m-p/626125?ru=244295&amp;amp;sr=stream&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 04 Jun 2021 13:18:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8-perl-error-while-creating-code-coverage-file-using-lcov-on/m-p/1287561#M175057</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2021-06-04T13:18:25Z</dc:date>
    </item>
    <item>
      <title>Re: imx8: perl error while creating code coverage file using lcov on i.MX8MQ with googletest framewo</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8-perl-error-while-creating-code-coverage-file-using-lcov-on/m-p/1291116#M175387</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;Installed bytes rpm package from perl5 manually in i.MX8 board. Issue resolved with this.&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Vipul Kumar&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 11 Jun 2021 06:26:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8-perl-error-while-creating-code-coverage-file-using-lcov-on/m-p/1291116#M175387</guid>
      <dc:creator>vsuneja63</dc:creator>
      <dc:date>2021-06-11T06:26:16Z</dc:date>
    </item>
  </channel>
</rss>