<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Error Building Process Stopped in imx8mm</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Error-Building-Process-Stopped-in-imx8mm/m-p/1286749#M174972</link>
    <description>&lt;P&gt;i have attached the file .There is not &amp;amp;IOMUX in that&lt;/P&gt;&lt;P&gt;i am using Android 10 OS files&lt;/P&gt;</description>
    <pubDate>Thu, 03 Jun 2021 10:36:03 GMT</pubDate>
    <dc:creator>Ruban1</dc:creator>
    <dc:date>2021-06-03T10:36:03Z</dc:date>
    <item>
      <title>Error Building Process Stopped in imx8mm</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-Building-Process-Stopped-in-imx8mm/m-p/1285091#M174792</link>
      <description>&lt;P&gt;Error Building Process Stopped in imx8mm&lt;/P&gt;&lt;P&gt;i added GPIO in imx8mm-evk.dts file inside freescale folder&lt;/P&gt;&lt;P&gt;&amp;amp;iomuxc {&lt;BR /&gt;pinctrl-0 = &amp;lt;&amp;amp;pinctrl_hog_1&amp;gt;;&lt;BR /&gt;pinctrl_hog_1: hoggrp-1 {&lt;BR /&gt;fsl,pins = &amp;lt;&lt;BR /&gt;MX8MM_IOMUXC_GPIO1_IO08_GPIO1_IO8 0x19&lt;BR /&gt;MX8MM_IOMUXC_SAI5_RXD3_GPIO3_IO24 0x41&lt;/P&gt;&lt;P&gt;&amp;gt;;&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;};&lt;/P&gt;&lt;P&gt;Wen i run ./imx-make.sh&lt;/P&gt;&lt;P&gt;It stops inbetween i hve attached a screenshot.&lt;/P&gt;</description>
      <pubDate>Tue, 01 Jun 2021 05:52:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-Building-Process-Stopped-in-imx8mm/m-p/1285091#M174792</guid>
      <dc:creator>Ruban1</dc:creator>
      <dc:date>2021-06-01T05:52:47Z</dc:date>
    </item>
    <item>
      <title>Re: Error Building Process Stopped in imx8mm</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-Building-Process-Stopped-in-imx8mm/m-p/1286715#M174965</link>
      <description>&lt;P&gt;You may take this for reference.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8x-mek.dtsi?h=rel_imx_5.4.47_2.2.0" target="_blank"&gt;https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8x-mek.dtsi?h=rel_imx_5.4.47_2.2.0&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;CODE&gt;&lt;/CODE&gt;&lt;/P&gt;
&lt;PRE&gt;&amp;amp;iomuxc {
	pinctrl-names = "default";
	pinctrl-0 = &amp;lt;&amp;amp;pinctrl_hog&amp;gt;;

	pinctrl_hog: hoggrp {
		fsl,pins = &amp;lt;
			IMX8QXP_MCLK_OUT0_ADMA_ACM_MCLK_OUT0       0x0600004c
			IMX8QXP_COMP_CTL_GPIO_1V8_3V3_GPIORHB_PAD  0x000514a0
		&amp;gt;;
	};&lt;/PRE&gt;
&lt;P&gt;&lt;LI-WRAPPER&gt;&lt;/LI-WRAPPER&gt;&lt;/P&gt;
&lt;PRE&gt;&lt;CODE&gt;&lt;/CODE&gt;&lt;/PRE&gt;</description>
      <pubDate>Thu, 03 Jun 2021 09:41:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-Building-Process-Stopped-in-imx8mm/m-p/1286715#M174965</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2021-06-03T09:41:37Z</dc:date>
    </item>
    <item>
      <title>Re: Error Building Process Stopped in imx8mm</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-Building-Process-Stopped-in-imx8mm/m-p/1286749#M174972</link>
      <description>&lt;P&gt;i have attached the file .There is not &amp;amp;IOMUX in that&lt;/P&gt;&lt;P&gt;i am using Android 10 OS files&lt;/P&gt;</description>
      <pubDate>Thu, 03 Jun 2021 10:36:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-Building-Process-Stopped-in-imx8mm/m-p/1286749#M174972</guid>
      <dc:creator>Ruban1</dc:creator>
      <dc:date>2021-06-03T10:36:03Z</dc:date>
    </item>
    <item>
      <title>Re: Error Building Process Stopped in imx8mm</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-Building-Process-Stopped-in-imx8mm/m-p/1286754#M174976</link>
      <description>&lt;P&gt;imx8mm.dtsi is for the chip. You should modify the dts or dtsi file for the board. There should have a imx8mm-evk.dts for the evk board.&lt;/P&gt;</description>
      <pubDate>Thu, 03 Jun 2021 10:42:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-Building-Process-Stopped-in-imx8mm/m-p/1286754#M174976</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2021-06-03T10:42:17Z</dc:date>
    </item>
    <item>
      <title>Re: Error Building Process Stopped in imx8mm</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-Building-Process-Stopped-in-imx8mm/m-p/1287205#M175018</link>
      <description>&lt;P&gt;i have imx8mm-evk.dts file&amp;nbsp;&lt;/P&gt;&lt;P&gt;in that i hve &amp;amp; iomux but inside that function. imx8mm-evk function is not available .&lt;/P&gt;&lt;P&gt;I have attached the file below&amp;nbsp;&lt;/P&gt;&lt;P&gt;So to add&amp;nbsp;&lt;/P&gt;&lt;P&gt;MX8MM_IOMUXC_SAI5_RXD3_GPIO3_IO24&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;0x41&lt;/P&gt;&lt;P&gt;In which inner function should i add .So it wil be available in below path&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;$ ls /sys/class/gpio&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 04 Jun 2021 03:28:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-Building-Process-Stopped-in-imx8mm/m-p/1287205#M175018</guid>
      <dc:creator>Ruban1</dc:creator>
      <dc:date>2021-06-04T03:28:19Z</dc:date>
    </item>
    <item>
      <title>Re: Error Building Process Stopped in imx8mm</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-Building-Process-Stopped-in-imx8mm/m-p/1287854#M175081</link>
      <description>&lt;P&gt;So, I shown you the example in imx8x-mek.dtsi above. You can do the same in imx8mm-evk.dts.&lt;/P&gt;</description>
      <pubDate>Sun, 06 Jun 2021 13:13:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-Building-Process-Stopped-in-imx8mm/m-p/1287854#M175081</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2021-06-06T13:13:31Z</dc:date>
    </item>
  </channel>
</rss>