<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Unable to enter u-boot while pressing any key</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Unable-to-enter-u-boot-while-pressing-any-key/m-p/1285677#M174849</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Well there is not much of a step by step guide I can give, I tried on my side with default image and it stops well at uboot, I can even log in Linux properly after it finish booting.&lt;BR /&gt;&lt;BR /&gt;I'll recommend checking that the cable used for debug connection is correct and the cable have no damage.&lt;BR /&gt;&lt;BR /&gt;Also, checking that minicom have the correct configuration.&lt;BR /&gt;&lt;BR /&gt;What I always do is when I see the first uboot messages, I press Enter key a couple of times so I don't miss the countdown, and that’s it.&lt;BR /&gt;&lt;BR /&gt;Just for the record I use a windows host PC and use tera term for the serial connection.&lt;BR /&gt;&lt;BR /&gt;For a guide on how to get started with the i.MX8MP EVK you may take a look here:&lt;BR /&gt;&lt;A href="https://www.nxp.com/document/guide/get-started-with-the-i-mx-8m-plus-evk:GS-iMX-8M-Plus-EVK" target="_blank"&gt;https://www.nxp.com/document/guide/get-started-with-the-i-mx-8m-plus-evk:GS-iMX-8M-Plus-EVK&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
    <pubDate>Wed, 02 Jun 2021 00:12:36 GMT</pubDate>
    <dc:creator>AldoG</dc:creator>
    <dc:date>2021-06-02T00:12:36Z</dc:date>
    <item>
      <title>Unable to enter u-boot while pressing any key</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Unable-to-enter-u-boot-while-pressing-any-key/m-p/1283408#M174621</link>
      <description>&lt;P&gt;I am using i.mx8mp evk board. While booting from emmc, when i press any key within 2 seconds to stop auto-boot it is not happening. When after booting is completed, when I press anything after uboot it is not taking any input. Even this booting is not right, please check and give step by step detailed suggestion since I am a beginner how to do it? I tried twice but it is not recognising any input. Yesterday I tried to boot from sd card too but faced the same problem.&lt;/P&gt;&lt;P&gt;OUtput:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Welcome to minicom 2.7.1&lt;/P&gt;&lt;P&gt;OPTIONS: I18n&lt;BR /&gt;Compiled on Dec 23 2019, 02:06:26.&lt;BR /&gt;Port /dev/ttyUSB2, 03:18:21&lt;/P&gt;&lt;P&gt;Press CTRL-A Z for help on special keys&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;U-Boot SPL 2020.04-5.10.9-1.0.0+gad7b74b415 (Mar 05 2021 - 07:05:56 +0000)&lt;BR /&gt;DDRINFO: start DRAM init&lt;BR /&gt;DDRINFO: DRAM rate 4000MTS&lt;BR /&gt;DDRINFO:ddrphy calibration done&lt;BR /&gt;DDRINFO: ddrmix config done&lt;BR /&gt;Normal Boot&lt;BR /&gt;Trying to boot from BOOTROM&lt;BR /&gt;image offset 0x8000, pagesize 0x200, ivt offset 0x0&lt;BR /&gt;NOTICE: BL31: v2.4(release):lf-5.10.y-1.0.0-rc2-1-gba76d337e&lt;BR /&gt;NOTICE: BL31: Built : 08:27:48, Mar 1 2021&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;U-Boot 2020.04-5.10.9-1.0.0+gad7b74b415 (Mar 05 2021 - 07:05:56 +0000)&lt;/P&gt;&lt;P&gt;CPU: i.MX8MP[8] rev1.1 1800 MHz (running at 1200 MHz)&lt;BR /&gt;CPU: Commercial temperature grade (0C to 95C) at 25C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Model: NXP i.MX8MPlus LPDDR4 EVK board&lt;BR /&gt;DRAM: 6 GiB&lt;BR /&gt;TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C2 0x50]&lt;BR /&gt;SNK.Power3.0 on CC2&lt;BR /&gt;tcpc_pd_receive_message: Polling ALERT register, TCPC_ALERT_RX_STATUS bit failed, ret = -62&lt;BR /&gt;Power supply on USB2&lt;BR /&gt;TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x50]&lt;BR /&gt;MMC: FSL_SDHC: 1, FSL_SDHC: 2&lt;BR /&gt;Loading Environment from MMC... Run CMD11 1.8V switch&lt;BR /&gt;*** Warning - bad CRC, using default environment&lt;/P&gt;&lt;P&gt;[*]-Video Link 0Can't find cec device id=0x3c&lt;BR /&gt;fail to probe panel device adv7535@3d&lt;BR /&gt;fail to get display timings&lt;BR /&gt;probe video device failed, ret -19&lt;/P&gt;&lt;P&gt;[0] lcd-controller@32e80000, video&lt;BR /&gt;[1] mipi_dsi@32e60000, video_bridge&lt;BR /&gt;[2] adv7535@3d, panel&lt;BR /&gt;Can't find cec device id=0x3c&lt;BR /&gt;fail to probe panel device adv7535@3d&lt;BR /&gt;fail to get display timings&lt;BR /&gt;probe video device failed, ret -19&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;/P&gt;&lt;P&gt;BuildInfo:&lt;BR /&gt;- ATF ba76d33&lt;BR /&gt;- U-Boot 2020.04-5.10.9-1.0.0+gad7b74b415&lt;/P&gt;&lt;P&gt;Run CMD11 1.8V switch&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc1 is current device&lt;BR /&gt;flash target is MMC:1&lt;BR /&gt;Run CMD11 1.8V switch&lt;BR /&gt;Net:&lt;BR /&gt;Warning: ethernet@30be0000 using MAC address from ROM&lt;/P&gt;&lt;P&gt;Warning: ethernet@30bf0000 using MAC address from ROM&lt;BR /&gt;eth0: ethernet@30be0000, eth1: ethernet@30bf0000 [PRIME]&lt;BR /&gt;Fastboot: Normal&lt;BR /&gt;Normal Boot&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;Run CMD11 1.8V switch&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc1 is current device&lt;BR /&gt;Run CMD11 1.8V switch&lt;BR /&gt;Booting from net ...&lt;BR /&gt;ethernet@30bf0000 Waiting for PHY auto negotiation to complete.................&lt;BR /&gt;U-Boot SPL 2020.04-5.10.9-1.0.0+gad7b74b415 (Mar 05 2021 - 07:05:56 +0000)&lt;BR /&gt;DDRINFO: start DRAM init&lt;BR /&gt;DDRINFO: DRAM rate 4000MTS&lt;BR /&gt;DDRINFO:ddrphy calibration done&lt;BR /&gt;DDRINFO: ddrmix config done&lt;BR /&gt;Normal Boot&lt;BR /&gt;Trying to boot from BOOTROM&lt;BR /&gt;image offset 0x8000, pagesize 0x200, ivt offset 0x0&lt;BR /&gt;NOTICE: BL31: v2.4(release):lf-5.10.y-1.0.0-rc2-1-gba76d337e&lt;BR /&gt;NOTICE: BL31: Built : 08:27:48, Mar 1 2021&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;U-Boot 2020.04-5.10.9-1.0.0+gad7b74b415 (Mar 05 2021 - 07:05:56 +0000)&lt;/P&gt;&lt;P&gt;CPU: i.MX8MP[8] rev1.1 1800 MHz (running at 1200 MHz)&lt;BR /&gt;CPU: Commercial temperature grade (0C to 95C) at 25C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Model: NXP i.MX8MPlus LPDDR4 EVK board&lt;BR /&gt;DRAM: 6 GiB&lt;BR /&gt;TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C2 0x50]&lt;BR /&gt;Power supply on USB2&lt;BR /&gt;TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x50]&lt;BR /&gt;MMC: FSL_SDHC: 1, FSL_SDHC: 2&lt;BR /&gt;Loading Environment from MMC... Run CMD11 1.8V switch&lt;BR /&gt;*** Warning - bad CRC, using default environment&lt;/P&gt;&lt;P&gt;[*]-Video Link 0Can't find cec device id=0x3c&lt;BR /&gt;fail to probe panel device adv7535@3d&lt;BR /&gt;fail to get display timings&lt;BR /&gt;probe video device failed, ret -19&lt;/P&gt;&lt;P&gt;[0] lcd-controller@32e80000, video&lt;BR /&gt;[1] mipi_dsi@32e60000, video_bridge&lt;BR /&gt;[2] adv7535@3d, panel&lt;BR /&gt;Can't find cec device id=0x3c&lt;BR /&gt;fail to probe panel device adv7535@3d&lt;BR /&gt;fail to get display timings&lt;BR /&gt;probe video device failed, ret -19&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;/P&gt;&lt;P&gt;BuildInfo:&lt;BR /&gt;- ATF ba76d33&lt;BR /&gt;- U-Boot 2020.04-5.10.9-1.0.0+gad7b74b415&lt;/P&gt;&lt;P&gt;Run CMD11 1.8V switch&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc1 is current device&lt;BR /&gt;flash target is MMC:1&lt;BR /&gt;Run CMD11 1.8V switch&lt;BR /&gt;Net:&lt;BR /&gt;Warning: ethernet@30be0000 using MAC address from ROM&lt;/P&gt;&lt;P&gt;Warning: ethernet@30bf0000 using MAC address from ROM&lt;BR /&gt;eth0: ethernet@30be0000, eth1: ethernet@30bf0000 [PRIME]&lt;BR /&gt;Fastboot: Normal&lt;BR /&gt;Normal Boot&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;Run CMD11 1.8V switch&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc1 is current device&lt;BR /&gt;Run CMD11 1.8V switch&lt;BR /&gt;Booting from net ...&lt;BR /&gt;ethernet@30bf0000 Waiting for PHY auto negotiation to complete........&lt;BR /&gt;U-Boot SPL 2020.04-5.10.9-1.0.0+gad7b74b415 (Mar 05 2021 - 07:05:56 +0000)&lt;BR /&gt;DDRINFO: start DRAM init&lt;BR /&gt;DDRINFO: DRAM rate 4000MTS&lt;BR /&gt;DDRINFO:ddrphy calibration done&lt;BR /&gt;DDRINFO: ddrmix config done&lt;BR /&gt;Normal Boot&lt;BR /&gt;Trying to boot from BOOTROM&lt;BR /&gt;image offset 0x8000, pagesize 0x200, ivt offset 0x0&lt;BR /&gt;NOTICE: BL31: v2.4(release):lf-5.10.y-1.0.0-rc2-1-gba76d337e&lt;BR /&gt;NOTICE: BL31: Built : 08:27:48, Mar 1 2021&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;U-Boot 2020.04-5.10.9-1.0.0+gad7b74b415 (Mar 05 2021 - 07:05:56 +0000)&lt;/P&gt;&lt;P&gt;CPU: i.MX8MP[8] rev1.1 1800 MHz (running at 1200 MHz)&lt;BR /&gt;CPU: Commercial temperature grade (0C to 95C) at 25C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Model: NXP i.MX8MPlus LPDDR4 EVK board&lt;BR /&gt;DRAM: 6 GiB&lt;BR /&gt;TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C2 0x50]&lt;BR /&gt;Power supply on USB2&lt;BR /&gt;TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x50]&lt;BR /&gt;MMC: FSL_SDHC: 1, FSL_SDHC: 2&lt;BR /&gt;Loading Environment from MMC... Run CMD11 1.8V switch&lt;BR /&gt;*** Warning - bad CRC, using default environment&lt;/P&gt;&lt;P&gt;[*]-Video Link 0Can't find cec device id=0x3c&lt;BR /&gt;fail to probe panel device adv7535@3d&lt;BR /&gt;fail to get display timings&lt;BR /&gt;probe video device failed, ret -19&lt;/P&gt;&lt;P&gt;[0] lcd-controller@32e80000, video&lt;BR /&gt;[1] mipi_dsi@32e60000, video_bridge&lt;BR /&gt;[2] adv7535@3d, panel&lt;BR /&gt;Can't find cec device id=0x3c&lt;BR /&gt;fail to probe panel device adv7535@3d&lt;BR /&gt;fail to get display timings&lt;BR /&gt;probe video device failed, ret -19&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;/P&gt;&lt;P&gt;BuildInfo:&lt;BR /&gt;- ATF ba76d33&lt;BR /&gt;- U-Boot 2020.04-5.10.9-1.0.0+gad7b74b415&lt;/P&gt;&lt;P&gt;Run CMD11 1.8V switch&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc1 is current device&lt;BR /&gt;flash target is MMC:1&lt;BR /&gt;Run CMD11 1.8V switch&lt;BR /&gt;Net:&lt;BR /&gt;Warning: ethernet@30be0000 using MAC address from ROM&lt;/P&gt;&lt;P&gt;Warning: ethernet@30bf0000 using MAC address from ROM&lt;BR /&gt;eth0: ethernet@30be0000, eth1: ethernet@30bf0000 [PRIME]&lt;BR /&gt;Fastboot: Normal&lt;BR /&gt;Normal Boot&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;Run CMD11 1.8V switch&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc1 is current device&lt;BR /&gt;Run CMD11 1.8V switch&lt;BR /&gt;Booting from net ...&lt;BR /&gt;ethernet@30bf0000 Waiting for PHY auto negotiation to complete......................................... TIMEOUT !&lt;BR /&gt;phy_startup() failed: -110FAILED: -110ethernet@30be0000 Waiting for PHY auto negotiation to complete......................................... TIMEOUT !&lt;BR /&gt;Could not initialize PHY ethernet@30be0000&lt;BR /&gt;BOOTP broadcast 1&lt;BR /&gt;BOOTP broadcast 2&lt;BR /&gt;BOOTP broadcast 3&lt;BR /&gt;BOOTP broadcast 4&lt;BR /&gt;BOOTP broadcast 5&lt;BR /&gt;BOOTP broadcast 6&lt;BR /&gt;BOOTP broadcast 7&lt;BR /&gt;BOOTP broadcast 8&lt;BR /&gt;BOOTP broadcast 9&lt;BR /&gt;BOOTP broadcast 10&lt;BR /&gt;BOOTP broadcast 11&lt;BR /&gt;BOOTP broadcast 12&lt;BR /&gt;BOOTP broadcast 13&lt;BR /&gt;BOOTP broadcast 14&lt;BR /&gt;BOOTP broadcast 15&lt;BR /&gt;BOOTP broadcast 16&lt;BR /&gt;BOOTP broadcast 17&lt;/P&gt;&lt;P&gt;Retry time exceeded; starting again&lt;BR /&gt;ethernet@30be0000 Waiting for PHY auto negotiation to complete......................................... TIMEOUT !&lt;BR /&gt;Could not initialize PHY ethernet@30be0000&lt;BR /&gt;BOOTP broadcast 1&lt;BR /&gt;BOOTP broadcast 2&lt;BR /&gt;BOOTP broadcast 3&lt;BR /&gt;BOOTP broadcast 4&lt;BR /&gt;BOOTP broadcast 5&lt;BR /&gt;BOOTP broadcast 6&lt;BR /&gt;BOOTP broadcast 7&lt;BR /&gt;BOOTP broadcast 8&lt;BR /&gt;BOOTP broadcast 9&lt;BR /&gt;BOOTP broadcast 10&lt;BR /&gt;BOOTP broadcast 11&lt;BR /&gt;BOOTP broadcast 12&lt;BR /&gt;BOOTP broadcast 13&lt;BR /&gt;BOOTP broadcast 14&lt;BR /&gt;BOOTP broadcast 15&lt;BR /&gt;BOOTP broadcast 16&lt;BR /&gt;BOOTP broadcast 17&lt;/P&gt;&lt;P&gt;Retry time exceeded; starting again&lt;BR /&gt;WARN: Cannot load the DT&lt;/P&gt;</description>
      <pubDate>Thu, 27 May 2021 10:33:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Unable-to-enter-u-boot-while-pressing-any-key/m-p/1283408#M174621</guid>
      <dc:creator>kenizgandhi</dc:creator>
      <dc:date>2021-05-27T10:33:57Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to enter u-boot while pressing any key</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Unable-to-enter-u-boot-while-pressing-any-key/m-p/1285677#M174849</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Well there is not much of a step by step guide I can give, I tried on my side with default image and it stops well at uboot, I can even log in Linux properly after it finish booting.&lt;BR /&gt;&lt;BR /&gt;I'll recommend checking that the cable used for debug connection is correct and the cable have no damage.&lt;BR /&gt;&lt;BR /&gt;Also, checking that minicom have the correct configuration.&lt;BR /&gt;&lt;BR /&gt;What I always do is when I see the first uboot messages, I press Enter key a couple of times so I don't miss the countdown, and that’s it.&lt;BR /&gt;&lt;BR /&gt;Just for the record I use a windows host PC and use tera term for the serial connection.&lt;BR /&gt;&lt;BR /&gt;For a guide on how to get started with the i.MX8MP EVK you may take a look here:&lt;BR /&gt;&lt;A href="https://www.nxp.com/document/guide/get-started-with-the-i-mx-8m-plus-evk:GS-iMX-8M-Plus-EVK" target="_blank"&gt;https://www.nxp.com/document/guide/get-started-with-the-i-mx-8m-plus-evk:GS-iMX-8M-Plus-EVK&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Wed, 02 Jun 2021 00:12:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Unable-to-enter-u-boot-while-pressing-any-key/m-p/1285677#M174849</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2021-06-02T00:12:36Z</dc:date>
    </item>
  </channel>
</rss>