<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックimxrt1024 flexpwm PWM_X</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imxrt1024-flexpwm-PWM-X/m-p/1283963#M174660</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using the FlexPWM of imxrt1024 to generate PWM. There is no problem with PWM_A and PWM_B channels, but there is&amp;nbsp; no PWM output when I using PWM_X. I see that some people have asked this question in the post, but no one make it clear and there is not a solution.&lt;/P&gt;&lt;P&gt;I used MCUXpresso config tools to configure the pins as PMW_X function. I also found that in the peripheral configuration, both channel A and B can select the PWM function, but the X channel does not have this option. In the official SDK, the PWM_SetupPwm function does not seem to be able to configure PWM_X.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can anyone explain what is going on?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="po-pony_0-1622186532704.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/145756i5B9126A543C7EC43/image-size/medium?v=v2&amp;amp;px=400" role="button" title="po-pony_0-1622186532704.png" alt="po-pony_0-1622186532704.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="po-pony_1-1622186588323.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/145757i5FCDC73B1170CE9A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="po-pony_1-1622186588323.png" alt="po-pony_1-1622186588323.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 28 May 2021 07:29:19 GMT</pubDate>
    <dc:creator>po-pony</dc:creator>
    <dc:date>2021-05-28T07:29:19Z</dc:date>
    <item>
      <title>imxrt1024 flexpwm PWM_X</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imxrt1024-flexpwm-PWM-X/m-p/1283963#M174660</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using the FlexPWM of imxrt1024 to generate PWM. There is no problem with PWM_A and PWM_B channels, but there is&amp;nbsp; no PWM output when I using PWM_X. I see that some people have asked this question in the post, but no one make it clear and there is not a solution.&lt;/P&gt;&lt;P&gt;I used MCUXpresso config tools to configure the pins as PMW_X function. I also found that in the peripheral configuration, both channel A and B can select the PWM function, but the X channel does not have this option. In the official SDK, the PWM_SetupPwm function does not seem to be able to configure PWM_X.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can anyone explain what is going on?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="po-pony_0-1622186532704.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/145756i5B9126A543C7EC43/image-size/medium?v=v2&amp;amp;px=400" role="button" title="po-pony_0-1622186532704.png" alt="po-pony_0-1622186532704.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="po-pony_1-1622186588323.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/145757i5FCDC73B1170CE9A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="po-pony_1-1622186588323.png" alt="po-pony_1-1622186588323.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 28 May 2021 07:29:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imxrt1024-flexpwm-PWM-X/m-p/1283963#M174660</guid>
      <dc:creator>po-pony</dc:creator>
      <dc:date>2021-05-28T07:29:19Z</dc:date>
    </item>
    <item>
      <title>Re: imxrt1024 flexpwm PWM_X</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imxrt1024-flexpwm-PWM-X/m-p/1284943#M174773</link>
      <description>&lt;P&gt;Hello po-pony,&lt;/P&gt;
&lt;P&gt;I looked for other threads regarding this topic and it seems that there are confusions in regards of the PWM_X pin.&lt;/P&gt;
&lt;P&gt;There are only two FlexPWMs on the i.MXRT1024. The PWM_X is not an independent signal, it is an accessory signal, it's rising edge and falling edge are controlled by the VAL0 and VAL1 registers.&lt;/P&gt;
&lt;P&gt;PWM_X pin can also optionally output a third PWM signal from each submodule. However, this function is apparently not enabled on the SDK driver, only capture is available.&lt;/P&gt;
&lt;P&gt;You can find how this is setup in Figure 50-2 PWM Submodule, on the i.MXRT1024 Reference Manual.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-center" image-alt="Figure 50-2 PWM.jpg" style="width: 880px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/145911iED5F9BF99134A431/image-size/large?v=v2&amp;amp;px=999" role="button" title="Figure 50-2 PWM.jpg" alt="Figure 50-2 PWM.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN style="font-family: inherit;"&gt;I hope that this information helps!&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Gustavo&lt;/P&gt;</description>
      <pubDate>Mon, 31 May 2021 22:37:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imxrt1024-flexpwm-PWM-X/m-p/1284943#M174773</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2021-05-31T22:37:14Z</dc:date>
    </item>
    <item>
      <title>Re: imxrt1024 flexpwm PWM_X</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imxrt1024-flexpwm-PWM-X/m-p/1284993#M174780</link>
      <description>&lt;P&gt;Hi &lt;SPAN&gt;Gustavo&lt;/SPAN&gt;&lt;SPAN class=""&gt;，&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;This is the clearest explanation about PWM_X so far. Your info help me a lot, thank you very much.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;po-pony&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 01 Jun 2021 01:26:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imxrt1024-flexpwm-PWM-X/m-p/1284993#M174780</guid>
      <dc:creator>po-pony</dc:creator>
      <dc:date>2021-06-01T01:26:36Z</dc:date>
    </item>
  </channel>
</rss>