<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: FlexRAM OCRAM</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/FlexRAM-OCRAM/m-p/1283849#M174652</link>
    <description>&lt;P&gt;Thank you！&lt;/P&gt;</description>
    <pubDate>Fri, 28 May 2021 03:52:05 GMT</pubDate>
    <dc:creator>po-pony</dc:creator>
    <dc:date>2021-05-28T03:52:05Z</dc:date>
    <item>
      <title>FlexRAM OCRAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FlexRAM-OCRAM/m-p/1277218#M174085</link>
      <description>&lt;P&gt;It is stated in the application note -&amp;nbsp;&lt;SPAN class="fontstyle0"&gt;AN12077,&amp;nbsp;&lt;/SPAN&gt;that the minimum configuration of OCRAM is 64 KB&lt;SPAN class="fontstyle0"&gt;. This is&lt;BR /&gt;required due to ROM code requires at least 64 KB of RAM for its execution. The minimum OCRAM requirements can be device dependent.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;But I can't find any such description in the 1024/1050 reference manual. All described are “RAM size of ITCM, DTCM and OCRAM can be configured from 0 to full RAM Array size separately".&lt;/P&gt;&lt;P&gt;I set OCRAM to 0, and the code seems to be able to run, so what is the actual situation?&lt;/P&gt;</description>
      <pubDate>Sun, 16 May 2021 10:26:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FlexRAM-OCRAM/m-p/1277218#M174085</guid>
      <dc:creator>po-pony</dc:creator>
      <dc:date>2021-05-16T10:26:50Z</dc:date>
    </item>
    <item>
      <title>Re: FlexRAM OCRAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FlexRAM-OCRAM/m-p/1277365#M174108</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/186749"&gt;@po-pony&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;Hello,&lt;BR /&gt;&lt;SPAN style="left: 599.4px; top: 346.667px; font-size: 20px; font-family: serif; transform: scaleX(0.799081);"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P class="Normal"&gt;&lt;SPAN class="tm5"&gt;&amp;nbsp; Some memory is needed for boot purposes, therefore - although FlexRAM can be configured&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN class="tm5"&gt;for any size, including zero - really the minimum configuration of OCRAM of 64 KB is required&lt;BR /&gt;by boot ROM - this is correct. This relates only to boot ROM, which is affected only by &lt;/SPAN&gt;&lt;SPAN class="tm5"&gt;the FUSE FlexRAM bank configuration. &lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Yuri.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 17 May 2021 05:34:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FlexRAM-OCRAM/m-p/1277365#M174108</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2021-05-17T05:34:07Z</dc:date>
    </item>
    <item>
      <title>Re: FlexRAM OCRAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FlexRAM-OCRAM/m-p/1283849#M174652</link>
      <description>&lt;P&gt;Thank you！&lt;/P&gt;</description>
      <pubDate>Fri, 28 May 2021 03:52:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FlexRAM-OCRAM/m-p/1283849#M174652</guid>
      <dc:creator>po-pony</dc:creator>
      <dc:date>2021-05-28T03:52:05Z</dc:date>
    </item>
  </channel>
</rss>