<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MIPI-DSI Driver in U-boot for i.Mx8 MM in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-DSI-Driver-in-U-boot-for-i-Mx8-MM/m-p/1282656#M174580</link>
    <description>&lt;P&gt;Hello Igor,&lt;/P&gt;&lt;P&gt;I tired to add the panel in dts as below:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;File:&lt;/STRONG&gt;&lt;EM&gt;&amp;nbsp;arch/arm/dts/fsl-imx8mm-var-dart.dts&lt;/EM&gt;&lt;/P&gt;&lt;DIV class="lia-spoiler-container-editor"&gt;+&lt;BR /&gt;+&amp;amp;lcdif {&lt;BR /&gt;+ status = "okay";&lt;BR /&gt;+};&lt;BR /&gt;+&lt;BR /&gt;+&amp;amp;mipi_dsi {&lt;BR /&gt;+ status = "okay";&lt;BR /&gt;+ panel@0 {&lt;BR /&gt;+ compatible = "simple-panel";&lt;BR /&gt;+ reg = &amp;lt;0&amp;gt;;&lt;BR /&gt;+ pinctrl-0 = &amp;lt;&amp;amp;pinctrl_mipi_dsi_rst&amp;gt;;&lt;BR /&gt;+ reset-gpio =&amp;lt;&amp;amp;gpio5 26 GPIO_ACTIVE_LOW&amp;gt;;&lt;BR /&gt;+ dsi-lanes = &amp;lt;4&amp;gt;;&lt;BR /&gt;+ video-mode = &amp;lt;2&amp;gt;; /* 0: burst mode (high speed)&lt;BR /&gt;+ * 1: Low-Power Mode&lt;BR /&gt;+ */&lt;BR /&gt;+ vrefresh = &amp;lt;60&amp;gt;;&lt;BR /&gt;+ panel-width-mm = &amp;lt;52&amp;gt;;&lt;BR /&gt;+ panel-height-mm = &amp;lt;107&amp;gt;;&lt;BR /&gt;+ //backlight = &amp;lt;&amp;amp;backlight&amp;gt;; //comment it for now&lt;BR /&gt;+ };&lt;BR /&gt;+};&lt;/DIV&gt;&lt;P&gt;Q1. The driver is not getting probed after making the above changes, What can be the issue?&lt;/P&gt;&lt;P&gt;Q2. I&amp;nbsp;&lt;SPAN&gt;tried writing the init sequence&amp;nbsp;of LCD taking reference of the rm68000 but when we read back the reg values were&amp;nbsp;&lt;/SPAN&gt;different?&lt;/P&gt;&lt;P&gt;Q3. What is "imx_mipi_dsi_bridge_attach" in "imx_mipi_dsi_bridge.c/.h" file what is this file used for, Not getting this bridge here? As I am directly connecting the MIPI DSI display to MIPI DSI port.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Kailas Kharse&lt;/P&gt;</description>
    <pubDate>Thu, 27 May 2021 05:17:52 GMT</pubDate>
    <dc:creator>kailas_kharse</dc:creator>
    <dc:date>2021-05-27T05:17:52Z</dc:date>
    <item>
      <title>MIPI-DSI Driver in U-boot for i.Mx8 MM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-DSI-Driver-in-U-boot-for-i-Mx8-MM/m-p/1281804#M174506</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I wanted to use LCD UE040HD-RB40-L043A based on Driver IC ST7703 in U-boot, I have a working driver for ST7703 in Kernel working fine.&lt;/P&gt;&lt;P&gt;Can you please share the reference to how can I port the same driver to U-boot?&lt;/P&gt;&lt;P&gt;Do we have MIPI-DSI support is available in U-boot for i.Mx8MM?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Kailas Kharse&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 25 May 2021 12:06:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIPI-DSI-Driver-in-U-boot-for-i-Mx8-MM/m-p/1281804#M174506</guid>
      <dc:creator>kailas_kharse</dc:creator>
      <dc:date>2021-05-25T12:06:14Z</dc:date>
    </item>
    <item>
      <title>Re: MIPI-DSI Driver in U-boot for i.Mx8 MM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-DSI-Driver-in-U-boot-for-i-Mx8-MM/m-p/1282106#M174528</link>
      <description>&lt;P&gt;Hi Kailas&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;for i.MX8MM U-boot MIPI-DSI support one can look at below link, adjust&lt;/P&gt;
&lt;P&gt;struct display_info_t const displays[] for new lcd :&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/uboot-imx/tree/board/freescale/imx8mm_evk/imx8mm_evk.c?h=imx_v2019.04_5.4.3_2.0.0" target="_blank"&gt;https://source.codeaurora.org/external/imx/uboot-imx/tree/board/freescale/imx8mm_evk/imx8mm_evk.c?h=imx_v2019.04_5.4.3_2.0.0&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Wed, 26 May 2021 00:33:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIPI-DSI-Driver-in-U-boot-for-i-Mx8-MM/m-p/1282106#M174528</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-05-26T00:33:50Z</dc:date>
    </item>
    <item>
      <title>Re: MIPI-DSI Driver in U-boot for i.Mx8 MM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-DSI-Driver-in-U-boot-for-i-Mx8-MM/m-p/1282656#M174580</link>
      <description>&lt;P&gt;Hello Igor,&lt;/P&gt;&lt;P&gt;I tired to add the panel in dts as below:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;File:&lt;/STRONG&gt;&lt;EM&gt;&amp;nbsp;arch/arm/dts/fsl-imx8mm-var-dart.dts&lt;/EM&gt;&lt;/P&gt;&lt;DIV class="lia-spoiler-container-editor"&gt;+&lt;BR /&gt;+&amp;amp;lcdif {&lt;BR /&gt;+ status = "okay";&lt;BR /&gt;+};&lt;BR /&gt;+&lt;BR /&gt;+&amp;amp;mipi_dsi {&lt;BR /&gt;+ status = "okay";&lt;BR /&gt;+ panel@0 {&lt;BR /&gt;+ compatible = "simple-panel";&lt;BR /&gt;+ reg = &amp;lt;0&amp;gt;;&lt;BR /&gt;+ pinctrl-0 = &amp;lt;&amp;amp;pinctrl_mipi_dsi_rst&amp;gt;;&lt;BR /&gt;+ reset-gpio =&amp;lt;&amp;amp;gpio5 26 GPIO_ACTIVE_LOW&amp;gt;;&lt;BR /&gt;+ dsi-lanes = &amp;lt;4&amp;gt;;&lt;BR /&gt;+ video-mode = &amp;lt;2&amp;gt;; /* 0: burst mode (high speed)&lt;BR /&gt;+ * 1: Low-Power Mode&lt;BR /&gt;+ */&lt;BR /&gt;+ vrefresh = &amp;lt;60&amp;gt;;&lt;BR /&gt;+ panel-width-mm = &amp;lt;52&amp;gt;;&lt;BR /&gt;+ panel-height-mm = &amp;lt;107&amp;gt;;&lt;BR /&gt;+ //backlight = &amp;lt;&amp;amp;backlight&amp;gt;; //comment it for now&lt;BR /&gt;+ };&lt;BR /&gt;+};&lt;/DIV&gt;&lt;P&gt;Q1. The driver is not getting probed after making the above changes, What can be the issue?&lt;/P&gt;&lt;P&gt;Q2. I&amp;nbsp;&lt;SPAN&gt;tried writing the init sequence&amp;nbsp;of LCD taking reference of the rm68000 but when we read back the reg values were&amp;nbsp;&lt;/SPAN&gt;different?&lt;/P&gt;&lt;P&gt;Q3. What is "imx_mipi_dsi_bridge_attach" in "imx_mipi_dsi_bridge.c/.h" file what is this file used for, Not getting this bridge here? As I am directly connecting the MIPI DSI display to MIPI DSI port.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Kailas Kharse&lt;/P&gt;</description>
      <pubDate>Thu, 27 May 2021 05:17:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIPI-DSI-Driver-in-U-boot-for-i-Mx8-MM/m-p/1282656#M174580</guid>
      <dc:creator>kailas_kharse</dc:creator>
      <dc:date>2021-05-27T05:17:52Z</dc:date>
    </item>
    <item>
      <title>Re: MIPI-DSI Driver in U-boot for i.Mx8 MM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-DSI-Driver-in-U-boot-for-i-Mx8-MM/m-p/1286008#M174886</link>
      <description>&lt;P&gt;Hello Igor,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Do you have any update on the above thread, we are blocked can you please help on priority.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks ,&lt;BR /&gt;Kailas K.&lt;/P&gt;</description>
      <pubDate>Wed, 02 Jun 2021 09:06:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIPI-DSI-Driver-in-U-boot-for-i-Mx8-MM/m-p/1286008#M174886</guid>
      <dc:creator>kailas_kharse</dc:creator>
      <dc:date>2021-06-02T09:06:08Z</dc:date>
    </item>
    <item>
      <title>Re: MIPI-DSI Driver in U-boot for i.Mx8 MM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-DSI-Driver-in-U-boot-for-i-Mx8-MM/m-p/1295266#M175772</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/37066"&gt;@igorpadykov&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I also have a same requirement as &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/139188"&gt;@kailas_kharse&lt;/a&gt; i tried the same as you suggested&lt;/P&gt;&lt;P&gt;I tried adding the struct display_info_t in the board file but the enable function is not getting called do we need to set any environment variabled or some configuration needs to be enabled??&lt;/P&gt;&lt;P&gt;Can you write in detail how the struct display_info_t works? What are the configuration to enable??&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;</description>
      <pubDate>Mon, 21 Jun 2021 07:59:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIPI-DSI-Driver-in-U-boot-for-i-Mx8-MM/m-p/1295266#M175772</guid>
      <dc:creator>sd05</dc:creator>
      <dc:date>2021-06-21T07:59:30Z</dc:date>
    </item>
    <item>
      <title>Re: MIPI-DSI Driver in U-boot for i.Mx8 MM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-DSI-Driver-in-U-boot-for-i-Mx8-MM/m-p/1295354#M175782</link>
      <description>&lt;P&gt;one can try to add #def CONFIG_VIDEO to uboot/include/configs/imx8mm_evk.h&lt;BR /&gt;&lt;A href="https://source.codeaurora.org/external/imx/uboot-imx/tree/include/configs/imx8mm_evk.h?h=imx_v2019.04_5.4.3_2.0.0" target="_blank"&gt;https://source.codeaurora.org/external/imx/uboot-imx/tree/include/configs/imx8mm_evk.h?h=imx_v2019.04_5.4.3_2.0.0&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;remove adv7535,MIPI2HDMI from from board/freescale/imx8mm_evk/imx8mm_evk.c&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/uboot-imx/tree/board/freescale/imx8mm_evk/imx8mm_evk.c?h=imx_v2019.04_5.4.3_2.0.0" target="_blank"&gt;https://source.codeaurora.org/external/imx/uboot-imx/tree/board/freescale/imx8mm_evk/imx8mm_evk.c?h=imx_v2019.04_5.4.3_2.0.0&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 21 Jun 2021 10:01:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIPI-DSI-Driver-in-U-boot-for-i-Mx8-MM/m-p/1295354#M175782</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-06-21T10:01:08Z</dc:date>
    </item>
    <item>
      <title>Re: MIPI-DSI Driver in U-boot for i.Mx8 MM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-DSI-Driver-in-U-boot-for-i-Mx8-MM/m-p/1295357#M175785</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/37066"&gt;@igorpadykov&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for your quick response..&lt;/P&gt;&lt;P&gt;I have already added the said configs in my custom board config file and only added the display_info_t struct as in the imx8mm_evk.c but the enable function is not getting called.&lt;/P&gt;&lt;P&gt;Please guide with the full process.&lt;/P&gt;&lt;P&gt;Please note that I am having my custom board not using imx8mm_evk.c board file.&lt;/P&gt;&lt;P&gt;This task is on priority for us and struggling with this for a month please help us to get it resolved.&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Mon, 21 Jun 2021 10:12:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIPI-DSI-Driver-in-U-boot-for-i-Mx8-MM/m-p/1295357#M175785</guid>
      <dc:creator>sd05</dc:creator>
      <dc:date>2021-06-21T10:12:06Z</dc:date>
    </item>
    <item>
      <title>Re: MIPI-DSI Driver in U-boot for i.Mx8 MM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-DSI-Driver-in-U-boot-for-i-Mx8-MM/m-p/1295367#M175787</link>
      <description>&lt;P&gt;&lt;SPAN&gt;MX 8M Mini processor to provide&amp;nbsp;&lt;/SPAN&gt;&lt;EM&gt;MIPI&lt;/EM&gt;&lt;SPAN&gt;-&lt;/SPAN&gt;&lt;EM&gt;DSI&lt;/EM&gt;&lt;SPAN&gt;, MIPI-CSI, LVDS interfaces and Audio ... The MYC-C8MMX CPU Module is using NXP's 14 x 14&amp;nbsp;&lt;/SPAN&gt;&lt;EM&gt;mm&lt;/EM&gt;&lt;SPAN&gt;, 0.5&amp;nbsp;&lt;/SPAN&gt;&lt;EM&gt;mm&lt;/EM&gt;&lt;SPAN&gt;&amp;nbsp;pitch, ... Many peripheral&amp;nbsp;&lt;/SPAN&gt;&lt;EM&gt;drivers&lt;/EM&gt;&lt;SPAN&gt;&amp;nbsp;are in source code to help accelerate customers' designs​. ... Source Code Provided. Bootstrap program.&amp;nbsp;&lt;/SPAN&gt;&lt;EM&gt;U&lt;/EM&gt;&lt;SPAN&gt;-&lt;/SPAN&gt;&lt;EM&gt;boot&lt;/EM&gt;&lt;SPAN&gt;. The primary bootstrap.&lt;/SPAN&gt;&lt;A href="https://guestsurvey.onl/tag/tellbaskinrobbins-com-here-to-claim-coupon/" target="_self"&gt;TellBaskinRobbins&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 21 Jun 2021 10:28:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIPI-DSI-Driver-in-U-boot-for-i-Mx8-MM/m-p/1295367#M175787</guid>
      <dc:creator>melania77</dc:creator>
      <dc:date>2021-06-21T10:28:01Z</dc:date>
    </item>
    <item>
      <title>Re: MIPI-DSI Driver in U-boot for i.Mx8 MM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-DSI-Driver-in-U-boot-for-i-Mx8-MM/m-p/1295379#M175791</link>
      <description>&lt;P&gt;also one can check&amp;nbsp;rm67191_panel in dts&lt;/P&gt;
&lt;P&gt;&lt;A href="https://github.com/varigit/uboot-imx/blob/imx_v2020.04_5.4.70_2.3.2_var01/arch/arm/dts/imx8mm-evk.dts" target="_blank" rel="noopener"&gt;https://github.com/varigit/uboot-imx/blob/imx_v2020.04_5.4.70_2.3.2_var01/arch/arm/dts/imx8mm-evk.dts&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Another example boundary devices uboot nitrogen MX8M Mini LTK080A60A004T mipi display :&lt;/P&gt;
&lt;P&gt;&lt;A href="https://github.com/boundarydevices/u-boot-imx6/blob/boundary-v2020.10/board/boundary/nitrogen8mm_som/nitrogen8mm_som.c" target="_blank"&gt;https://github.com/boundarydevices/u-boot-imx6/blob/boundary-v2020.10/board/boundary/nitrogen8mm_som/nitrogen8mm_som.c&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Mon, 21 Jun 2021 10:55:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIPI-DSI-Driver-in-U-boot-for-i-Mx8-MM/m-p/1295379#M175791</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-06-21T10:55:26Z</dc:date>
    </item>
    <item>
      <title>Re: MIPI-DSI Driver in U-boot for i.Mx8 MM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-DSI-Driver-in-U-boot-for-i-Mx8-MM/m-p/1295427#M175795</link>
      <description>&lt;P&gt;Thanks &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/37066"&gt;@igorpadykov&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But this is not the info I am seeking&lt;/P&gt;&lt;P&gt;I want to know the api sequence following which the lcd init_sequence is called and splash screen is display on lcd panel&lt;/P&gt;&lt;P&gt;Need help from some uboot expert&lt;/P&gt;</description>
      <pubDate>Mon, 21 Jun 2021 12:34:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIPI-DSI-Driver-in-U-boot-for-i-Mx8-MM/m-p/1295427#M175795</guid>
      <dc:creator>sd05</dc:creator>
      <dc:date>2021-06-21T12:34:19Z</dc:date>
    </item>
  </channel>
</rss>