<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMX8M nano evk Linux BSP prebuilt boot from SD in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-nano-evk-Linux-BSP-prebuilt-boot-from-SD/m-p/1282542#M174571</link>
    <description>&lt;P&gt;Thank you very much. I was able to debug and see in the log an error reported in this &lt;A href="https://community.nxp.com/t5/i-MX-Processors/Can-t-find-PMIC-PCA9450/m-p/1163833" target="_self"&gt;post&lt;/A&gt;. It turns auto that I have a 8MNANOD4-EVK thus I have downloaded the LF_v5.4.3 BSP and it worked.&lt;/P&gt;</description>
    <pubDate>Wed, 26 May 2021 11:38:55 GMT</pubDate>
    <dc:creator>ncovallero</dc:creator>
    <dc:date>2021-05-26T11:38:55Z</dc:date>
    <item>
      <title>IMX8M nano evk Linux BSP prebuilt boot from SD</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-nano-evk-Linux-BSP-prebuilt-boot-from-SD/m-p/1280444#M174391</link>
      <description>&lt;P&gt;Hi all,&lt;BR /&gt;&lt;BR /&gt;I have a IMX 8M Nano EVK board and I am trying to flash in the SD the latest LB downloaded from &lt;A href="https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX" target="_blank" rel="noopener"&gt;https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;I am following chapter "&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;&lt;SPAN&gt;4.3.2&lt;/SPAN&gt;&lt;SPAN&gt;Copying the full SD card image" of Linux User's Guide.&lt;BR /&gt;&lt;BR /&gt;So I plug my SD in the SD Reader and then launching the command:&lt;BR /&gt;&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;&lt;SPAN&gt;sudo dd if=imx-image-full-imx8mnevk.wic of=/dev/sdb bs=1M &amp;amp;&amp;amp; sync&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;&lt;SPAN&gt;Then I plugged it to the EVK board, setting properly the switches in manner to boot from the SD but nothing happens at power on. I know that it can boot from the SD correctly because we have another SD with Ubuntu Bionic that can correctly boot (I see the video output via HDMI) provided by an ex-employee. I need to make this work at least with the prebuilt Linux versions NXP provides.&lt;BR /&gt;&lt;BR /&gt;Is there something I am missing?&lt;BR /&gt;&lt;BR /&gt;Thanks in advance&lt;BR /&gt;&lt;BR /&gt;UPDATE:&lt;BR /&gt;I also tried the solution mention in the question &lt;A href="https://community.nxp.com/t5/i-MX-Processors/Understanding-imx8mqevk-and-booting-linux-from-sdcard/m-p/957623/thread-id/143066" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/Understanding-imx8mqevk-and-booting-linux-from-sdcard/m-p/957623/thread-id/143066&lt;/A&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;&lt;SPAN&gt;So I did the following operations:&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;&lt;SPAN&gt;&lt;BR /&gt;sudo dd if=imx-image-full-imx8mnevk.wic of=/dev/sdb bs=1M &amp;amp;&amp;amp; sync&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;&lt;SPAN&gt;sudo dd if=fsl-image-mfgtool-initramfs-imx_mfgtools.cpio.gz.u-boot of=/dev/sdb bs=1k seek=32 conv=fsync&lt;BR /&gt;&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;&lt;SPAN&gt;But it still does not boot.&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 21 May 2021 15:09:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8M-nano-evk-Linux-BSP-prebuilt-boot-from-SD/m-p/1280444#M174391</guid>
      <dc:creator>ncovallero</dc:creator>
      <dc:date>2021-05-21T15:09:30Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8M nano evk Linux BSP prebuilt boot from SD</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-nano-evk-Linux-BSP-prebuilt-boot-from-SD/m-p/1282038#M174518</link>
      <description>&lt;P&gt;Hi ncovallero,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Well, it could be that the board is getting stuck before anything boot, you could try to see activity on the debug port, you can follow the instructions from the web page, link below. Also one can try to program the sd with the mfgtool on serial mode, the instructions can be found on the Linux users guide that comes with the BSP, also link below.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/document/guide/getting-started-with-the-i-mx-8m-nano-evk-board:GS-8MNANOLPD4-EVK" target="_blank"&gt;https://www.nxp.com/document/guide/getting-started-with-the-i-mx-8m-nano-evk-board:GS-8MNANOLPD4-EVK&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/release-note/IMX_LINUX_RELEASE_NOTES.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/release-note/IMX_LINUX_RELEASE_NOTES.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Israel.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 25 May 2021 20:03:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8M-nano-evk-Linux-BSP-prebuilt-boot-from-SD/m-p/1282038#M174518</guid>
      <dc:creator>nxf63675</dc:creator>
      <dc:date>2021-05-25T20:03:14Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8M nano evk Linux BSP prebuilt boot from SD</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-nano-evk-Linux-BSP-prebuilt-boot-from-SD/m-p/1282542#M174571</link>
      <description>&lt;P&gt;Thank you very much. I was able to debug and see in the log an error reported in this &lt;A href="https://community.nxp.com/t5/i-MX-Processors/Can-t-find-PMIC-PCA9450/m-p/1163833" target="_self"&gt;post&lt;/A&gt;. It turns auto that I have a 8MNANOD4-EVK thus I have downloaded the LF_v5.4.3 BSP and it worked.&lt;/P&gt;</description>
      <pubDate>Wed, 26 May 2021 11:38:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8M-nano-evk-Linux-BSP-prebuilt-boot-from-SD/m-p/1282542#M174571</guid>
      <dc:creator>ncovallero</dc:creator>
      <dc:date>2021-05-26T11:38:55Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8M nano evk Linux BSP prebuilt boot from SD</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-nano-evk-Linux-BSP-prebuilt-boot-from-SD/m-p/1285149#M174796</link>
      <description>&lt;P&gt;Hi, I finally found the solution. I finally was able to see the debug info through the serial port and I found the error "Can't find PMIC", after googling a bit I found that there exists two versions of the IMX8 Nano evaluation board. I have the 8MNANOD4-EVK which is not supported by the latest prebuilt linux binaries, so I downloaded a previous version and it did work.&lt;/P&gt;</description>
      <pubDate>Tue, 01 Jun 2021 07:07:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8M-nano-evk-Linux-BSP-prebuilt-boot-from-SD/m-p/1285149#M174796</guid>
      <dc:creator>ncovallero</dc:creator>
      <dc:date>2021-06-01T07:07:30Z</dc:date>
    </item>
  </channel>
</rss>