<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Issue flashing prebuilt android image in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Issue-flashing-prebuilt-android-image/m-p/1282044#M174520</link>
    <description>&lt;P&gt;Thanks for the reference Igor.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Do you know where I can download ' imx-sdcard-partition.sh'?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Seems I can download Linux pre-built image, but not Android for some reason.&lt;/P&gt;</description>
    <pubDate>Tue, 25 May 2021 20:26:19 GMT</pubDate>
    <dc:creator>pwcel</dc:creator>
    <dc:date>2021-05-25T20:26:19Z</dc:date>
    <item>
      <title>Issue flashing prebuilt android image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issue-flashing-prebuilt-android-image/m-p/1281199#M174456</link>
      <description>&lt;P&gt;Following the Jan 2021 release of the 'Android_Quick_Start_Guide.pdf' but can't flash pre-built android image.&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Ubuntu 18.04&lt;/LI&gt;&lt;LI&gt;uuu version: tried 1.3.124 and 1.4.72, got same error for both&lt;/LI&gt;&lt;LI&gt;added udev rules&lt;/LI&gt;&lt;LI&gt;lsusb reports that device is found "Bus 001 Device 010: ID 1fc9:0129 NXP Semiconductors"&lt;/LI&gt;&lt;LI&gt;the file the script is looking to access "/tmp/u-boot-imx8qm-mek-uuu.imx" doesn't exist&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Are there any commands I can use to directly flash without use of script?&lt;/P&gt;&lt;P&gt;&amp;gt;sudo ./uuu_imx_android_flash.sh -f imx8qm -e&lt;BR /&gt;This script is validated with uuu 1.4.72 version, it is recommended to align with this version.&lt;BR /&gt;dtbo is supported&lt;BR /&gt;dual slot is supported&lt;BR /&gt;dynamic parttition is supported&lt;BR /&gt;vendor_boot parttition is supported&lt;BR /&gt;generate lines to flash u-boot-imx8qm.imx to the partition of bootloader0&lt;BR /&gt;generate lines to flash partition-table.img to the partition of gpt&lt;BR /&gt;generate lines to flash dtbo-imx8qm.img to the partition of dtbo_a&lt;BR /&gt;generate lines to flash boot.img to the partition of boot_a&lt;BR /&gt;generate lines to flash vendor_boot.img to the partition of vendor_boot_a&lt;BR /&gt;generate lines to flash vbmeta-imx8qm.img to the partition of vbmeta_a&lt;BR /&gt;generate lines to flash dtbo-imx8qm.img to the partition of dtbo_b&lt;BR /&gt;generate lines to flash boot.img to the partition of boot_b&lt;BR /&gt;generate lines to flash vendor_boot.img to the partition of vendor_boot_b&lt;BR /&gt;generate lines to flash vbmeta-imx8qm.img to the partition of vbmeta_b&lt;BR /&gt;generate lines to flash super.img to the partition of super&lt;BR /&gt;uuu script generated, start to invoke uuu with the generated uuu script&lt;BR /&gt;uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.127-9-g22c5181&lt;/P&gt;&lt;P&gt;Wait for Known USB Device Appear...&lt;BR /&gt;&lt;STRONG&gt;Error: fail open file: &amp;gt;/tmp/u-boot-imx8qm-mek-uuu.imx&lt;/STRONG&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 24 May 2021 15:51:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issue-flashing-prebuilt-android-image/m-p/1281199#M174456</guid>
      <dc:creator>pwcel</dc:creator>
      <dc:date>2021-05-24T15:51:56Z</dc:date>
    </item>
    <item>
      <title>Re: Issue flashing prebuilt android image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issue-flashing-prebuilt-android-image/m-p/1281357#M174462</link>
      <description>&lt;P&gt;Hi Kelly&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;one can try to follow sect."Programming Images" Android User's Guide on link&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/software/embedded-software/i-mx-software/android-os-for-i-mx-applications-processors:IMXANDROID?tab=In-Depth_Tab" target="_blank"&gt;https://www.nxp.com/design/software/embedded-software/i-mx-software/android-os-for-i-mx-applications-processors:IMXANDROID?tab=In-Depth_Tab&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Mon, 24 May 2021 23:37:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issue-flashing-prebuilt-android-image/m-p/1281357#M174462</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-05-24T23:37:28Z</dc:date>
    </item>
    <item>
      <title>Re: Issue flashing prebuilt android image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issue-flashing-prebuilt-android-image/m-p/1282041#M174519</link>
      <description>&lt;P&gt;[replied to message below]&lt;/P&gt;</description>
      <pubDate>Tue, 25 May 2021 20:27:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issue-flashing-prebuilt-android-image/m-p/1282041#M174519</guid>
      <dc:creator>pwcel</dc:creator>
      <dc:date>2021-05-25T20:27:29Z</dc:date>
    </item>
    <item>
      <title>Re: Issue flashing prebuilt android image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issue-flashing-prebuilt-android-image/m-p/1282044#M174520</link>
      <description>&lt;P&gt;Thanks for the reference Igor.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Do you know where I can download ' imx-sdcard-partition.sh'?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Seems I can download Linux pre-built image, but not Android for some reason.&lt;/P&gt;</description>
      <pubDate>Tue, 25 May 2021 20:26:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issue-flashing-prebuilt-android-image/m-p/1282044#M174520</guid>
      <dc:creator>pwcel</dc:creator>
      <dc:date>2021-05-25T20:26:19Z</dc:date>
    </item>
    <item>
      <title>Re: Issue flashing prebuilt android image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issue-flashing-prebuilt-android-image/m-p/1283585#M174636</link>
      <description>&lt;P&gt;Issue was that I was trying to download the wrong software. iMX 8 Quad 8M != iMX 8 QuadMax&lt;/P&gt;&lt;P&gt;Script is in the iMX8QM image package&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 27 May 2021 15:25:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issue-flashing-prebuilt-android-image/m-p/1283585#M174636</guid>
      <dc:creator>pwcel</dc:creator>
      <dc:date>2021-05-27T15:25:34Z</dc:date>
    </item>
  </channel>
</rss>