<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Booting Firmware from Different Memory Location in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Booting-Firmware-from-Different-Memory-Location/m-p/1281572#M174479</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are working on designing Firmware Over the Air features on the iMX RT1020 MCU. We have defined three partition in external QSPI flash which is XIP.&lt;/P&gt;&lt;P&gt;0x60000000 - Bootloader&lt;BR /&gt;0x60081000 - Firmware 1&lt;BR /&gt;0x60211000 - Firmware 2&lt;/P&gt;&lt;P&gt;Initially, the bootloader will boot from the firmware stored at memory location&amp;nbsp;0x60081000. When the request for firmware upgrade receives, the device will check the active firmware partition and will download the image at inactive partition. For the first firmware upgrade, image will be downloaded at&amp;nbsp;memory location 0x60211000.&lt;/P&gt;&lt;P&gt;We need to now boot from the second partition which is&amp;nbsp;0x60211000.&lt;/P&gt;&lt;P&gt;Question: Is it possible to boot an image stored at address 0x60211000 if binary is compiled with flash configuration in the MCUXpresso as below, (first partition address)&lt;/P&gt;&lt;P&gt;BOARD_FLASH (rx) : ORIGIN = 0x60081000, LENGTH = 0x800000 /* 8M bytes (alias Flash) */&lt;/P&gt;&lt;P&gt;Is there any way we can configure the addresses relative rather than absolute from the linker script.&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Dipak Sharma&lt;/P&gt;</description>
    <pubDate>Tue, 25 May 2021 07:53:02 GMT</pubDate>
    <dc:creator>Dipak01</dc:creator>
    <dc:date>2021-05-25T07:53:02Z</dc:date>
    <item>
      <title>Booting Firmware from Different Memory Location</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Booting-Firmware-from-Different-Memory-Location/m-p/1281572#M174479</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are working on designing Firmware Over the Air features on the iMX RT1020 MCU. We have defined three partition in external QSPI flash which is XIP.&lt;/P&gt;&lt;P&gt;0x60000000 - Bootloader&lt;BR /&gt;0x60081000 - Firmware 1&lt;BR /&gt;0x60211000 - Firmware 2&lt;/P&gt;&lt;P&gt;Initially, the bootloader will boot from the firmware stored at memory location&amp;nbsp;0x60081000. When the request for firmware upgrade receives, the device will check the active firmware partition and will download the image at inactive partition. For the first firmware upgrade, image will be downloaded at&amp;nbsp;memory location 0x60211000.&lt;/P&gt;&lt;P&gt;We need to now boot from the second partition which is&amp;nbsp;0x60211000.&lt;/P&gt;&lt;P&gt;Question: Is it possible to boot an image stored at address 0x60211000 if binary is compiled with flash configuration in the MCUXpresso as below, (first partition address)&lt;/P&gt;&lt;P&gt;BOARD_FLASH (rx) : ORIGIN = 0x60081000, LENGTH = 0x800000 /* 8M bytes (alias Flash) */&lt;/P&gt;&lt;P&gt;Is there any way we can configure the addresses relative rather than absolute from the linker script.&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Dipak Sharma&lt;/P&gt;</description>
      <pubDate>Tue, 25 May 2021 07:53:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Booting-Firmware-from-Different-Memory-Location/m-p/1281572#M174479</guid>
      <dc:creator>Dipak01</dc:creator>
      <dc:date>2021-05-25T07:53:02Z</dc:date>
    </item>
    <item>
      <title>Re: Booting Firmware from Different Memory Location</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Booting-Firmware-from-Different-Memory-Location/m-p/1283605#M174637</link>
      <description>&lt;P&gt;Hello Dipak,&lt;/P&gt;
&lt;P&gt;You want to compile an image with one address, but you want to execute it from a completely different address, correct? If so, this is not possible.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Victor&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 27 May 2021 16:17:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Booting-Firmware-from-Different-Memory-Location/m-p/1283605#M174637</guid>
      <dc:creator>victorjimenez</dc:creator>
      <dc:date>2021-05-27T16:17:31Z</dc:date>
    </item>
    <item>
      <title>Re: Booting Firmware from Different Memory Location</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Booting-Firmware-from-Different-Memory-Location/m-p/1283614#M174638</link>
      <description>&lt;P&gt;Hi Victor,&lt;/P&gt;&lt;P&gt;Thanks for the information.&lt;/P&gt;&lt;P&gt;You have correctly understood my concern. Yes, It is not possible. We will look for some alternatives.&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Dipak Sharma&lt;/P&gt;</description>
      <pubDate>Thu, 27 May 2021 16:31:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Booting-Firmware-from-Different-Memory-Location/m-p/1283614#M174638</guid>
      <dc:creator>Dipak01</dc:creator>
      <dc:date>2021-05-27T16:31:07Z</dc:date>
    </item>
  </channel>
</rss>