<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MCIMX8M-EVK - Linux image - development setup in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MCIMX8M-EVK-Linux-image-development-setup/m-p/1280880#M174435</link>
    <description>&lt;P&gt;if you need this .sh file,&amp;nbsp; you can use the command like:&lt;/P&gt;
&lt;P&gt;DISTRO=fsl-imx-wayland MACHINE=imx8mmevk source imx-setup-release.sh -b build-wayland&lt;/P&gt;
&lt;P&gt;bitbake image -c populate_sdk， for example choose core-image-minimal as image, then use the command like :&lt;/P&gt;
&lt;P&gt;bitbake core-image-minimal -c populate_sdk, then you can find this under "build-wayland/tmp/work/imx8mmevk-poky-linux/core-image-minimal/1.0-r0$"&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 24 May 2021 06:21:46 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2021-05-24T06:21:46Z</dc:date>
    <item>
      <title>MCIMX8M-EVK - Linux image - development setup</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCIMX8M-EVK-Linux-image-development-setup/m-p/1280536#M174399</link>
      <description>&lt;P&gt;Hello folks.&lt;/P&gt;&lt;P&gt;I am new to&amp;nbsp;MCIMX8M-EVK. I would like to setup by development environment. Can someone point to the correct setup file. For example, I have this file for imx8mplus:&lt;BR /&gt;fsl-imx-internal-wayland-glibc-x86_64-imx-image-full-aarch64-imx8mpevk-toolchain-5.4-zeus.sh&lt;/P&gt;&lt;P&gt;I need similar file for&amp;nbsp;MCIMX8M-EVK.&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;P&gt;Azhar&lt;/P&gt;</description>
      <pubDate>Fri, 21 May 2021 18:49:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCIMX8M-EVK-Linux-image-development-setup/m-p/1280536#M174399</guid>
      <dc:creator>azhar</dc:creator>
      <dc:date>2021-05-21T18:49:30Z</dc:date>
    </item>
    <item>
      <title>Re: MCIMX8M-EVK - Linux image - development setup</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCIMX8M-EVK-Linux-image-development-setup/m-p/1280855#M174433</link>
      <description>&lt;P&gt;if you need build environment for linux, you can refer to the yocto user guide&lt;/P&gt;
&lt;P&gt;"&lt;A href="https://www.nxp.com/docs/en/user-guide/IMX_YOCTO_PROJECT_USERS_GUIDE.pdf&amp;quot;" target="_blank"&gt;https://www.nxp.com/docs/en/user-guide/IMX_YOCTO_PROJECT_USERS_GUIDE.pdf"&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;current bsp includes the compiler&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 24 May 2021 05:47:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCIMX8M-EVK-Linux-image-development-setup/m-p/1280855#M174433</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2021-05-24T05:47:51Z</dc:date>
    </item>
    <item>
      <title>Re: MCIMX8M-EVK - Linux image - development setup</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCIMX8M-EVK-Linux-image-development-setup/m-p/1280880#M174435</link>
      <description>&lt;P&gt;if you need this .sh file,&amp;nbsp; you can use the command like:&lt;/P&gt;
&lt;P&gt;DISTRO=fsl-imx-wayland MACHINE=imx8mmevk source imx-setup-release.sh -b build-wayland&lt;/P&gt;
&lt;P&gt;bitbake image -c populate_sdk， for example choose core-image-minimal as image, then use the command like :&lt;/P&gt;
&lt;P&gt;bitbake core-image-minimal -c populate_sdk, then you can find this under "build-wayland/tmp/work/imx8mmevk-poky-linux/core-image-minimal/1.0-r0$"&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 24 May 2021 06:21:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCIMX8M-EVK-Linux-image-development-setup/m-p/1280880#M174435</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2021-05-24T06:21:46Z</dc:date>
    </item>
  </channel>
</rss>