<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Kernel stuck at starting kernel</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-stuck-at-starting-kernel/m-p/1280164#M174372</link>
    <description>&lt;P&gt;I am using a specific board designed around IMX6. The SDRAM settings are ok as we are using the same setting as for u-boot 2014 that works already with kernel 3.10. Please note that kernel 4.19 can boot with u-boot 2014 and kernel 3.10 boot also with u-boot 2019 but kernel 4.19 cannot boot with u-boot 2019.&lt;/P&gt;</description>
    <pubDate>Fri, 21 May 2021 07:16:18 GMT</pubDate>
    <dc:creator>mohamed-ali_fod</dc:creator>
    <dc:date>2021-05-21T07:16:18Z</dc:date>
    <item>
      <title>Kernel stuck at starting kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-stuck-at-starting-kernel/m-p/1278149#M174206</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;The 4.19 kernel doesn't boot on imx6, there is a hang at Starting kernel as mentioned below in case of initramfs, I attached the u-boot 2019.04 environment and kernel config, we use "setenv bootargs console=${console},${baudrate} root=/dev/ram0 rootfstype=ramfs", any idea please?&lt;/P&gt;&lt;P&gt;SF: Detected w25q256 with page size 256 Bytes, erase size 4 KiB, total 32 MiB&lt;BR /&gt;device 0 offset 0x760000, size 0x20000&lt;BR /&gt;SF: 131072 bytes @ 0x760000 Read: OK&lt;BR /&gt;device 0 offset 0x780000, size 0x500000&lt;BR /&gt;SF: 5242880 bytes @ 0x780000 Read: OK&lt;BR /&gt;device 0 offset 0xc80000, size 0x1380000&lt;BR /&gt;SF: 20447232 bytes @ 0xc80000 Read: OK&lt;BR /&gt;## Booting kernel from Legacy Image at 12000000 ...&lt;BR /&gt;Image Name: Linux-4.19.35-imx-4.19.35-1.1.0&lt;BR /&gt;Image Type: ARM Linux Kernel Image (uncompressed)&lt;BR /&gt;Data Size: 3707096 Bytes = 3.5 MiB&lt;BR /&gt;Load Address: 10008000&lt;BR /&gt;Entry Point: 10008000&lt;BR /&gt;Verifying Checksum ... OK&lt;BR /&gt;## Loading init Ramdisk from Legacy Image at 19000000 ...&lt;BR /&gt;Image Name: tgur-access-image-update-tgur-ac&lt;BR /&gt;Image Type: ARM Linux RAMDisk Image (uncompressed)&lt;BR /&gt;Data Size: 5418159 Bytes = 5.2 MiB&lt;BR /&gt;Load Address: 00000000&lt;BR /&gt;Entry Point: 00000000&lt;BR /&gt;Verifying Checksum ... OK&lt;BR /&gt;## Flattened Device Tree blob at 18000000&lt;BR /&gt;Booting using the fdt blob at 0x18000000&lt;BR /&gt;Loading Kernel Image ... OK&lt;BR /&gt;Using Device Tree in place at 18000000, end 18013cc4&lt;BR /&gt;&lt;BR /&gt;Starting kernel ...&lt;/P&gt;</description>
      <pubDate>Tue, 18 May 2021 09:53:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-stuck-at-starting-kernel/m-p/1278149#M174206</guid>
      <dc:creator>mohamed-ali_fod</dc:creator>
      <dc:date>2021-05-18T09:53:28Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel stuck at starting kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-stuck-at-starting-kernel/m-p/1278409#M174223</link>
      <description>&lt;P&gt;Kernel 3.10 is working fine with the same u-boot 2019.04&lt;/P&gt;&lt;P&gt;------START UPDATE DISTRIBUTION ------&lt;BR /&gt;SF: Detected w25q256 with page size 256 Bytes, erase size 4 KiB, total 32 MiB&lt;BR /&gt;device 0 offset 0x760000, size 0x20000&lt;BR /&gt;SF: 131072 bytes @ 0x760000 Read: OK&lt;BR /&gt;device 0 offset 0x780000, size 0x500000&lt;BR /&gt;SF: 5242880 bytes @ 0x780000 Read: OK&lt;BR /&gt;device 0 offset 0xc80000, size 0x1380000&lt;BR /&gt;SF: 20447232 bytes @ 0xc80000 Read: OK&lt;BR /&gt;## Booting kernel from Legacy Image at 12000000 ...&lt;BR /&gt;Image Name: Linux-3.10.17-rt12+pamela-dual-l&lt;BR /&gt;Image Type: ARM Linux Kernel Image (uncompressed)&lt;BR /&gt;Data Size: 3355992 Bytes = 3.2 MiB&lt;BR /&gt;Load Address: 10008000&lt;BR /&gt;Entry Point: 10008000&lt;BR /&gt;Verifying Checksum ... OK&lt;BR /&gt;## Loading init Ramdisk from Legacy Image at 19000000 ...&lt;BR /&gt;Image Name: tgur-access-image-update-tgur-ac&lt;BR /&gt;Image Type: ARM Linux RAMDisk Image (uncompressed)&lt;BR /&gt;Data Size: 5418159 Bytes = 5.2 MiB&lt;BR /&gt;Load Address: 00000000&lt;BR /&gt;Entry Point: 00000000&lt;BR /&gt;Verifying Checksum ... OK&lt;BR /&gt;## Flattened Device Tree blob at 18000000&lt;BR /&gt;Booting using the fdt blob at 0x18000000&lt;BR /&gt;Loading Kernel Image ... OK&lt;BR /&gt;Using Device Tree in place at 18000000, end 1800dbfa&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;Booting Linux on physical CPU 0x0&lt;BR /&gt;Initializing cgroup subsys cpuset&lt;BR /&gt;Initializing cgroup subsys cpu&lt;BR /&gt;Initializing cgroup subsys cpuacct&lt;BR /&gt;Linux version 3.10.17-rt12+pamela-dual-lite-04.09.15+gc88bcca (actia-es@bbc65510a8cd) (gcc version 4.8.4 (GCC) ) #1 PREEMPT RT Sun Apr 25 13:54:14 UTC 2021&lt;BR /&gt;CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c5387d&lt;BR /&gt;CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache&lt;BR /&gt;Machine: Freescale i.MX6 Quad/DualLite (Device Tree), model: Pamela TGUR Access i.MX6 Solo Board&lt;BR /&gt;cma: CMA: reserved 32 MiB at 4e000000&lt;BR /&gt;Memory policy: ECC disabled, Data cache writeback&lt;BR /&gt;------------[ cut here ]------------&lt;BR /&gt;WARNING: at arch/arm/kernel/devtree.c:147 arm_dt_init_cpu_maps+0x11c/0x1a4()&lt;BR /&gt;DT /cpu 2 nodes greater than max cores 1, capping them&lt;BR /&gt;Modules linked in:&lt;BR /&gt;CPU: 0 PID: 0 Comm: swapper Not tainted 3.10.17-rt12+pamela-dual-lite-04.09.15+gc88bcca #1&lt;BR /&gt;[&amp;lt;8001378c&amp;gt;] (unwind_backtrace+0x0/0x134) from [&amp;lt;80011d0c&amp;gt;] (show_stack+0x10/0x14)&lt;BR /&gt;[&amp;lt;80011d0c&amp;gt;] (show_stack+0x10/0x14) from [&amp;lt;800268c0&amp;gt;] (warn_slowpath_common+0x54/0x68)&lt;BR /&gt;[&amp;lt;800268c0&amp;gt;] (warn_slowpath_common+0x54/0x68) from [&amp;lt;80026904&amp;gt;] (warn_slowpath_fmt+0x30/0x40)&lt;BR /&gt;[&amp;lt;80026904&amp;gt;] (warn_slowpath_fmt+0x30/0x40) from [&amp;lt;805ea47c&amp;gt;] (arm_dt_init_cpu_maps+0x11c/0x1a4)&lt;BR /&gt;[&amp;lt;805ea47c&amp;gt;] (arm_dt_init_cpu_maps+0x11c/0x1a4) from [&amp;lt;805e9e44&amp;gt;] (setup_arch+0x644/0x69c)&lt;BR /&gt;[&amp;lt;805e9e44&amp;gt;] (setup_arch+0x644/0x69c) from [&amp;lt;805e6798&amp;gt;] (start_kernel+0x7c/0x334)&lt;BR /&gt;[&amp;lt;805e6798&amp;gt;] (start_kernel+0x7c/0x334) from [&amp;lt;10008070&amp;gt;] (0x10008070)&lt;BR /&gt;---[ end trace 0000000000000001 ]---&lt;BR /&gt;CPU: All CPU(s) started in SVC mode.&lt;BR /&gt;Built 1 zonelists in Zone order, mobility grouping on. Total pages: 260096&lt;BR /&gt;Kernel command line: console=ttymxc0,115200 root=/dev/ram0 rootfstype=ramfs&lt;BR /&gt;PID hash table entries: 4096 (order: 2, 16384 bytes)&lt;BR /&gt;Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)&lt;BR /&gt;Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)&lt;BR /&gt;Memory: 1024MB = 1024MB total&lt;BR /&gt;Memory: 994348k/994348k available, 54228k reserved, 0K highmem&lt;BR /&gt;Virtual kernel memory layout:&lt;BR /&gt;vector : 0xffff0000 - 0xffff1000 ( 4 kB)&lt;BR /&gt;fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)&lt;BR /&gt;vmalloc : 0xc0800000 - 0xff000000 (1000 MB)&lt;BR /&gt;lowmem : 0x80000000 - 0xc0000000 (1024 MB)&lt;BR /&gt;modules : 0x7f000000 - 0x80000000 ( 16 MB)&lt;BR /&gt;.text : 0x80008000 - 0x805e56a4 (6006 kB)&lt;BR /&gt;.init : 0x805e6000 - 0x8061641c ( 194 kB)&lt;BR /&gt;.data : 0x80618000 - 0x8065e008 ( 281 kB)&lt;BR /&gt;.bss : 0x8065e008 - 0x806c3260 ( 405 kB)&lt;BR /&gt;SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1&lt;BR /&gt;NR_IRQS:16 nr_irqs:16 16&lt;/P&gt;</description>
      <pubDate>Tue, 18 May 2021 18:06:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-stuck-at-starting-kernel/m-p/1278409#M174223</guid>
      <dc:creator>mohamed-ali_fod</dc:creator>
      <dc:date>2021-05-18T18:06:31Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel stuck at starting kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-stuck-at-starting-kernel/m-p/1279617#M174315</link>
      <description>&lt;P&gt;Are you using the Yocto BSP to build the image?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 20 May 2021 08:43:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-stuck-at-starting-kernel/m-p/1279617#M174315</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2021-05-20T08:43:23Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel stuck at starting kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-stuck-at-starting-kernel/m-p/1279638#M174317</link>
      <description>&lt;P&gt;Yes I am using Yocto warrior.&lt;/P&gt;</description>
      <pubDate>Thu, 20 May 2021 09:08:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-stuck-at-starting-kernel/m-p/1279638#M174317</guid>
      <dc:creator>mohamed-ali_fod</dc:creator>
      <dc:date>2021-05-20T09:08:59Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel stuck at starting kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-stuck-at-starting-kernel/m-p/1280100#M174362</link>
      <description>&lt;P&gt;Which processor are you using? Are you building the proper image for the processor?&lt;/P&gt;
&lt;P&gt;Which board are you using? The original SDRAM settings is for the EVK board. If your board is using different SDRAM, the SDRAM setting is needed to modify.&lt;/P&gt;
&lt;P&gt;In the u-boot, the debug console is set in the bootargs. e.g. ttymxc0. If you are using different UART for debug console, please change the bootargs in u-boot accordingly.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 21 May 2021 05:00:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-stuck-at-starting-kernel/m-p/1280100#M174362</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2021-05-21T05:00:46Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel stuck at starting kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-stuck-at-starting-kernel/m-p/1280164#M174372</link>
      <description>&lt;P&gt;I am using a specific board designed around IMX6. The SDRAM settings are ok as we are using the same setting as for u-boot 2014 that works already with kernel 3.10. Please note that kernel 4.19 can boot with u-boot 2014 and kernel 3.10 boot also with u-boot 2019 but kernel 4.19 cannot boot with u-boot 2019.&lt;/P&gt;</description>
      <pubDate>Fri, 21 May 2021 07:16:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-stuck-at-starting-kernel/m-p/1280164#M174372</guid>
      <dc:creator>mohamed-ali_fod</dc:creator>
      <dc:date>2021-05-21T07:16:18Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel stuck at starting kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-stuck-at-starting-kernel/m-p/1280357#M174383</link>
      <description>&lt;P&gt;The old u-boot is using &amp;lt;board&amp;gt;.c file for the configuration. The new version of u-boot is using device tree. Do you modify the device tree file in the new version of u-boot accordingly?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 21 May 2021 11:05:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-stuck-at-starting-kernel/m-p/1280357#M174383</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2021-05-21T11:05:19Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel stuck at starting kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-stuck-at-starting-kernel/m-p/1282431#M174551</link>
      <description>&lt;P&gt;Yes I modified the device tree the u-boot is working fine it detects usb, network, spi flash and so on....&lt;/P&gt;</description>
      <pubDate>Wed, 26 May 2021 08:57:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-stuck-at-starting-kernel/m-p/1282431#M174551</guid>
      <dc:creator>mohamed-ali_fod</dc:creator>
      <dc:date>2021-05-26T08:57:37Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel stuck at starting kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-stuck-at-starting-kernel/m-p/1283660#M174642</link>
      <description>&lt;P&gt;There are newer version of BSP that support i.MX6 processors.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX?tab=In-Depth_Tab" target="_blank"&gt;https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX?tab=In-Depth_Tab&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You may try the new version of BSP.&lt;/P&gt;</description>
      <pubDate>Thu, 27 May 2021 18:20:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-stuck-at-starting-kernel/m-p/1283660#M174642</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2021-05-27T18:20:02Z</dc:date>
    </item>
  </channel>
</rss>