<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: IMX6Q capture linux driver</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-capture-linux-driver/m-p/231366#M17431</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Omar,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1 - For documentation about relationship between ipu linux drivers, you can check the document "Lnux_6DQ_RM_L3.0.35_1.1.0.pdf" chapter 5.2 - Software Operation, pages 49 and 50. You can find this document inside L3.0.35_1.1.0_LINUXDOCS_BUNDLE package.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2 - If you use V4L2 driver, it will handle the ipu functions (e.g. rotaion, resize and etc) as needed. To know or change the way V4L2 works, you need to check/change its source code : linux/driver/media/video/mxc/output/mxc_vout.c.&lt;/P&gt;&lt;P&gt;Rgds&lt;/P&gt;&lt;P&gt;Rogerio&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 Mar 2013 17:06:48 GMT</pubDate>
    <dc:creator>rogerio_silva</dc:creator>
    <dc:date>2013-03-26T17:06:48Z</dc:date>
    <item>
      <title>IMX6Q capture linux driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-capture-linux-driver/m-p/231365#M17430</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;DEars,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a question to better understand and use the video capture part of the imx6Q.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can see in driver /media/video/imx/capture that i have ov5642.c driver (it configure I"c interface to the sensor, init register, etc etc... if mipi set up also the mipi interface).&lt;/P&gt;&lt;P&gt;then I have several layers (CIS, IPU , etc) the the last one I suppose is the V4l_imX)_capture&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;First question is:&lt;/P&gt;&lt;P&gt;1) is there any schematic block to better understand the relationship between them?)&lt;/P&gt;&lt;P&gt;2) all of that layer has their own ioctls... how i can specify wich one i want to use. (i.e the mirror or rotate can be done by IPU or by sensor itself.... how i can say from V4L2 to use that ioctl or that other....)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Omar Pighi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Mar 2013 11:55:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-capture-linux-driver/m-p/231365#M17430</guid>
      <dc:creator>Selea</dc:creator>
      <dc:date>2013-03-19T11:55:37Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6Q capture linux driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-capture-linux-driver/m-p/231366#M17431</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Omar,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1 - For documentation about relationship between ipu linux drivers, you can check the document "Lnux_6DQ_RM_L3.0.35_1.1.0.pdf" chapter 5.2 - Software Operation, pages 49 and 50. You can find this document inside L3.0.35_1.1.0_LINUXDOCS_BUNDLE package.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2 - If you use V4L2 driver, it will handle the ipu functions (e.g. rotaion, resize and etc) as needed. To know or change the way V4L2 works, you need to check/change its source code : linux/driver/media/video/mxc/output/mxc_vout.c.&lt;/P&gt;&lt;P&gt;Rgds&lt;/P&gt;&lt;P&gt;Rogerio&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Mar 2013 17:06:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-capture-linux-driver/m-p/231366#M17431</guid>
      <dc:creator>rogerio_silva</dc:creator>
      <dc:date>2013-03-26T17:06:48Z</dc:date>
    </item>
  </channel>
</rss>