<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: boot up by tftpboot in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/boot-up-by-tftpboot/m-p/1278725#M174239</link>
    <description>&lt;P&gt;anybody can give some ideas?&lt;/P&gt;</description>
    <pubDate>Wed, 19 May 2021 07:28:00 GMT</pubDate>
    <dc:creator>mm2021</dc:creator>
    <dc:date>2021-05-19T07:28:00Z</dc:date>
    <item>
      <title>boot up by tftpboot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/boot-up-by-tftpboot/m-p/1278163#M174208</link>
      <description>&lt;P&gt;I'm debugging the i.MX 8M Mini board.&lt;/P&gt;&lt;P&gt;Now I can compile the kernel and get Image file. I put the Image file to SD card to replace the old one, the board can boot up to linux smoothly.&lt;BR /&gt;Now I'd like to get Image in ubbot by tftpboot.&lt;/P&gt;&lt;P&gt;As far as I know, in uboot, I can use the following command to load Image to ram:&lt;BR /&gt;tftp &amp;lt;addr in ram&amp;gt; Image&lt;/P&gt;&lt;P&gt;But how to set the address in ddr?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 18 May 2021 10:09:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/boot-up-by-tftpboot/m-p/1278163#M174208</guid>
      <dc:creator>mm2021</dc:creator>
      <dc:date>2021-05-18T10:09:54Z</dc:date>
    </item>
    <item>
      <title>Re: boot up by tftpboot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/boot-up-by-tftpboot/m-p/1278725#M174239</link>
      <description>&lt;P&gt;anybody can give some ideas?&lt;/P&gt;</description>
      <pubDate>Wed, 19 May 2021 07:28:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/boot-up-by-tftpboot/m-p/1278725#M174239</guid>
      <dc:creator>mm2021</dc:creator>
      <dc:date>2021-05-19T07:28:00Z</dc:date>
    </item>
    <item>
      <title>Re: boot up by tftpboot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/boot-up-by-tftpboot/m-p/1281355#M174460</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/186625"&gt;@mm2021&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please read the Linux user guide, chapter 4.4.1.2 Downloading an image to MMC/SD, there you will find how to do the configuration and the steps to follow.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/user-guide/IMX_LINUX_USERS_GUIDE.pdf" target="_blank" rel="noopener"&gt;https://www.nxp.com/docs/en/user-guide/IMX_LINUX_USERS_GUIDE.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;For the loadaddr I think it is 0x40480000, also you could see this address if you, on U-boot write printenv and look for that address.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope this helps you.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Israel.&lt;/P&gt;</description>
      <pubDate>Mon, 24 May 2021 23:21:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/boot-up-by-tftpboot/m-p/1281355#M174460</guid>
      <dc:creator>nxf63675</dc:creator>
      <dc:date>2021-05-24T23:21:26Z</dc:date>
    </item>
  </channel>
</rss>