<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックUsing PCT2075DP-ARD with MIMXRT1020-EVK Board</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Using-PCT2075DP-ARD-with-MIMXRT1020-EVK-Board/m-p/1277698#M174145</link>
    <description>&lt;P&gt;Hi, I have a&amp;nbsp;MIMXRT1020-EVK Board and a&amp;nbsp;PCT2075DP-ARD. Is there some guide for making these two things together? I have already checked the 'Getting Started' for&amp;nbsp;PCT2075DP-ARD, and it has a tutorial for&amp;nbsp;Using PCT2075DP-ARD with MIMXRT1050-EVK Board.&amp;nbsp; Are the steps the same, or is there a different way? Any help is much appreciated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 17 May 2021 15:44:30 GMT</pubDate>
    <dc:creator>nilz</dc:creator>
    <dc:date>2021-05-17T15:44:30Z</dc:date>
    <item>
      <title>Using PCT2075DP-ARD with MIMXRT1020-EVK Board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-PCT2075DP-ARD-with-MIMXRT1020-EVK-Board/m-p/1277698#M174145</link>
      <description>&lt;P&gt;Hi, I have a&amp;nbsp;MIMXRT1020-EVK Board and a&amp;nbsp;PCT2075DP-ARD. Is there some guide for making these two things together? I have already checked the 'Getting Started' for&amp;nbsp;PCT2075DP-ARD, and it has a tutorial for&amp;nbsp;Using PCT2075DP-ARD with MIMXRT1050-EVK Board.&amp;nbsp; Are the steps the same, or is there a different way? Any help is much appreciated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 17 May 2021 15:44:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-PCT2075DP-ARD-with-MIMXRT1020-EVK-Board/m-p/1277698#M174145</guid>
      <dc:creator>nilz</dc:creator>
      <dc:date>2021-05-17T15:44:30Z</dc:date>
    </item>
    <item>
      <title>Re: Using PCT2075DP-ARD with MIMXRT1020-EVK Board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-PCT2075DP-ARD-with-MIMXRT1020-EVK-Board/m-p/1277790#M174152</link>
      <description>&lt;P&gt;Hello Nilz,&lt;/P&gt;
&lt;P&gt;The i.MXRT1020-EVK is very similar to the i.MXRT1050-EVK, so you should be able to follow the steps on the Getting Started for the i.MXRT1050-EVK.&lt;/P&gt;
&lt;P&gt;I hope that this information helps!&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Gustavo&lt;/P&gt;</description>
      <pubDate>Mon, 17 May 2021 22:09:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-PCT2075DP-ARD-with-MIMXRT1020-EVK-Board/m-p/1277790#M174152</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2021-05-17T22:09:56Z</dc:date>
    </item>
    <item>
      <title>Re: Using PCT2075DP-ARD with MIMXRT1020-EVK Board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-PCT2075DP-ARD-with-MIMXRT1020-EVK-Board/m-p/1281966#M174513</link>
      <description>&lt;P&gt;&lt;SPAN&gt;In the document, 'UM11581 - Arduino Shields GUI and firmware installation', on page 5 and 6,&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Under the headings '3.1.2 Modifying the EVK' and '&lt;SPAN&gt;3.1.3 Flashing the firmware'&lt;/SPAN&gt;, I have some queries(&lt;FONT color="#FF0000"&gt;In red&lt;/FONT&gt;); kindly help me with the solution.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;3.1.2 Modifying the EVK&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;There are changes that need to be made to the EVK for this step to work. Four resistors&lt;BR /&gt;need to be shunted to connect the SPI port: R280, R281, R270, R278. (&lt;FONT color="#FF0000"&gt;Do I have to do this step for&amp;nbsp;MIMXRT1020-EVK Board?&lt;FONT color="#000000"&gt;)&lt;/FONT&gt;&lt;/FONT&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;3.1.3 Flashing the firmware&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;The IMXRT1050_v1.0.8_3.bin image is required for this step. (&lt;FONT color="#FF0000"&gt;Where to find the bin image for MIMXRT1020-EVK Board?&lt;/FONT&gt;)&lt;BR /&gt;The guideline for flashing .bin image to imxrt1050 from a Windows PC includes the&lt;BR /&gt;following steps:&amp;nbsp;(&lt;FONT color="#FF0000"&gt;Are&amp;nbsp;the steps required for&amp;nbsp;MIMXRT1020-EVK Board? if so, where to find the instruction?&lt;/FONT&gt;)&lt;BR /&gt;1. Detection of rt1050 requires “Windows serial driver” which is available in the following&lt;BR /&gt;link. &lt;A href="https://os.mbed.com/docs/mbed-os/v5.14/tutorials/windows-serial-driver.html" target="_blank"&gt;https://os.mbed.com/docs/mbed-os/v5.14/tutorials/windows-serial-driver.html&lt;/A&gt;&amp;nbsp;&lt;BR /&gt;2. Connect the evk to windows PC via usb cable in j28 connector and install the driver.&lt;BR /&gt;Here we are going to flash by OpenSDA MSD drag/drop steps.&lt;BR /&gt;3. Configure the power supply from the Debug USB (connect J1 5-6).&amp;nbsp;&lt;BR /&gt;Connect J28 OpenSDA interface with USB cable.&lt;BR /&gt;4. Set SW7 to OFF-OFF-OFF-ON.&amp;nbsp;&lt;BR /&gt;5. Power on board.&lt;BR /&gt;6. Computer detects RT1050-EVK as removable device. Drag the generated *.bin file&lt;BR /&gt;into RT1050-EVK&lt;BR /&gt;7. Power off. Set SW7 to OFF-ON-ON-OFF.&lt;BR /&gt;8. Power on. Push on board reset button.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Nilanjan&lt;/P&gt;</description>
      <pubDate>Tue, 25 May 2021 16:26:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-PCT2075DP-ARD-with-MIMXRT1020-EVK-Board/m-p/1281966#M174513</guid>
      <dc:creator>nilz</dc:creator>
      <dc:date>2021-05-25T16:26:07Z</dc:date>
    </item>
    <item>
      <title>Re: Using PCT2075DP-ARD with MIMXRT1020-EVK Board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-PCT2075DP-ARD-with-MIMXRT1020-EVK-Board/m-p/1285594#M174840</link>
      <description>&lt;P&gt;Hello Nilz,&lt;/P&gt;
&lt;P&gt;Upon further observation, while the i.MXRT1020 and i.MXRT1050 are very similar, the usage of this PCT2075DP Arduino Shield requires firmware an additional HW modifications and I couldn’t locate information on what would be the required firmware and HW setup for the i.MXRT1020.&lt;/P&gt;
&lt;P&gt;My apologies for the inconvenience.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Gustavo&lt;/P&gt;</description>
      <pubDate>Tue, 01 Jun 2021 19:14:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-PCT2075DP-ARD-with-MIMXRT1020-EVK-Board/m-p/1285594#M174840</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2021-06-01T19:14:35Z</dc:date>
    </item>
  </channel>
</rss>